Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs KRIA ... reproducing the benchmark results
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: albertabeef
  • Date Created: 18 May 2021 3:42 PM Date Created
  • Views 7932 views
  • Likes 8 likes
  • Comments 10 comments
  • kria
  • benchmarking
  • vitis-ai
Related
Recommended

KRIA ... reproducing the benchmark results

albertabeef
albertabeef
18 May 2021

In this blog series, I discuss various topics regarding Kria.

 

Introduction

If you did not see my overview of the new Kria KV260 Vision AI Starter Kit, check it out on hackster:

http://avnet.me/kria-tutorial

 

I wanted to reproduce the benchmarks that were reported in the WP529 White Paper : "Kria K26 SOM: The Ideal Platform for Vision AI at the Edge".

 

As described in my hackster project, Kria now includes management of "app"s that can be installed, loaded, and unloaded, at runtime.

This is an extremely convenient feature, but as a result will not make all pre-built models from the Xilinx model zoo available.  Only the models used by each "app" are installed.

 

In order to reproduce the benchmarks, I had to first rebuild all the models from the model zoo for the Kria apps.

As you may suspect, the DPU used "can" be different for each "app", since each app includes a new bitstream.

 

Here is the workflow I describe in this blog:

  • choose an app to use for benchmarking
  • determine the DPU configuration used by the app
  • compile the model zoo for this DPU configuration
  • copy model zoo to Kria
  • install VART runtime
  • install Vitis-AI-Library examples
  • run benchmarks
  • measure power

 

I chose to use the smartcam app.

 

Determining the DPU configuration

There are several ways to determine the DPU configuration for each app.

The first is to simply check the Kria app store:

https://xilinx.github.io/kria-apps-docs/master/docs/smartcamera/docs/customize_ai_models.html

https://xilinx.github.io/kria-apps-docs/master/docs/aibox-reid/docs/customize_ai_models-aib.html

 

From these descriptions, we know that the "smartcam" and "aibox-reid" apps use the B3136 DPU.

They also indicate to the use the following arch.json file to compile AI models for this DPU architecture.

{

   "fingerprint":"0x1000020F6014406"

}

 

This is an encrypted version of the following more human-readable version, which I will use:

{

   "target":"DPUCZDX8G_ISA0_B3136_MAX_BG2"

}

 

Another way to query the DPU configuration is to use dexplorer.  The dexplorer comes with the DNNDK runtime, and can be installed as follows:

 

root@xilinx-k26-starterkit-2020_2:~# dnf install dnndk-dev

 

Attempting to use dexplorer on the KV260 turned out to be a little tricky since it expects the presence of a /usr/lib/dpu.xclbin file.

 

root@xilinx-k26-starterkit-2020_2:~# dexplorer --whoami

[DNNDK_XRT] Cannot find device, index: 0

 

root@xilinx-k26-starterkit-2020_2:~# xmutil unloadapp

Removing accel /lib/firmware/xilinx/kv260-dp

root@xilinx-k26-starterkit-2020_2:~# xmutil loadapp kv260-smartcam

...

DFX-MGRD> Loaded kv260-smartcam successfully

 

root@xilinx-k26-starterkit-2020_2:~# dexplorer --whoami

[DNNDK_XRT] Invalid bitstream: /usr/lib/dpu.xclbin

 

root@xilinx-k26-starterkit-2020_2:~# ls /usr/lib/dpu.xclbin

ls: cannot access '/usr/lib/dpu.xclbin': No such file or directory

root@xilinx-k26-starterkit-2020_2:~# ls /lib/firmware/xilinx/kv260-smartcam/kv260-smartcam.xclbin

/lib/firmware/xilinx/kv260-smartcam/kv260-smartcam.xclbin

root@xilinx-k26-starterkit-2020_2:~# ln -s /lib/firmware/xilinx/kv260-smartcam/kv260-smartcam.xclbin /usr/lib/dpu.xclbin

 

root@xilinx-k26-starterkit-2020_2:~# dexplorer --whoami

[DPU IP Spec]

IP  Timestamp            : 2020-11-02 15:15:00

DPU Core Count           : 1

 

[DPU Core Configuration List]

DPU Core                 : #0

DPU Enabled              : Yes

DPU Arch                 : B3136

DPU Target Version       : v1.4.1

DPU Freqency             : 300 MHz

Ram Usage                : Low

DepthwiseConv            : Enabled

DepthwiseConv+Relu6      : Enabled

Conv+Leakyrelu           : Enabled

Conv+Relu6               : Enabled

Channel Augmentation     : Enabled

Average Pool             : Enabled

 

root@xilinx-k26-starterkit-2020_2:~#

 

This confirms that the KV260 smartcam app has a B3136 DPU, with low RAM usage.

 

 

Compiling the Model Zoo for Kria

The compilation process went very smoothly with the previously defined arch.json file and the following script:

https://github.com/Avnet/vitis/blob/2020.2/app/zoo/compile_modelzoo.sh

 

For instructions on how to use this script, please refer to Appendix 1 in my Hackster.IO project:

http://avnet.me/vitis-ai-1.3-project

 

The resulting vitis_ai_library/models directory was copied to the SD card image’s /usr/share/vitis_ai_library directory.

 

Since I have built the modelzoo for the B3136 (low ram) DPU architecture, I have made it available here :

http://avnet.me/kv260-b3136lr-modelzoo-v1.3

 

 

Copying the Model Zoo to Kria

 

Before copy the model zoo, we need to determine if there is enough space on the root file system.  This can be achieve with the "df" command.

 

root@xilinx-k26-starterkit-2020_2:~# df

Filesystem     1K-blocks   Used Available Use% Mounted on

devtmpfs         1490120      4   1490116   1% /dev

/dev/mmcblk0p2   3029196 895236   1957832  32% /

tmpfs            2014784    180   2014604   1% /run

tmpfs            2014784    224   2014560   1% /var/volatile

/dev/mmcblk0p1   1062864 371660    691204  35% /boot

root@xilinx-k26-starterkit-2020_2:~#

 

The size of the boot partition is only 1GB, and the size of the root file system ( / ) is only 3GB, so clearly the 16GB micro SDcard is not being used to its full capacity.

 

Since the pre-built model zoo is over 5GB in size, we need to expand the root file system ( / ).  I used a script in Xilinx's dpu_optimize package to accomplish this:

 

root@xilinx-k26-starterkit-2020_2:~# wget https://github.com/Xilinx/Vitis-AI/raw/v1.3/dsa/DPU-TRD/app/dpu_sw_optimize.tar.gz

Connecting to github.com (140.82.114.3:443)

wget: note: TLS certificate validation not implemented

Connecting to raw.githubusercontent.com (185.199.111.133:443)

saving to 'dpu_sw_optimize.tar.gz'

dpu_sw_optimize.tar. 100% |********************************************************************************|  6581  0:00:00 ETA

'dpu_sw_optimize.tar.gz' saved

root@xilinx-k26-starterkit-2020_2:~# tar -xvzf dpu_sw_optimize.tar.gz

dpu_sw_optimize/

dpu_sw_optimize/zynqmp/

dpu_sw_optimize/zynqmp/functions/

dpu_sw_optimize/zynqmp/functions/irps5401

dpu_sw_optimize/zynqmp/functions/ext4_auto_resize.sh

dpu_sw_optimize/zynqmp/functions/zynqmp_qos_en.sh

dpu_sw_optimize/zynqmp/functions/irps5401.c

dpu_sw_optimize/zynqmp/README.md

dpu_sw_optimize/zynqmp/zynqmp_dpu_optimize.sh

root@xilinx-k26-starterkit-2020_2:~# cd dpu_sw_optimize/zynqmp/

root@xilinx-k26-starterkit-2020_2:~/dpu_sw_optimize/zynqmp# ./zynqmp_dpu_optimize.sh

Auto resize ext4 partition ...[✔]

Start QoS config ...[✔]

root@xilinx-k26-starterkit-2020_2:~/dpu_sw_optimize/zynqmp#

 

root@xilinx-k26-starterkit-2020_2:~/dpu_sw_optimize/zynqmp# cd -

/home/root

root@xilinx-k26-starterkit-2020_2:~# df

Filesystem     1K-blocks   Used Available Use% Mounted on

devtmpfs         1490120      4   1490116   1% /dev

/dev/mmcblk0p2  14067652 901472  12537864   7% /

tmpfs            2014784    184   2014600   1% /run

tmpfs            2014784    224   2014560   1% /var/volatile

/dev/mmcblk0p1   1062864 371660    691204  35% /boot

root@xilinx-k26-starterkit-2020_2:~#

 

We now have 12GB available on the root file system.  We can copy the model zoo over to the SD card's root file system partition.

The Vitis-AI-Library example applications expect these models to be in the following directory, so that is where I put them.

 

/usr/share/vitis_ai_library/models

 

If you have built the model zoo yourself, you can copy it to the SD card using a native linux machine.

 

$ ls /media/abbeef/root/vitis_ai_library

samples

$ sudo cp -r vitis_ai_library/models /media/abbeef/root/usr/shared/vitis_ai_library/.

 

 

Alternatively, you can download and extract it on the Kria device directly using wget and tar:

 

root@xilinx-k26-starterkit-2020_2:~# wget http://avnet.me/kv260-b3136lr-modelzoo-v1.3 -O kv260-b3136lr-modelzoo-v1.3.tar.xz

Connecting to avnet.me (12.9.136.95:80)

Connecting to avnet.me (12.9.136.95:443)

wget: note: TLS certificate validation not implemented

Connecting to docs.avnet.com (12.9.136.156:443)

saving to 'kv260-b3136lr-modelzoo-v1.3.tar.xz'

kv260-b3136lr-modelz 100% |********************************************************************************| 2121M  0:00:00 ETA

'kv260-b3136lr-modelzoo-v1.3.tar.xz' saved

 

root@xilinx-k26-starterkit-2020_2:~# mkdir -p /usr/share/vitis_ai_library

root@xilinx-k26-starterkit-2020_2:~# tar -xvJf kv260-b3136lr-modelzoo-v1.3.tar.xz -C /usr/share/vitis_ai_library/

...

 

The complete list of models in the model zoo can be queried as follows:

 

root@xilinx-k26-starterkit-2020_2:~# ls /usr/share/vitis_ai_library/models/

ENet_cityscapes_pt              inception_v2_tf             pointpillars_kitti_12000_0_pt  ssd_mobilenet_v1_coco_tf

FPN-resnet18_Endov              inception_v3                pointpillars_kitti_12000_1_pt  ssd_mobilenet_v2

FPN-resnet18_covid19-seg_pt     inception_v3_tf             refinedet_VOC_tf               ssd_mobilenet_v2_coco_tf

FPN_Res18_Medical_segmentation  inception_v3_tf2            refinedet_baseline             ssd_pedestrian_pruned_0_97

MLPerf_resnet50_v1.5_tf         inception_v4                refinedet_pruned_0_8           ssd_resnet_50_fpn_coco_tf

MT-resnet18_mixed_pt            inception_v4_2016_09_09_tf  refinedet_pruned_0_92          ssd_traffic_pruned_0_9

RefineDet-Medical_EDD_tf        medical_seg_cell_tf2        refinedet_pruned_0_96          ssdlite_mobilenet_v2_coco_tf

SemanticFPN_cityscapes_pt       mlperf_ssd_resnet34_tf      reid                           tiny_yolov3_vmss

densebox_320_320                mobilenet_1_0_224_tf2       resnet18                       unet_chaos-CT_pt

densebox_640_360                mobilenet_edge_0_75_tf      resnet50                       vgg_16_tf

face-quality                    mobilenet_edge_1_0_tf       resnet50_tf2                   vgg_19_tf

face-quality_pt                 mobilenet_v1_0_25_128_tf    resnet_v1_101_tf               vpgnet_pruned_0_99

face_landmark                   mobilenet_v1_0_5_160_tf     resnet_v1_152_tf               yolov2_voc

facerec-resnet20_mixed_pt       mobilenet_v1_1_0_224_tf     resnet_v1_50_tf                yolov2_voc_pruned_0_66

facerec_resnet20                mobilenet_v2                resnet_v2_101_tf               yolov2_voc_pruned_0_71

facerec_resnet64                mobilenet_v2_1_0_224_tf     resnet_v2_152_tf               yolov2_voc_pruned_0_77

facereid-large_pt               mobilenet_v2_1_4_224_tf     resnet_v2_50_tf                yolov3_adas_pruned_0_9

facereid-small_pt               mobilenet_v2_cityscapes_tf  retinaface                     yolov3_bdd

fpn                             multi_task                  salsanext_pt                   yolov3_voc

hourglass-pe_mpii               openpose_pruned_0_3         semantic_seg_citys_tf2         yolov3_voc_tf

inception_resnet_v2_tf          personreid-res18_pt         sp_net                         yolov4_leaky_spp_m

inception_v1                    personreid-res50_pt         squeezenet

inception_v1_tf                 plate_detect                ssd_adas_pruned_0_95

inception_v2                    plate_num                   ssd_inception_v2_coco_tf

 

 

Install the VART runtime

 

The VART runtime and Vitis-AI-Library support can be installed with dnf, if not done so already.

 

root@xilinx-k26-starterkit-2020_2:~# dnf install vart

Last metadata expiration check: 0:00:54 ago on Tue May 18 10:00:18 2021.

Package vart-1.3.0-r0.0.aarch64 is already installed.

Dependencies resolved.

Nothing to do.

Complete!

root@xilinx-k26-starterkit-2020_2:~# dnf install vitis-ai-library

Last metadata expiration check: 0:01:00 ago on Tue May 18 10:00:18 2021.

Package vitis-ai-library-1.3.0-r0.0.aarch64 is already installed.

Dependencies resolved.

Nothing to do.

Complete!

root@xilinx-k26-starterkit-2020_2:~#

 

 

Install build tools

In order to build the Vitis-AI-Library examples, we need to install some build tools.

There may be another package that includes the ones I have identified, but installing these packages has worked for me.

 

root@xilinx-k26-starterkit-2020_2:~# dnf install cmake

root@xilinx-k26-starterkit-2020_2:~# dnf install g++

root@xilinx-k26-starterkit-2020_2:~# dnf install g++-symlinks

root@xilinx-k26-starterkit-2020_2:~# dnf install gcc-symlinks

root@xilinx-k26-starterkit-2020_2:~# dnf install binutils

root@xilinx-k26-starterkit-2020_2:~# dnf install pkgconfig

 

In addition, the smartcam Kria app has a "development" package define, which also needs to be installed.

 

root@xilinx-k26-starterkit-2020_2:~# dnf install packagegroup-kv260-smartcam-dev

 

We also need to install the glog, protobuf, and opencv libraries.

 

root@xilinx-k26-starterkit-2020_2:~# dnf install libglog-dev

root@xilinx-k26-starterkit-2020_2:~# dnf install libprotobuf-dev

root@xilinx-k26-starterkit-2020_2:~# dnf install packagegroup-petalinux-opencv-dev

 

 

And finally, we need to install git.

 

root@xilinx-k26-starterkit-2020_2:~# dnf install git

 

 

Install the Vitis-AI-Library examples

 

Next, we install the Vitis-AI-Library examples (from the Vitis-AI github repository), along with images and video files (from separate downloadable archives)

 

root@xilinx-k26-starterkit-2020_2:~# git clone -b v1.3 http://github.com/Xilinx/Vitis-AI

Cloning into 'Vitis-AI'...

warning: redirecting to https://github.com/Xilinx/Vitis-AI/

remote: Enumerating objects: 45300, done.

remote: Counting objects: 100% (1721/1721), done.

remote: Compressing objects: 100% (962/962), done.

remote: Total 45300 (delta 771), reused 1443 (delta 640), pack-reused 43579

Receiving objects: 100% (45300/45300), 1.16 GiB | 8.89 MiB/s, done.

Resolving deltas: 100% (17716/17716), done.

Updating files: 100% (25165/25165), done.

root@xilinx-k26-starterkit-2020_2:~# wget https://www.xilinx.com/bin/public/openDownload?filename=vitis_ai_library_r1.3.0_images.tar.gz -O vitis_ai_library_r1.3.0_images.tar.gz

Connecting to www.xilinx.com (23.78.212.102:443)

wget: note: TLS certificate validation not implemented

Connecting to xilinx.entitlenow.com (50.18.203.105:443)

Connecting to xilinx-ax-dl.entitlenow.com (23.41.208.67:443)

saving to 'vitis_ai_library_r1.3.0_images.tar.gz'

vitis_ai_library_r1. 100% |********************************************************************************|  178M  0:00:00 ETA

'vitis_ai_library_r1.3.0_images.tar.gz' saved

root@xilinx-k26-starterkit-2020_2:~# wget https://www.xilinx.com/bin/public/openDownload?filename=vitis_ai_library_r1.3.0_video.tar.gz -O vitis_ai_library_r1.3.0_video.tar.gz

Connecting to www.xilinx.com (23.78.212.102:443)

wget: note: TLS certificate validation not implemented

Connecting to xilinx.entitlenow.com (50.18.203.105:443)

Connecting to xilinx-ax-dl.entitlenow.com (23.41.208.67:443)

saving to 'vitis_ai_library_r1.3.0_video.tar.gz'

vitis_ai_library_r1. 100% |********************************************************************************|  683M  0:00:00 ETA

'vitis_ai_library_r1.3.0_video.tar.gz' saved

root@xilinx-k26-starterkit-2020_2:~#

root@xilinx-k26-starterkit-2020_2:~# tar -xzvf vitis_ai_library_r1.3.0_images.tar.gz -C Vitis-AI/demo/Vitis-AI-Library

...

root@xilinx-k26-starterkit-2020_2:~# tar -xzvf vitis_ai_library_r1.3.0_video.tar.gz -C Vitis-AI/demo/Vitis-AI-Library

...

root@xilinx-k26-starterkit-2020_2:~#

 

 

 

Run Benchmarks

 

Prior to running the Vitis-AI-Library benchmarking applications, we need to load the smartcam app.

 

root@xilinx-k26-starterkit-2020_2:~# xmutil unloadapp

Removing accel /lib/firmware/xilinx/kv260-dp

root@xilinx-k26-starterkit-2020_2:~# xmutil loadapp kv260-smartcam

[ 1781.374226] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /fpga-full/firmware-name

[ 1781.384313] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /fpga-full/fpga-config-from-dmabuf

[ 1781.395267] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /fpga-full/resets

[ 1781.404839] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /amba/zynqmp-display@fd4a0000/status

[ 1781.415968] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /amba/zynqmp-display@fd4a0000/zynqmp_dp_snd_pcm0/status

[ 1781.428743] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /amba/zynqmp-display@fd4a0000/zynqmp_dp_snd_pcm1/status

[ 1781.441515] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /amba/zynqmp-display@fd4a0000/zynqmp_dp_snd_card/status

[ 1781.454288] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /amba/zynqmp-display@fd4a0000/zynqmp_dp_snd_codec0/status

[ 1781.467831] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/overlay0

[ 1781.477662] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/overlay1

[ 1781.487488] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/afi0

[ 1781.496965] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/clocking0

[ 1781.506879] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/clocking1

[ 1781.516792] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/overlay2

[ 1781.526619] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/overlay7

[ 1781.536444] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/misc_clk_0

[ 1781.546444] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/misc_clk_1

[ 1781.556445] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/misc_clk_2

[ 1781.566451] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/misc_clk_5

[ 1781.576450] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/misc_clk_6

[ 1781.586450] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/overlay8

[ 1781.596276] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/ap1302_clk

[ 1781.606276] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/ap1302_vdd

[ 1781.616275] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/ap1302_vaa

[ 1781.626274] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/ap1302_vddio

[ 1781.636447] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/axi_iic

[ 1781.646187] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/i2c_mux

[ 1781.655925] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/ap1302

[ 1781.665578] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/isp_out

[ 1781.675318] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/isp_csiss

[ 1781.685230] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/isp_csiss_out

[ 1781.695489] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/isp_csiss_in

[ 1781.705663] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/isp_fb_wr_csi

[ 1781.715922] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/isp_vcap_csi_in

[ 1781.726356] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/overlay9

[ 1781.736182] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/i2s_audio_formatter

[ 1781.746963] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/audio_rx

[ 1781.756788] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/audio_tx

[ 1781.766615] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/overlay10

[ 1781.776526] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/vcu

[ 1781.785920] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/al5e

[ 1781.795400] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/al5d

[ 1781.804886] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/overlay11

[ 1781.814798] OF: overlay: WARNING: memory leak will occur if overlay removed, property: /__symbols__/zocl

[ 1781.844708] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000

[ 1782.081422] debugfs: Directory '4-003c' with parent 'regmap' already present!

[ 1789.538930] xlnx_snd_card xlnx_snd_card.1.auto: ASoC: failed to init link xilinx-i2s_playback: -517

[ 1789.548004] xlnx_snd_card xlnx_snd_card.1.auto: xlnx-i2s-snd-card-0 registration failed

[ 1789.556982] xlnx_snd_card xlnx_snd_card.1.auto: ASoC: failed to init link xilinx-i2s_playback: -517

[ 1789.566035] xlnx_snd_card xlnx_snd_card.1.auto: xlnx-i2s-snd-card-0 registration failed

[ 1789.606372] zocl-drm amba:zyxclmm_drm: IRQ index 8 not found

DFX-MGRD> Loaded kv260-smartcam successfully

root@xilinx-k26-starterkit-2020_2:~#

 

root@xilinx-k26-starterkit-2020_2:~# cd Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification#

 

We need to build the applications, which can be accomplished with the provided build.sh script:

 

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification# ./build.sh

 

 

The "Inception V4" benchmark can be run with the "inception_v4" model as follows:

 

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification# ./test_performance_classification inception_v4 ./test_performance_classification.list

WARNING: Logging before InitGoogleLogging() is written to STDERR

I0517 08:54:39.092998  1368 benchmark.hpp:176] writing report to <STDOUT>

I0517 08:54:39.093426  1368 benchmark.hpp:203] waiting for 0/30 seconds, 1 threads running

I0517 08:54:49.093545  1368 benchmark.hpp:203] waiting for 10/30 seconds, 1 threads running

I0517 08:54:59.093717  1368 benchmark.hpp:203] waiting for 20/30 seconds, 1 threads running

I0517 08:55:09.093981  1368 benchmark.hpp:211] waiting for threads terminated

FPS=21.7154

E2E_MEAN=45918.8

DPU_MEAN=44712.8

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification# ./test_performance_classification inception_v4 ./test_performance_classification.list  -t 2

WARNING: Logging before InitGoogleLogging() is written to STDERR

I0517 08:55:38.212355  1372 benchmark.hpp:176] writing report to <STDOUT>

I0517 08:55:38.449954  1372 benchmark.hpp:203] waiting for 0/30 seconds, 2 threads running

I0517 08:55:48.450148  1372 benchmark.hpp:203] waiting for 10/30 seconds, 2 threads running

I0517 08:55:58.450333  1372 benchmark.hpp:203] waiting for 20/30 seconds, 2 threads running

I0517 08:56:08.450574  1372 benchmark.hpp:211] waiting for threads terminated

FPS=22.2965

E2E_MEAN=89349.7

DPU_MEAN=88150.2

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification#

 

The "VGG-16" benchmark can be run with the "vgg_16_tf" model as follows:

 

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification# ./test_performance_classification vgg_16_tf ./test_performance_classification.list

WARNING: Logging before InitGoogleLogging() is written to STDERR

I0517 08:58:34.406569  1377 benchmark.hpp:176] writing report to <STDOUT>

I0517 08:58:34.406996  1377 benchmark.hpp:203] waiting for 0/30 seconds, 1 threads running

I0517 08:58:44.407114  1377 benchmark.hpp:203] waiting for 10/30 seconds, 1 threads running

I0517 08:58:54.407289  1377 benchmark.hpp:203] waiting for 20/30 seconds, 1 threads running

I0517 08:59:04.407541  1377 benchmark.hpp:211] waiting for threads terminated

FPS=24.6415

E2E_MEAN=40484.6

DPU_MEAN=39740.1

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification# ./test_performance_classification vgg_16_tf ./test_performance_classification.list -t 2

WARNING: Logging before InitGoogleLogging() is written to STDERR

I0517 08:59:13.142040  1379 benchmark.hpp:176] writing report to <STDOUT>

I0517 08:59:13.173197  1379 benchmark.hpp:203] waiting for 0/30 seconds, 2 threads running

I0517 08:59:23.173395  1379 benchmark.hpp:203] waiting for 10/30 seconds, 2 threads running

I0517 08:59:33.173573  1379 benchmark.hpp:203] waiting for 20/30 seconds, 2 threads running

I0517 08:59:43.173820  1379 benchmark.hpp:211] waiting for threads terminated

FPS=25.1091

E2E_MEAN=79404.2

DPU_MEAN=78672.6

 

The "Tiny Yolo V3" benchmark can be run with the "tiny_yolov3_vmss" model as follows:

 

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification# ./test_performance_classification tiny_yolov3_vmss ./test_performance_classification.list

WARNING: Logging before InitGoogleLogging() is written to STDERR

I0517 09:01:08.726274  1383 benchmark.hpp:176] writing report to <STDOUT>

I0517 09:01:08.726711  1383 benchmark.hpp:203] waiting for 0/30 seconds, 1 threads running

I0517 09:01:18.726832  1383 benchmark.hpp:203] waiting for 10/30 seconds, 1 threads running

I0517 09:01:28.727010  1383 benchmark.hpp:203] waiting for 20/30 seconds, 1 threads running

I0517 09:01:38.727262  1383 benchmark.hpp:211] waiting for threads terminated

FPS=87.567

E2E_MEAN=11412.4

DPU_MEAN=9558.2

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification# ./test_performance_classification tiny_yolov3_vmss ./test_performance_classification.list -t 2

WARNING: Logging before InitGoogleLogging() is written to STDERR

I0517 09:01:50.013595  1390 benchmark.hpp:176] writing report to <STDOUT>

I0517 09:01:50.048226  1390 benchmark.hpp:203] waiting for 0/30 seconds, 2 threads running

I0517 09:02:00.048419  1390 benchmark.hpp:203] waiting for 10/30 seconds, 2 threads running

I0517 09:02:10.048614  1390 benchmark.hpp:203] waiting for 20/30 seconds, 2 threads running

I0517 09:02:20.048866  1390 benchmark.hpp:211] waiting for threads terminated

FPS=104.659

E2E_MEAN=19094.4

DPU_MEAN=17283.1

 

The "ResNet-50" benchmark can be run with the "resnet50" model as follows:

 

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification# ./test_performance_classification resnet50 ./test_performance_classification.list

WARNING: Logging before InitGoogleLogging() is written to STDERR

I0517 09:02:48.036540  1397 benchmark.hpp:176] writing report to <STDOUT>

I0517 09:02:48.036958  1397 benchmark.hpp:203] waiting for 0/30 seconds, 1 threads running

I0517 09:02:58.037081  1397 benchmark.hpp:203] waiting for 10/30 seconds, 1 threads running

I0517 09:03:08.037258  1397 benchmark.hpp:203] waiting for 20/30 seconds, 1 threads running

I0517 09:03:18.037518  1397 benchmark.hpp:211] waiting for threads terminated

FPS=56.6142

E2E_MEAN=17623.9

DPU_MEAN=16854

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification# ./test_performance_classification resnet50 ./test_performance_classification.list -t 2

WARNING: Logging before InitGoogleLogging() is written to STDERR

I0517 09:03:29.841747  1400 benchmark.hpp:176] writing report to <STDOUT>

I0517 09:03:29.959035  1400 benchmark.hpp:203] waiting for 0/30 seconds, 2 threads running

I0517 09:03:39.959229  1400 benchmark.hpp:203] waiting for 10/30 seconds, 2 threads running

I0517 09:03:49.959414  1400 benchmark.hpp:203] waiting for 20/30 seconds, 2 threads running

I0517 09:03:59.959667  1400 benchmark.hpp:211] waiting for threads terminated

FPS=59.2421

E2E_MEAN=33676.1

DPU_MEAN=32919.4

 

The "SSD Mobilenet-V1" benchmark can be run with the "ssd_mobilenet_v1_coco_tf" model as follows:

 

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification# ./test_performance_classification ssd_mobilenet_v1_coco_tf ./test_performance_classification.list

WARNING: Logging before InitGoogleLogging() is written to STDERR

I0517 09:04:33.465210  1403 benchmark.hpp:176] writing report to <STDOUT>

I0517 09:04:33.465633  1403 benchmark.hpp:203] waiting for 0/30 seconds, 1 threads running

I0517 09:04:43.465754  1403 benchmark.hpp:203] waiting for 10/30 seconds, 1 threads running

I0517 09:04:53.465931  1403 benchmark.hpp:203] waiting for 20/30 seconds, 1 threads running

I0517 09:05:03.466182  1403 benchmark.hpp:211] waiting for threads terminated

FPS=121.656

E2E_MEAN=8211.38

DPU_MEAN=7106.28

root@xilinx-k26-starterkit-2020_2:~/Vitis-AI-avnet/demo/Vitis-AI-Library/samples/classification# ./test_performance_classification ssd_mobilenet_v1_coco_tf ./test_performance_classification.list -t 2

WARNING: Logging before InitGoogleLogging() is written to STDERR

I0517 09:05:09.751721  1405 benchmark.hpp:176] writing report to <STDOUT>

I0517 09:05:09.794981  1405 benchmark.hpp:203] waiting for 0/30 seconds, 2 threads running

I0517 09:05:19.795178  1405 benchmark.hpp:203] waiting for 10/30 seconds, 2 threads running

I0517 09:05:29.795367  1405 benchmark.hpp:203] waiting for 20/30 seconds, 2 threads running

I0517 09:05:39.795616  1405 benchmark.hpp:211] waiting for threads terminated

FPS=140.663

E2E_MEAN=14201.6

DPU_MEAN=13083.4

 

 

Nearly all of the benchmark results were slightly higher than those reported in the WP529 White Paper.

  • Sign in to reply

Top Comments

  • kevinkeryk
    kevinkeryk over 5 years ago +1
    Thank you Mario for showing how to do this so that we can compare "Apples to Apples" with other platforms to see the true performance increase that we see with the DPU acceleration! -Kevin
  • quandv
    quandv over 5 years ago +1
    Thank Mario for very interesting blog. I am going through your instructions but I've encountered issues: 1. It failed with command: dnf install packagegroup-petalinux-kv260-smartcam-dev result: "Last metadata…
  • quandv
    quandv over 5 years ago in reply to quandv +1
    The command dnf install packagegroup-petalinux-kv260-smartcam-dev didn't work with me, then I tried dnf install packagegroup-kv260-smartcam-dev. It's working. ./build.sh is also working.
Parents
  • quandv
    quandv over 5 years ago

    Thank Mario for very interesting blog.

    I am going through your instructions but I've encountered issues:

    1. It failed with command: dnf install packagegroup-petalinux-kv260-smartcam-dev

    result: "Last metadata expiration check: 12:45:37 ago on Sun Jul 11 19:02:37 2021.

    No match for argument: packagegroup-petalinux-kv260-aibox-reid-dev

    Error: Unable to find a match"

     

    2. I cannot build examples, I think it related to issue 1.

    xilinx-k26-starterkit-2020_2:~/Vitis-AI/demo/Vitis-AI-Library/samples/classification$ ./build.sh

    test_accuracy_classification.cpp:16:10: fatal error: vitis/ai/proto/dpu_model_param.pb.h: No such file or directory

       16 | #include <vitis/ai/proto/dpu_model_param.pb.h>

          |          ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

    compilation terminated.

    test_accuracy_classification_mt.cpp:16:10: fatal error: glog/logging.h: No such file or directory

       16 | #include <glog/logging.h>

          |          ^~~~~~~~~~~~~~~~

    compilation terminated.

    test_accuracy_classification_squeezenet.cpp:16:10: fatal error: glog/logging.h: No such file or directory

       16 | #include <glog/logging.h>

          |          ^~~~~~~~~~~~~~~~

    compilation terminated.

    test_jpeg_classification.cpp:16:10: fatal error: glog/logging.h: No such file or directory

       16 | #include <glog/logging.h>

          |          ^~~~~~~~~~~~~~~~

    compilation terminated.

    test_jpeg_classification_cifar.cpp:18:10: fatal error: opencv2/core.hpp: No such file or directory

       18 | #include <opencv2/core.hpp>

          |          ^~~~~~~~~~~~~~~~~~

    compilation terminated.

    test_jpeg_classification_squeezenet.cpp:16:10: fatal error: glog/logging.h: No such file or directory

       16 | #include <glog/logging.h>

          |          ^~~~~~~~~~~~~~~~

    compilation terminated.

    test_performance_classification.cpp:17:10: fatal error: vitis/ai/benchmark.hpp: No such file or directory

       17 | #include <vitis/ai/benchmark.hpp>

          |          ^~~~~~~~~~~~~~~~~~~~~~~~

    compilation terminated.

    test_performance_classification_squeezenet.cpp:18:10: fatal error: vitis/ai/benchmark.hpp: No such file or directory

       18 | #include <vitis/ai/benchmark.hpp>

          |          ^~~~~~~~~~~~~~~~~~~~~~~~

    compilation terminated.

    test_video_classification.cpp:16:10: fatal error: glog/logging.h: No such file or directory

       16 | #include <glog/logging.h>

          |          ^~~~~~~~~~~~~~~~

    compilation terminated.

     

    Please help to take a look into it.

    Thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • quandv
    quandv over 5 years ago

    Thank Mario for very interesting blog.

    I am going through your instructions but I've encountered issues:

    1. It failed with command: dnf install packagegroup-petalinux-kv260-smartcam-dev

    result: "Last metadata expiration check: 12:45:37 ago on Sun Jul 11 19:02:37 2021.

    No match for argument: packagegroup-petalinux-kv260-aibox-reid-dev

    Error: Unable to find a match"

     

    2. I cannot build examples, I think it related to issue 1.

    xilinx-k26-starterkit-2020_2:~/Vitis-AI/demo/Vitis-AI-Library/samples/classification$ ./build.sh

    test_accuracy_classification.cpp:16:10: fatal error: vitis/ai/proto/dpu_model_param.pb.h: No such file or directory

       16 | #include <vitis/ai/proto/dpu_model_param.pb.h>

          |          ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

    compilation terminated.

    test_accuracy_classification_mt.cpp:16:10: fatal error: glog/logging.h: No such file or directory

       16 | #include <glog/logging.h>

          |          ^~~~~~~~~~~~~~~~

    compilation terminated.

    test_accuracy_classification_squeezenet.cpp:16:10: fatal error: glog/logging.h: No such file or directory

       16 | #include <glog/logging.h>

          |          ^~~~~~~~~~~~~~~~

    compilation terminated.

    test_jpeg_classification.cpp:16:10: fatal error: glog/logging.h: No such file or directory

       16 | #include <glog/logging.h>

          |          ^~~~~~~~~~~~~~~~

    compilation terminated.

    test_jpeg_classification_cifar.cpp:18:10: fatal error: opencv2/core.hpp: No such file or directory

       18 | #include <opencv2/core.hpp>

          |          ^~~~~~~~~~~~~~~~~~

    compilation terminated.

    test_jpeg_classification_squeezenet.cpp:16:10: fatal error: glog/logging.h: No such file or directory

       16 | #include <glog/logging.h>

          |          ^~~~~~~~~~~~~~~~

    compilation terminated.

    test_performance_classification.cpp:17:10: fatal error: vitis/ai/benchmark.hpp: No such file or directory

       17 | #include <vitis/ai/benchmark.hpp>

          |          ^~~~~~~~~~~~~~~~~~~~~~~~

    compilation terminated.

    test_performance_classification_squeezenet.cpp:18:10: fatal error: vitis/ai/benchmark.hpp: No such file or directory

       18 | #include <vitis/ai/benchmark.hpp>

          |          ^~~~~~~~~~~~~~~~~~~~~~~~

    compilation terminated.

    test_video_classification.cpp:16:10: fatal error: glog/logging.h: No such file or directory

       16 | #include <glog/logging.h>

          |          ^~~~~~~~~~~~~~~~

    compilation terminated.

     

    Please help to take a look into it.

    Thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • quandv
    quandv over 5 years ago in reply to quandv

    The command dnf install packagegroup-petalinux-kv260-smartcam-dev didn't work with me, then I tried dnf install packagegroup-kv260-smartcam-dev. It's working.

    ./build.sh is also working.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • albertabeef
    albertabeef over 5 years ago in reply to quandv

    Quan,
    Thank you for the feedback.

    I had a typo in the instructions ... packagegroup-petalinux-kv260-smartcam-dev should have been packagegroup-kv260-smartcam-dev.

     

    Also, I had to install the following packages:
    dnf install libglog-dev

    dnf install libprotobuf-devdnf install packagegroup-petalinux-opencv-dev

     

    I have updated the blog instructions.

    Regards,

    Mario.