Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs led 10w
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 18 Jun 2012 6:29 AM Date Created
  • Views 458 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

led 10w

e14 Contributor
e14 Contributor
18 Jun 2012

As a major feature of intelligent lighting, in fact, wireless control as early as in 2005, has been applied to lighting control, but due to various bottlenecks and cost constraints, making it into the mainstream market until now. Wireless control of the biggest challenges is how to ensure the stability and accuracy of wireless transmission and reception, and automatically connect. Wired power line carrier (PLC) transmission, wireless transmission, need to continue to face the interference of various environmental factors.

The current mainstream wireless transmission standard Zigbee, Bluetooth and WiFi. Liang Jian-rong said that Bluetooth transmission distance is shorter, less transmission channel; WiFi power consumption and higher equipment costs; for the family in terms of only lighting, Zigbee more technical and cost advantages.

Wilbur D. led 1w wireless lighting solutions that popular Zigbee standard, developed in cooperation with TI's control network platform. Liang Jian, Rongjie Shao, after the R & D team of more than 10 people in Australia up to two years of specialized investment, Wilbur D. technologies has introduced a variety of led power 10w   lighting solutions to overcome the stability and accuracy of wireless transmission and reception issues, and China manufacturers to provide direct input from development to production of technical services.

Chinese manufacturers, wireless technology, a higher threshold, the general production engineers in debugging and application are also facing great difficulties. In this regard, said Liang Jian-rong, Wilbur D. led power 50w wireless lighting solution can provide services such as production testing, and specifically launched the called "PSWnetwork, the platform for ordinary engineers ready to solve various technical problems.

When the popularity of LED lighting?

As the nuclear power plant shut down, electricity, making Japan an accident to become a big market for the global LED home lighting is the first popular after the earthquake. And because the main reason of cost, when the High Power LED 50W lighting can be scaled up local popularity of the divergent views on a big mystery.

Liang Jian-rong detailed analysis of each quarter of the price of led 10w  lights are dropping, according to the current average rate of decline forecast for about 2-3 years when the cost of up to 0.7-1 times the price of ordinary lamps can fully spread to the people at home.