Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs LED 240W
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 15 Jun 2012 9:29 AM Date Created
  • Views 684 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

LED 240W

e14 Contributor
e14 Contributor
15 Jun 2012

With the trot to enhance the LED luminous efficiency and process, coupled with global carbon reduction, environmental consciousness, LED strip lights applications gradually branched out into the indoor lighting market, the prospect of high-profile, and is considered a new generation of light source to replace the traditional light source. LED as the light source of indoor lighting with energy-saving environmental protection, long life, resistance to vibration, low power consumption, small size, difficult to attenuation, suitable for low temperatures and light-emitting efficiency of a number of advantages, but the heat problem is that the impact of high power LED stepping into popularization of the bottleneck. The leader of the global cooling solutions built quasi-motor (SUNON) R & D LED indoor lighting cooling module, combined with the flexible design of the fan and module, declaring taken the high power led indoor lighting cooling module development a big step!

 

 

Ring design, innovation and a patent barrier to prevent hot air reflow

 

 

As a leader of the global cooling solutions built quasi-thermal bottleneck to realizing the LED light source used in indoor lighting, set up the LED cooling R & D team, with nearly three decades of rich experience in thermal processing, thermal design focus on the LED Blue 150W   interior lighting developed. The innovative design of the Sunon LED indoor and lighting bulb cooling modules, additional in the fan into the outlet of the module has a rectifier and the patent barrier ring (Blocking Ring) to increase the function of air velocity on the one hand you can quickly diversion hot air to bring out to prevent The hot air reflow bulb temperature, compared to the general barrier-free ring design in the lower temperature, lower 10 ° C in lower noise levels than the general design to reduce 17dBA.

 

Innovative two bi-directional fan running patent design to prevent dust deposition in extended lamp life

 

 

LED 200W interior light bulb installed in the location of the ceiling, very easy to siltation dust, efficiency and service life of light bulbs in order to overcome this problem, Sunon fan design, development leads the world in the two-way operation patented design. Import patented circuit design, control fans start running clockwise manner and the bulb on the dust disperse to avoid running into the cooling module and the light bulb and performance degradation due to dust adhesion in the space contact; clockwise a few seconds automatically into a reverse direction of the cooling function.

 

Innovative three quiet cooling design, build high-quality living environment

 

 

Applied to the indoor cooling solution, the operation when the requirements of no less than the thermal performance of the sound quality. In order to achieve the design goals of the best sound quality, LED interior lighting bulbs cooling module uses magnetic levitation motor fan (MagLev Motor Fan), emphasizing the balance of the fan sound quality and mute design, indoor environment required a quiet, comfortable and free from the realm of the interference, to create the best sound texture, the fundamental solution of the users of noise nuisance, and to show the quiet operation of antipyretic efficacy, LED 400W    indoor lighting products tend to be more humane and practical.