Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs LED 400W
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 23 Jul 2012 2:55 AM Date Created
  • Views 439 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

LED 400W

e14 Contributor
e14 Contributor
23 Jul 2012

The development of LED lighting technology, developed countries attach great importance to the study of the LED test methods and standards. Organizations such as the American National Standards the detection Institute (NIST), an internationally renowned testing experts to carry out the LED 200W test, focus on the LED light emitting characteristics, temperature characteristics and lumen characteristics, test methods, trying to establish the full set of LED test methods and technical standards in the LED test has been walking in the forefront of the world.

Characteristics of the semiconductor light-emitting diode (LED) because of its small size, directional emission of light, high brightness, the PN junction electrical characteristics, so many new problems in quality evaluation and testing methods. Different applications, determines the performance requirements of LED strip lights  products. From the optical properties of LEDs for display brightness, viewing angle, color and other parameters. LED for general lighting, pay more attention to the luminous flux, spatial distribution of the beam, the parameters of color, the color rendering properties, and biological applications of LED, it is even more concerned about the parameters of the biological effective radiated power, the effective irradiance. In addition, the light-emitting diode is both a light source, but also a power-type semiconductor devices, about its quality must be a comprehensive evaluation of many aspects of optical, electrical and thermal.

LED Floodlight 80W products from the point of view of the structure and the industrial development of LED products currently mainly need to consider several parameters of the optical properties, electrical properties, thermal properties, radiation safety and life.

Optical properties: the LED optical properties are mainly related to the performance requirements of the spectrum, brightness, and chroma. According to new industry standards set by the semiconductor light-emitting diode test method ", the main luminescence peak wavelength, spectral radiation bandwidth, axial luminous intensity, the beam angle of half intensity, luminous flux, radiant flux, luminous efficiency, chromaticity coordinates, color temperature, color purity and dominant wavelength and color rendering index and other parameters. The LED display with visual visual effects, so the relevant color temperature and

Color index is not a requirement, and white LED lighting, these two parameters is particularly important, it is an important indicator of lighting atmosphere and the effect, and the color purity and dominant wavelength generally does not require.

Electrical properties: the LED Blue 150W PN junction electrical characteristics, determines the electrical properties different from the traditional light source, LED lighting applications, one-way non-linear electrical properties, low-voltage drive, as well as static-sensitive features. The main measurement parameters include the forward drive current, forward voltage drop and reverse leakage current, reverse breakdown voltage and electrostatic sensitivity.

Thermal performance: lighting with LED luminous efficiency and power to improve one of the key issues in the development of LED 400W industry, at the same time, LED PN junction temperature and shell heat issues is particularly important, generally with thermal resistance, case temperature, said junction temperature and other parameters.