Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs LED aqaurium light-01
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 20 Aug 2011 1:55 AM Date Created
  • Views 612 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

LED aqaurium light-01

e14 Contributor
e14 Contributor
20 Aug 2011
First we need to clarify aquarium lighting, aquarium lighting describes any type of light that is used to illuminate an aquarium tank or in some instances, such as with reef aquariums, support the life contained within.
So Led Aquarium Lighting, as the name suggests, is a kind of aquarium lighting which use led as light sources.
See the picture to the left (90
W led aquarium lighting) as an example.
Led aquarium lightings are very common today. When they emerged, people preferred them for lunar lighting that can be implemented to come on at night, simulating the glow of the moon over the tank. Today, they seem to be their preference for the whole day aquarium lighting as an array of different colored LEDs can be used in combination to simulate spectral coverage that is suitable for marine life growth. The Cidly led aquarium lighting works of art that will nicely complement any coral, reef, live rock for the tank.
See the picture below (For Reef and live rock tank) as an example.
Cidly Led aquarium Lighting are normally using 10000-20000K bright white LEDs and 460nm blue in ratio. High output Lumen, high PAR value, long life span up to 50,000 hours, runs cool with low heat exhaust needed, easy installment, environmental friendly and wonderful working performance. The led aquarium light can focus the light to the bottom of the     tank with 30 degree view angle, and 60 degree is also optional. They save energy up to (50%-80%), much more efficient with high PAR reading and no UV radiation harm.
LED aquarium lights are the next generation in aquarium lighting , they are perfect replacement for traditional aquarium lights like: incandescent bulb, normal output fluorescent lighting, compact fluorescent lighting, high output T5 T8 bulbs, VHO fluorescent tubes, HO lamps or metal halide lighting(MH) etc.
 
http://www.cidly.com
 
miya
skype:cidly57
msn:wlm1113@hotmail.com
icq:629926901
Attachments: