Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs LED Blue 150W
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 25 May 2012 9:43 AM Date Created
  • Views 949 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

LED Blue 150W

e14 Contributor
e14 Contributor
25 May 2012

Fluorescent tubes have a wide range of applications, supermarkets, schools, office, city, subway, etc. in their daily lives, anything can appear with the public places, you can see the extensive use of the fluorescent How to make LED life and brightness reached to a satisfactory standard, a considerable significance of the topic! LED 400W  fluorescent lamp to maintain long life and high brightness problem to be solved are: power supply, LED light, heat, security, four key technologies.

A. Power supply

Power first and foremost requirement is a high efficiency, high-efficiency products, heat stability is bound to. Usually two options in the power supply section useful for isolation and non-isolated, isolated volume is too large, and less efficient in use, the installation will have a lot of problems, as non-isolated products in the market prospects, we mainly discussed in this non-isolated the driver program.

Two.high power led  light source

Taiwan sulfur Cummings patent structure of the LED light source, its chips placed on a pin, heat silver pin directly to the chip node tropical out, with the-line products, and traditional product placement in the heat qualitatively different from the chip junction temperature is not cumulative, in order to ensure good use of the light source lamp beads, to ensure the long life of the light source lamp beads, low light.

Traditional patch products, through the gold wire connection of the chip is negative, heat is also generated by the chip over gold wire to the silver feet, the conduction of heat and electricity conduction money long thermal accumulation time a direct impact on the life of the LED 200W tube.

3. Heat

Infrared radiation heat is introduced and applied to the fluorescent tube, is an important means to increase lamp life. In consideration of the heat, we will separate the heat of the LED strip lights  source lamp beads, cooling and power, without disturbing each other so as to ensure thermal reasonable.

There are three ways of heat conduction, convection, conduction and radiation. Achieve in a closed environment, convection and conduction is likely to be smaller, heat dissipation by radiation, is considered the focus of fluorescent tubes.

4. Security

Their safety security, this is mainly PC flame-retardant plastic tube, because the infrared heat can penetrate the PC pipe, we design considerations LED lights use can be considered more a physical plastic insulation, even in the use of non- The isolated power supply can absolutely guarantee the safety of use.

LED Blue 150W   lamp has a rather long time, from the energy-saving effect, the face of its future application is very broad, in addition to energy saving, safe, long-life use, we should be concerned!

Safety! Is the first element in the design of LED fluorescent, fluorescent lamp using a PC fire-retardant materials, address security issues, how to improve the life of the above proposed solution to the number of LED fluorescent tube manufacturers to provide more way of thinking!