Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs LED Frustrations
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: funinalaska
  • Date Created: 19 Sep 2014 7:34 PM Date Created
  • Views 497 views
  • Likes 0 likes
  • Comments 0 comments
  • fading
  • pwm
  • tlc5940
  • led
  • rgb
  • cycling
Related
Recommended

LED Frustrations

funinalaska
funinalaska
19 Sep 2014

Ok, so I had ordered a bunch of the 2 pin RGB auto fading LEDs for a lighting project I am trying to figure out.

I ordered these:

http://www.ebay.com/itm/271537207523?_trksid=p2059210.m2749.l2649&var=570366597205&ssPageName=STRK%3AMEBIDX%3AIT

in 5mm slow-fast fade.

(as a side note I also ordered some 5mm warm white and I really like those)

so the auto fading ones do have a reset in them.

what that means is when power is disconnected for ANY length of time it resets the fade color.

The ones I have tried all start with blue color.

What that means is that they are not PWM dimmable.

They simply stay in their start color and will not fade when dimmed.

 

I am slightly disappointed by this because I was hoping to use them with a few TLC5940 chips that I got as well,

But I have a mess of 595 shift registers I will use instead.

I will use the 5940 on those warm white LEDs instead.

 

I just wanted to put it out there in case any one else was hoping to use these and have them in a PWM circuit they will not work.

 

I also wanted to use them for a random look but because they reset when the power is disconnected they actually sync up pretty well, not exactly, but very close.

so I think what I am going to do is use them on independent channels and have them turn on at random intervals between 0 and 3000ms I think that will sufficiently randomize them.

 

I'll still make use of them. image