Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs led power 50w
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 7 Apr 2012 2:47 AM Date Created
  • Views 442 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

led power 50w

e14 Contributor
e14 Contributor
7 Apr 2012

In today's hottest LED Flood light 10W industry, energy saving has been as synonymous with new energy. With the development of society, LED industry to high-power LED product transition. High-power LED driver power supply selection (species) of the LED drive power is the correct selection of the normal operation of electronic control systems for machinery and equipment is essential. In select high-power LED driver power supply (power LED driver power of knowledge), we have to consider factors and points are multi-faceted. So, in the selection process of high-power LED driver power supply, we must take into account those aspects of it? Many people may not understand this. In view of this small series by collecting, collating information, a detailed summarized considerations and select the points on select high-power LED drive power.

 

 

The principle of selection of high-power LED driver power supply (high-power LED driver power supply optional)

 

 

First according to the type of machinery and equipment, the load torque characteristics, speed range, the static speed accuracy, the starting torque and the use of environmental requirements and then decide the most appropriate choice of what kind of control method and protective structure of high-power LED driver power. The so-called combination is the best value for money under the premise of the actual process of production to meet the mechanical equipment requirements and use the occasion to achieve high-power LED driver power supply applications.

 

 

Choice of high-power led power 50w  factor to be considered

 

 

Choice of speed when using high-power LED driver power required from the process requirements, efficiency savings, payback period and other aspects to consider, if only from the technological requirements, the savings are to consider the following situations choose the more favorable Frequency Control:

 

 

Frequency Control instead of the gate or baffle to adjust the flow suitable for fans, pumps, compressors, boilers, for example: pumps, blowers, induced draft fan to implement Frequency Control, which removes the servo amplifier, electric operation, electric actuator and the water supply valve (or wind deflector), and makes the whole boiler boiler control system has been a fast dynamic response and high control accuracy and stability.

 

 

According to process requirements, the production line or single equipment needs requirements by program or by adjusting the motor speed, such as: packaging machine conveyor system according to the different varieties of products, you need to change the system transmission speed, and frequency control enable the governor control system institutions simple, accurate control, and easy to implement process control.

 

 

Frequency Control to replace the mechanical speed. Such as: machine tools, not only eliminates the need for a complicated gearbox, but also to improve the racing to meet the requirements of process control.

 

 

Select points of high-power led driver 120w supply

 

 

The first point depending on the load characteristics, select the proper control of high power LED driver power

 

 

High-power LED driver type of power available on the market many are increasingly powerful, high-power LED driver power supply performance is increasingly becoming the merits of the decision factors of speed performance, in addition to high-power LED Spotlight 30Wsupply manufacturing process itself congenital "condition, the high-power LED driver power supply what kind of control is also very important. The following table summarizes the performance characteristics of the recent years, a variety of high-power LED driver power control mode.

 

 

In summary, the induction motor variable frequency control, selection of different control methods, you can get the governing characteristics of the different performance characteristics.

 

 

The second high-power LED driver power protection structure according to the selection of the installation environment

 

 

Protective structure of the high-power LED Floodlight 80W supply to adapt to their installation environment, we must consider the factors of temperature, humidity, dust, pH, corrosive gases, whether long-term with high-power LED driver power supply, safe and reliable operation of the relationship significant. It also depends on technological innovation and development.