Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs led spot lights
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 12 Jul 2012 5:57 AM Date Created
  • Views 614 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

led spot lights

e14 Contributor
e14 Contributor
12 Jul 2012

In the global fight against the greenhouse effect, the environmental craze, LED replacement light source development in leaps and bounds development, not only the continuation of the environmental protection of the LED light source, long life, small size advantages, coupled with the growing maturity of high-brightness, high power LED technology, but also LEDreplace the daily light availability increased dramatically, becoming the first choice for energy conservation, alternative light source of high energy consumption ...

led 1w  light source has a number of environmental advantages, but early products in the design of heat treatment and high brightness, there are still some technical bottlenecks could not break through, but under the continuous improvement of the LED chip manufacturing process, the existing lighting with the LED light output lumens more nearly in everyday lighting needs, coupled with the component design of the IC solid form, so that the LED light source designed to add more flexibility and advantages.

LED light source is not easy to damage the long life advantages, Excluding composition, compared to traditional high-energy tungsten (incandescent) / halogen / high pressure sodium, mercury pollution concerns CCFL fluorescent lamps led power 10w  performance is quite excellent new choice of alternative light source.

However, in order to different everyday lighting applications, also for the luminous efficiency of light-shaped, thermal design and the overall use of cost and number of applications continued to improve the design of LED products, LED lighting is more practical value, rather than just show the environmental demands of the decorations.

led 10w light source, differences in material properties of the component itself, coupled with the light-emitting principle is different from the traditional lighting, light shape if not addressed, and improved lighting quality For light LED to replace the general day-to-day applications, there are still a number of restrictions, CRI illumination shape, color lighting, power conversion efficiency ... key issues need to strengthen through the optical physical design of the chip manufacturing process improvements or fixtures to further meet the needs of the general lighting.

led power 50w   solid state lighting is still the problem of high cost

In the actual lighting applications market, High Power LED 50W  solid state lighting there are still high-priced, high-cost limit, and want to accelerate the popularity of LED lighting applications in a short time, and related businesses still have the cost of components, production technology, validation criteria ... project, one by one to improve cost efficiency.