Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs LED Spotlight 30W
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 7 Jun 2012 9:55 AM Date Created
  • Views 457 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

LED Spotlight 30W

e14 Contributor
e14 Contributor
7 Jun 2012

The manufacturers of most of the publicity is the LED Floodlight 80W  lamp life of 50,000 hours, the whole lamp life of 35,000 hours. Practical application to be influenced by many factors, not reach the theoretical value. With the non-stop progress of LED technology, the costs continue to decline, and continuously improve the performance of energy saving, LED is gradually from the initial stage toward in-depth stage of lighting applications, both in the international market and domestic market, the LED has begun to enter the commercial lighting or even the department home lighting market, showing a good momentum of development. Its long life, high efficiency, energy saving features have already been more and more attention and research, LED lights and other products have been increasingly wide range of applications.

led driver 120w lights also has some shortcomings, can detect in single LED lights and LED Power Supply   lamps, aging, or have some differences. This distinction can be LED lights use the environment as well as a variety of other parameters were analyzed, and how to effectively extend the service life of LED lamp with a problem worth talking about.

First, LED lights choice of quality is a very important factor. The quality of the product of different packaging technology will have a considerable impact. LED light package with a common underfill than the Class A bad glue package out of the LED lights in the same aging environment, the light fades by 76%. Therefore, the choice of LED lights, the production of good packaging technology will greatly extend its service life.

Secondly, LED Spotlight 30W beads in the work of the time, a single lamp beads heat is relatively small, bracket the temperature does not exceed 45 degrees this time of the life of the LED lights would be ideal, but when the LED lights light group, the corresponding temperature will rise, not conducive to the LED lamps for a long time use.

Here there are two solutions, the first lamp beads, separated by a distance larger lanterns, the best distance of more than 25MM, and the second is when the LED work best next to a small fan to help disperse heat. This will also extend its service life.

In short, is afraid of the heat, the higher the temperature, the shorter the LED life, the lower the temperature, the longer LED life. LED ideal working temperature is of course zero minus 5. But this is basically impossible. Consumers select the LED Flood light 10W   must be the performance of it to understand, to be reasonable protection when in use, in order to play its optimal use effects, add luster to it for you。