Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs LED Spotlight 45W
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 3 Aug 2012 8:33 AM Date Created
  • Views 474 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

LED Spotlight 45W

e14 Contributor
e14 Contributor
3 Aug 2012

LED is the abbreviation of the English light emittingdiode (light emitting diode), the basic structure of an electroluminescent semiconductor materials, placed on a wire rack, then sealed with epoxy, four weeks and play a role in the protection of the internal wire .

 

 

In addition, the LED light source has many advantages:

Voltage: led power 50w low-voltage power supply voltage between 6 ~ 24V, depending on the product, so it is safer than the use of high-voltage power supply power supply, particularly in public places.

Performance: the energy consumption reduced by 80% than the same luminous efficiency of incandescent lamps.

Applicability: small LED small piece of each unit is 3 ~ 5mm square, so the device can be fabricated into various shapes, and is suitable for variable environment.

Stability: 100,000 hours, the light fades to 50% of the initial.

Response time: the response of its incandescent asked for the nanosecond to millisecond response time of the LED Light.

Environmental pollution: harmful metallic mercury.

Color: change the current color, light-emitting diodes by chemical modification methods to adjust the band structure and band gap, orange red Huanglv Lan multicolor light-emitting materials. Such as low current red LEDs, with the increase of the current turn to orange, yellow, and finally to green.

led driver 120w is called the fourth generation of automotive lighting, LED lights, with good quality in addition to higher one-time investment grade higher incandescent incomparable advantages, and without delay, energy-saving, long life, low heat, earthquake, color purity, has become a tungsten halogen lamp is bound to replace the product.

n addition, the automotive LED Spotlight 30W  lamp jewelry is a fire at home and abroad car accessories, this is a new car decoration products, which combines the safety, practicality, decorative as one. The chassis of automotive LED lamps have a good waterproof performance and impact resistance, usually without maintenance, do not scrub, power is only equivalent to the power of a car headlight, not use excessive burden to the car battery and engine. Product is installed in the car at the bottom (or the vehicle's interior), in the night, fog, rain and poor visibility on the road, it can be good for pedestrians or 36 vehicles to provide your car driving or parking position identification to reduce accidents. Open LED Flood light 10W  lights in the evening, the car (or car interior) at the bottom showing a variety of color of a red, blue, green, very beautiful, very popular with the family of all ages of youth car.