Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Makevember : Wire Frame Christmas Trees
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 11 Nov 2019 12:01 PM Date Created
  • Views 3243 views
  • Likes 15 likes
  • Comments 19 comments
  • makevember
  • wire frame trees
Related
Recommended

Makevember : Wire Frame Christmas Trees

dubbie
dubbie
11 Nov 2019

For a contribution to the Makevember topic I decided to make some wire frame Christmas tree decorations. I wanted to make them to look good and to have some LEDs on them. I didn't quite (yet) manage this although I have made something, see below.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I aim to try and improve more on the wire frame trees and then I will have to work out some way of attaching LEDs and getting them to light up nicely.

 

Dubbie

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 6 years ago +7
    Hi Dubbie, I got curious and decided to run my own experiment with some 3.16 mm ( 1/8 inch ) aluminum ground wire that I had in the shop. Here is the initial shape of the wire: I put the wire in the vise…
  • fmilburn
    fmilburn over 6 years ago in reply to dubbie +5
    I have not tried it but have seen several times where people used a drill to straighten copper wire: https://www.youtube.com/watch?v=meZRMNF-6tQ. A good idea to have eye protection and gloves while doing…
  • jw0752
    jw0752 over 6 years ago in reply to fmilburn +5
    I do a lot on things with wire as a structural material. I usually put one end of the wire in a secured vise and the other end in a drill chuck. I pull the wire as tight as I can and give it about one…
Parents
  • fmilburn
    fmilburn over 6 years ago

    I may try something like this with the grandkids...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to fmilburn

    It is surprising difficult to get something that looks good. One of things that made a difference was stretching the wire before bending it as the straights were then much straighter. It was fairly difficult though as it is 2 mm Aluminium wire, which is relatively soft but difficult to stretch! I used a small pair of pin nose pliers to make the corners/bends which, with a bit of practice can be made quite good.

     

    I really wanted to get two wire tress exactly the same and then connect LEDs between them. The Aluminium wire seems to have a low resistance so should (might?) work. But I just cannot get two trees exactly the same.

     

    Dubbie

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to dubbie

    I have not tried it but have seen several times where people used a drill to straighten copper wire:  https://www.youtube.com/watch?v=meZRMNF-6tQ. A good idea to have eye protection and gloves while doing that in case it over stresses and snaps.  Copper is pretty ductile so not sure if aluminum would work as well.

     

    I like your idea of using a jig.  I wonder if instead of using nails if you had a hole in a block to thread it through and then bend it would hold the bend better.  You could 3D print the blocks or make them from wood.  Edit:  actually I think your wire is too stiff for this on second thought although there may be a way to do this by threading the blocks and then placing them over nails used as posts.  jw0752 is pretty good about things like this.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 6 years ago in reply to fmilburn

    I do a lot on things with wire as a structural material. I usually put one end of the wire in a secured vise and the other end in a drill chuck. I pull the wire as tight as I can and give it about one turn per meter. It amazingly makes the wire as straight as can be.

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to fmilburn

    Frank,

     

    I hadn't thought of putting the wire into a drill like this. I might give it a go, although I'm not sure that 2 mm Aluminium wire will twist nicely. It might also produce a nice surface twist finish.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago in reply to fmilburn

    Frank,

     

    I hadn't thought of putting the wire into a drill like this. I might give it a go, although I'm not sure that 2 mm Aluminium wire will twist nicely. It might also produce a nice surface twist finish.

     

    Dubbie