Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Micro DC Motors #1 : A Bit Too Small
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 11 Mar 2019 12:08 PM Date Created
  • Views 2301 views
  • Likes 10 likes
  • Comments 12 comments
  • dc motors
  • tinymobot
Related
Recommended

Micro DC Motors #1 : A Bit Too Small

dubbie
dubbie
11 Mar 2019

For my TinyMobot  project ( Tiny24hourMoBot #5 : Post Script - Making it even Tinier ) I have been looking for some smaller motors to replace the continuous rotation micro servo motors I currently use. I have ordered a selection of various types, including some small stepper motors and the first of these have arrived.

 

There are micro DC motors approximately 8 mm long and 4 mm in diameter. They are designed to be vibrators in mobile phones so come with an off-centre weight attached. I didn't really appreciate how small this is and I think they might be just too small for me to be able to use effectively, see video below

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

As indicated in the video to be useful the off-centre weight has to be removed which can be done using two sets of pliers, one to hold the motor body (after removing the black rubber shroud, by the rim near the shaft, and a second set of pliers to hold the off-centre weight. A short, sharp  'tug' between the two pliers will usually remove the off-centre weight. Unfortunately, if too much force is used or the grips are not quite correct, the connecting wires can be removed or the whole commutator comes off, see photograph below.

 

image

 

I used the best close-up shot I could get with my camera which has a closeup macro feature especially for taking photographs of PCBs and soldered joints and I still had a great deal of trouble getting a shot even remotely in focus. The parts are so small that the camera tends to focus on the background, so I have a nice in-focus shot of the 'smooth' surface of my desk. But if you look carefully you can just see the two commutator springs in the black round bit on the left, and the shaft of the armature inside the cylindrical casing on the right.

 

I hope that some of the other motors are a bit bigger and more suitable for my purpose.

 

Dubbie

  • Sign in to reply

Top Comments

  • danielw
    danielw over 7 years ago +6
    Nice write up. Good to know how robust or not they are! I've seen these type motors used before in the toy Micro RC cars where they are really geared down. I've also seen them on tiny line followers. I…
  • danielw
    danielw over 7 years ago +4
    I had a rummage when I got home tonight to find a link I'd written down some time ago when I was looking at beam robots. www.robotroom.com click on motors then scroll down to tiny motors. Lots of different…
  • shabaz
    shabaz over 7 years ago +4
    Hi Dubbie, Wow, interesting find. They are tiny! For larger motors there are 'pinion remover' tools, but perhaps they are not available for such a small size. The photo below shows the idea, the plate…
Parents
  • ntewinkel
    ntewinkel over 7 years ago

    Brilliant!

     

    I tip my tiny hat to you for even attempting to go that small !! image

     

    Next step: build your own tiny little gearbox to go with it. image

     

    -Nico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to ntewinkel

    Nico,

     

    Funny you should say that, I have been thinking of making a tiny gear box to match one of these motors, once

    I find one I like.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 7 years ago in reply to dubbie

    image image image

    I fear I may be a terrible influence image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 7 years ago in reply to dubbie

    image image image

    I fear I may be a terrible influence image

    • Cancel
    • Vote Up +3 Vote Down