Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Mini Arcade Consoles
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: korn
  • Date Created: 25 Sep 2018 4:18 PM Date Created
  • Views 1351 views
  • Likes 4 likes
  • Comments 9 comments
  • raspberri pi
  • retropie
  • portable arcade
Related
Recommended

Mini Arcade Consoles

korn
korn
25 Sep 2018

My son and I decided to update the Cigar Box Game Controller we made last year using some boxes from harbor freight.

image

First thing was the artwork. Not my job… Probably why it came out so nice…

image

Starting with a 1/8 drill bit then moving on to forstner bits.

image

image

image

image

image

The trick with the plexi is to use the 1/8 hole to center the big bit and only drill halfway through.

Then flip it over and complete the hole. That way you don’t chip the plexi when you break through.

I had these lighted joysticks lying around. only problem is they need 12V power. I will just add a small boost converter to keep it USB powered.

image

the boost converter got a little 3D printed sled to protect the wiring side.

image

I temporarily removed the mounting plate to use as a drilling template.

image

Not too bad looking.

image

 

image

Now for the guts.

image

In the cigar box controller I used an AtMega8 but this time I’m using PIC 18F2550 Microchip.

I used a usb feedthrough so I can use them as standard USB controllers with other consoles if I want.

image

image

image

image

image

Now for the RetroPi

I printed up a bunch of mounting hardware and bezels.

image

I re did the bezel with a collar to hide the edge of the cut. I made the cuts by hand with a Dremel.

image

image

image

Now to extend the HDMI and power…

image

image

image

turns out the threads on the power plug were long enough to make it through the box and felt padding so I didn’t use the square plate I made.

I did print a nice washer for the inside instead….

image

The washer is just visible here. Its cone shaped to get it through the felt easily.

image

image

I still might add a headphone jack on the right side. At the retro gamer nights we sometimes use a guitar amp…..

I did add a separator to make a compartment to carry all the cables. I might make a lid for that when I get a chance.

image

I added a fuse and 6.8V Zener to protect the Pi in case someone plugs in a laptop power brick by mistake…

image

I also added a WiFi / Bluetooth hat and some silica gel packets…..

image

Everything on the back sits well below the hinges and feet so you can still stand them up on their edge without crushing anything.

image

Best part is you can connect both controllers to one Pi and play 2 player games…

Add some Xbox  or PS2 controllers for even more players…

  • Sign in to reply

Top Comments

  • Problemchild
    Problemchild over 7 years ago +3
    Nice bit of Mechanical re-purposing there , it would be nice to see a video of them working with the Monitor and everything together
  • DAB
    DAB over 7 years ago +2
    Very nice build, DAB
  • mcb1
    mcb1 over 7 years ago +2
    Great build and description of the various parts. I like the ability to carry the cables, so that it forms a complete device. Well done Mark
Parents
  • 14rhb
    14rhb over 7 years ago

    Great work there Robert,

     

    You've made me Google "Cigar Box Case" to see what designs are available !

     

    Rod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • korn
    korn over 7 years ago in reply to 14rhb

    Cigar boxes are like the big brother to Altoids tins.

     

    My Local library had a bunch in a store room. They wanted to do a Cigar Box Guitar class but the woman realized power tools and teens was too much of a risk.

     

    I made the prototype CBC for them.

     

    Since then since I switched the code from Atmega 8 to 18F2550

     

    I did a USB Midi descriptor and made a garage band controller out of a cigar box too.

     

    Tempted to do a DMX-512 controller next. Or an analog Synth cigar box.

     

    The kids liked it but I shouldn't have brought the guitar amp and connected it to the Mac. They knew garageband too well and it got loud. Good thing we were in the basement.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • korn
    korn over 7 years ago in reply to 14rhb

    Cigar boxes are like the big brother to Altoids tins.

     

    My Local library had a bunch in a store room. They wanted to do a Cigar Box Guitar class but the woman realized power tools and teens was too much of a risk.

     

    I made the prototype CBC for them.

     

    Since then since I switched the code from Atmega 8 to 18F2550

     

    I did a USB Midi descriptor and made a garage band controller out of a cigar box too.

     

    Tempted to do a DMX-512 controller next. Or an analog Synth cigar box.

     

    The kids liked it but I shouldn't have brought the guitar amp and connected it to the Mac. They knew garageband too well and it got loud. Good thing we were in the basement.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • 14rhb
    14rhb over 7 years ago in reply to korn

    I don't seem to be able to find any cases like the ones you've used. I also added search terms like decal, artwork, aluminium and camera case.

     

    I'll keep looking.

     

    Rod

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • korn
    korn over 7 years ago in reply to 14rhb

    they're made by a company called voyager. I get that at harbor freight tools.

     

     

    https://www.harborfreight.com/11-12-x-7-12-x-4-12-aluminum-case-69316.html