Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs My first 3D printing model
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 11 Feb 2015 9:27 AM Date Created
  • Views 1389 views
  • Likes 2 likes
  • Comments 7 comments
Related
Recommended

My first 3D printing model

e14 Contributor
e14 Contributor
11 Feb 2015

I got a Geeetech 3d-printer, and printed my first object. Here is how it’s made from ABS filament, and a lot of details about the model.

 

Start

Create 3D objects in reality, sounds difficult and magical. In the past, only factories can do it. But now it’s simple and the method is easy to understand.

 

A 3D model is cut into pieces or layers in computer, each layer is thinner than 1mm. Printing a layer is easy, just like painting with melting plastic, and then other layers upon it. It gets thicker and thicker and becomes the model you want.

image

Grids

In fact, the model is not totally solid. As you can see grids in the model, especially in the middle(the edge is solid). I think the grid structure can save material, it’s lighter but also has required strength--solid doesn’t means strong all the time.

image

Notes

Neighbor layers should be adhere to each other, however sometimes they are separated, because of unsuitable temperature or layer number. Changing conditions of printing can get different effects. And the bottom layer can not be easilypaste on the glass board below it, so glue is needed, don’t forget clear it after print.

image

Views

Different views of the 3D model, it’s only 5cm tall but consist of more than 100 layers and spent more than 4 hours. Not so fast but i think it’s cheaper and more convenient, than any other ways to get this 3D model. By the way, I purchased the 3D-printer from Geeetech: http://www.geeetech.com/acrylic-geeetech-i3-pro-3d-printer-diy-kit-p-884.html

it’s suitable for beginners like me.


image


  • Sign in to reply
Parents
  • mcb1
    mcb1 over 11 years ago

    Very good ...especially for a first print.

     

    BTW your link has an extra comma on the end which sends you to 404 error.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 11 years ago

    Very good ...especially for a first print.

     

    BTW your link has an extra comma on the end which sends you to 404 error.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1

    It's weird. There was no comma ,as you see,  when I edited.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to e14 Contributor

    One of the mysteries or 1's and 0's ...

    It is still there.

    The bit you see and the underlying link can be different. (just like a web page)

     

    I suggest you delete it and re-do it making sure the link is correct

    image

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1

    Oh, it works. Thank you so muchimage