Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs my own avr devolopement programming board
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 8 Mar 2015 6:28 AM Date Created
  • Views 861 views
  • Likes 0 likes
  • Comments 5 comments
Related
Recommended

my own avr devolopement programming board

e14 Contributor
e14 Contributor
8 Mar 2015

hai every one...

i am new to element 14.. i am beginner to electronics.. i have a doubt ..

i started to design  my own avr devolopement programming board last week.. i soldered components  and followed the site-

www.robotplatform.com/howto/...board/atmega8_dev_board_3.html.. i connect  my board to 9v supply, the output to board should be 5v using a voltage regulator 7805.. but when i checked my voltage at board using multimeter it shows only 0.95volts... also my status led is also not glowing... i rechecked all the connections.. it was absolutely right... guys help me...

Attachments:
image
  • Sign in to reply

Top Comments

  • michaelwylie
    michaelwylie over 11 years ago +1
    You have the input and output caps on the regulator? It can be unstable without them.
Parents
  • kouruu
    kouruu over 11 years ago

    I'm by no means an expert, but I would check for a short between your voltage rails and ground during your soldering. The 7805 shouldn't get hot without hooking up a big load on the 5v out ( which is is caused by the excess voltage from your 9v supply dissipated through heat. ) A short would allow the electrons to flow freely and force a high amp pull. Your 7805 would get hot and/or battery depending on short, if this is the case. Electricity will always follow the path of least resistance so if a short exists, it's unlikely you will get a voltage supply to the circuit. Another possibility would be a bad 7805. (Just cause it's new, that don't mean it works.)

     

    One thing I forgot to mention, to see if you have a short, you can take a multimeter and set it to continuity. The meter will beep if you touch the leads together. touch them to you voltage rail and ground and if it beeps, you have a short. Also, on your 9v power supply I assumed you used a battery, but either it be a battery or power supply unit, check your in voltage and make sure it's giving you a DC 9V.

     

    If this doesn't help, hopefully someone with more experience than myself can assist you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kouruu
    kouruu over 11 years ago

    I'm by no means an expert, but I would check for a short between your voltage rails and ground during your soldering. The 7805 shouldn't get hot without hooking up a big load on the 5v out ( which is is caused by the excess voltage from your 9v supply dissipated through heat. ) A short would allow the electrons to flow freely and force a high amp pull. Your 7805 would get hot and/or battery depending on short, if this is the case. Electricity will always follow the path of least resistance so if a short exists, it's unlikely you will get a voltage supply to the circuit. Another possibility would be a bad 7805. (Just cause it's new, that don't mean it works.)

     

    One thing I forgot to mention, to see if you have a short, you can take a multimeter and set it to continuity. The meter will beep if you touch the leads together. touch them to you voltage rail and ground and if it beeps, you have a short. Also, on your 9v power supply I assumed you used a battery, but either it be a battery or power supply unit, check your in voltage and make sure it's giving you a DC 9V.

     

    If this doesn't help, hopefully someone with more experience than myself can assist you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to kouruu

    thanks chris for your reply.. i rechecked the circuit.. and  fixed the problem.. thanks friend...image