Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs New FETs with lower Rds_on (and another FET)
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wolfgangfriedrich
  • Date Created: 17 Aug 2020 10:01 PM Date Created
  • Views 416 views
  • Likes 3 likes
  • Comments 0 comments
  • power delivery
  • rds(on)
  • usb-c
  • r ds_on
  • usb pd
  • fet
Related
Recommended

New FETs with lower Rds_on (and another FET)

wolfgangfriedrich
wolfgangfriedrich
17 Aug 2020

Time passes...

I finished the design of Rev4 (and Rev3 in between) of my USB-C PD Sink. Most important improvements are a 2nd switch to select the current and new switching FETs . The new FETs have a Rds_on of only 9.5 mOhm (at Vsg = 4.5V), which cuts the dissipation almost in half and keeps the board cooler, even with 5 A current draw.

And I did a measurement with 24 boards, which showed the real Rds_on to be 7.1mOhm on average, because the Vsg is ~15V at the 20V setting. Also the calculated junction temperature is quite low and much more manageable now.

 

Results:

image

 

 

And then I found an even better FETs that has a Rds_on of only 9.5 mOhm (at Vsg = 10V), which is just as good as the previous one as Vsg >10 V at the output setting of 12V or more.

This FET is the Diodes DMP3013SFV. same 3.3mm x 3.3mm footprint.

Again I did a measurement with 19 boards, which showed to real Rds_on to be 7.3 mOhm on average, because the Vsg is ~15V at the 20V setting.