Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Newly developed 'metallic glue' could replace welding
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 14 Jan 2016 8:42 PM Date Created
  • Views 1069 views
  • Likes 2 likes
  • Comments 7 comments
  • circuits
  • welding
  • metal
  • soldering
Related
Recommended

Newly developed 'metallic glue' could replace welding

e14 Contributor
e14 Contributor
14 Jan 2016

Hello

Found this article interesting and wanted to share.

I feel if this product could be used in high temperature applications, is strong, conductive and all the awesome they will initially claim- then hey - it would be nice to see and/or test with it.

Have there been attempts in the past for similar products that perhaps failed? I don't recall any off-hand.

I could see many applications if this was to come to market and was not crazy expensive....

  -Vinnie              (thanks go to dave...)

Here is a link to the article as well as the article itself (not sure on posting rules on element14) sure I will find out if I did this incorrectly.  Anyway, wanted to get your thoughts on this.

Scientists invent 'metallic glue' that works at room temperature - UPI.com

 

BOSTON, Jan. 8 (UPI) -- Researchers at Northeastern University -- a professor and two PhD students -- have invented a new sealant capable of creating a metal bond. They're calling it "metallic glue."

The glue can be used at room temperature, and its activation doesn't require high pressure.

"It's like welding or soldering but without the heat," lead researcher Hanchen Huang, a professor of mechanical and industrial engineering, explained in a press release.

Huang and his students-turned-research partners created the metallic glue using metallic nanorods. The rods are tiny metallic cores coated on one side with indium and on the other with gallium. The nanorods are situated along a substrate like interlocking teeth.

When gallium teeth meet indium teeth, they become liquid. But the metal core quickly turns that liquid back into a solid, creating a metal bond capable of conducting heat and electricity.

Unlike standard glue, the metallic glue maintains its integrity at high temperatures and pressures. It also possesses superior conductivity and is less prone to air and gas leaks.

Huang and his colleagues say the glue could be used to attach a CPU to a circuit board or a filament to a light bulb. The material achieves bonds similar to those created via soldering or welding, but without the heat that can be dangerous to workers and potentially damage the product.

"The metallic glue has multiple applications, many of them in the electronics industry," Huang said. "As a heat conductor, it may replace the thermal grease currently being used, and as an electrical conductor, it may replace today's solders. Particular products include solar cells, pipe fittings, and components for computers and mobile devices."

Researchers described their new material -- which they've spun off into a startup company, MesoGlue -- in the journal Advanced Materials and Processes.

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 10 years ago +2
    It sounds like a typical Uni research paper hype - remember that these guys are judged on papers and the number of citations. Even if it works it sounds like a long way off and very expensive - I can see…
  • DAB
    DAB over 10 years ago +1
    I can see possibilities for creating a metallic goo, which would harden at room temperature so that you could 3D print metal objects. DAB
Parents
  • michaelkellett
    michaelkellett over 10 years ago

    It sounds like a typical Uni research paper hype - remember that these guys are judged on papers and the number of citations.

    Even if it works it sounds like a long way off and very expensive - I can see it being used in very exotic applications but not being mainstream inside 20 years.

     

    As far as repairs go - it might just mean different techniques - I'm sure my ultrasonic chisel will be on the market in time to remove the first mass production MesoGlued parts image

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelkellett

    Probably hit the nail on the head with this... if and when such a product was to be available for use, using in remote locations for repair or even new work (solder and weld)

     

    Houston - we have a problem... This darn hubble telescope is jacked again, that clown who attached this wire set it up for failure ... can't plug my soldering iron in...actually the sun melted all my solder.... hey use my glue Jim, got it at element14 shop....  (extreme I know but seriously the stuff could be real handy in a jam, if it comes into existence that is. )

     

    Hey MK, who is marketing your chisel, I am trying to get my gamma ray knife to market.....

     

    ugh- so glad its Friday.......image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelkellett

    Probably hit the nail on the head with this... if and when such a product was to be available for use, using in remote locations for repair or even new work (solder and weld)

     

    Houston - we have a problem... This darn hubble telescope is jacked again, that clown who attached this wire set it up for failure ... can't plug my soldering iron in...actually the sun melted all my solder.... hey use my glue Jim, got it at element14 shop....  (extreme I know but seriously the stuff could be real handy in a jam, if it comes into existence that is. )

     

    Hey MK, who is marketing your chisel, I am trying to get my gamma ray knife to market.....

     

    ugh- so glad its Friday.......image