Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs NVIDIA Jetson Nano
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jomoenginer
  • Date Created: 8 Apr 2019 5:07 PM Date Created
  • Views 4008 views
  • Likes 10 likes
  • Comments 12 comments
  • nvidia jetson nano
  • Single Board Computer
  • robotics
  • ROS
Related
Recommended

NVIDIA Jetson Nano

jomoenginer
jomoenginer
8 Apr 2019

I recently received the NVIDIA Jetson Nano Developers Kit I had ordered.

https://www.nvidia.com/en-us/autonomous-machines/embedded-systems/jetson-nano/

 

Now it's time to build a JetBot for running ROS.  Let the fun begin.

 

image

  • Sign in to reply

Top Comments

  • ipv1
    ipv1 over 7 years ago +4
    This one is on my to-do list. Ordering one from NVIDIA soon and looking forward to your experience.
  • shabaz
    shabaz over 7 years ago +3
    Looking forward to hearing how it goes. Did you order directly from NVIDIA? I made a mistake, ordering from seeed : ( they changed their delivery date on me despite 1:1 reassurance that it was an accurate…
  • jomoenginer
    jomoenginer over 7 years ago in reply to shabaz +3
    Yeah, I ordered directly from NVIDIA as soon as it was available.
  • jomoenginer
    jomoenginer over 7 years ago in reply to jomoenginer

    Since the Jetson Nano is really a SOM on top of a carrier board, perhaps the power statement seems to be associated with the carrier board.

     

    The boot issue was resolved by reflashing the uSD card with Etcher (I'm using Ubuntu 16.04.6 LTS) and then running GParted on the uSD device and letting it allocate the rest of the space on the card.  Initially, when plugging the uSD back in to my PC there were errors reported and after looking this up I found the solution with GParted.  Although, there is a statement of such in the dmesg message.

     

    This is what was seen before running GParted

    [ 3480.214799] usb-storage 2-4.4:1.0: USB Mass Storage device detected
    [ 3480.214986] scsi host7: usb-storage 2-4.4:1.0
    [ 3481.245848] scsi 7:0:0:0: Direct-Access Mass Storage Device 1.00 PQ: 0 ANSI: 0 CCS
    [ 3481.246297] sd 7:0:0:0: Attached scsi generic sg4 type 0
    [ 3481.496082] sd 7:0:0:0: [sdd] 62521344 512-byte logical blocks: (32.0 GB/29.8 GiB)
    [ 3481.496698] sd 7:0:0:0: [sdd] Write Protect is off
    [ 3481.496702] sd 7:0:0:0: [sdd] Mode Sense: 03 00 00 00
    [ 3481.497336] sd 7:0:0:0: [sdd] No Caching mode page found
    [ 3481.497342] sd 7:0:0:0: [sdd] Assuming drive cache: write through
    [ 3481.506470] GPT:Primary header thinks Alt. header is not at the end of the disk.
    [ 3481.506473] GPT:25165823 != 62521343
    [ 3481.506474] GPT:Alternate GPT header not at the end of the disk.
    [ 3481.506476] GPT:25165823 != 62521343
    [ 3481.506476] GPT: Use GNU Parted to correct GPT errors.
    [ 3481.506500] sdd: sdd1 sdd2 sdd3 sdd4 sdd5 sdd6 sdd7 sdd8 sdd9 sdd10 sdd11 sdd12

    And fddisk

    sudo fdisk /dev/sdd
    
    Welcome to fdisk (util-linux 2.27.1).
    Changes will remain in memory only, until you decide to write them.
    Be careful before using the write command.
    
    GPT PMBR size mismatch (25165823 != 62521343) will be corrected by w(rite).
    GPT PMBR size mismatch (25165823 != 62521343) will be corrected by w(rite).
    
    Command (m for help): q

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 7 years ago in reply to jomoenginer

    That seems like an odd way to spec power consumption.  Maybe to account for power regulators in the path?

     

    Please post how you resolve your problem as I’ll be getting one in a few weeks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to DAB

    I plan to cover this in future postings, however from the NVIDIA Jetson Nano User's Guide:

     

    The carrier board consumes between 0.5W (at 2A) and 1.25W (at 4A) with no peripherals attached

     

    There are two options to power the Jetson Nano:

    1. 5V 4A Switching Power supply to the carrier board barrel jack. (A jumper is required to turn off the USB power option)

    2. 5V 2.5 A USB power supply

     

    However, I have yet to get the board to fully power on with any of the multiple power supplies I have on hand.  All I get is the NVIDIA Splash Screen.  Others have posted something similar on the NVIDIA forums which now includes me as well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 7 years ago in reply to mp2100

    I was wondering about that as well. Shipping rates are a bit different too. Its cheaper from Seeed as opposed to US/Canada

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mp2100
    mp2100 over 7 years ago in reply to shabaz

    shabaz yes, I noticed that Seeed moved the shipping date all the way into May.  That's a shame.  image   Newegg also lists the nano, but no shipping date is given.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>