Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs OLED I2C Silkscreens are wrong, or are they?
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: baldengineer
  • Date Created: 6 Feb 2021 7:11 PM Date Created
  • Views 11994 views
  • Likes 10 likes
  • Comments 3 comments
  • oled
  • i2c
  • baldengineer
Related
Recommended

OLED I2C Silkscreens are wrong, or are they?

baldengineer
baldengineer
6 Feb 2021

image

One-inch OLED displays with an SSD1306 controller talk to microcontrollers over I2C. Several libraries are available that make interfacing to these modules straightforward. You need to provide a few pieces of information: the screen size and the I2C address. However, knowing that address is something that plagues 1" OLED modules--especially those bought from grey market suppliers.

 

Their Silk Screen is WRONG! These claim their I2C address is 0x78, when it is actually 0x3C. Or is it?

 

Side note. For information on decoding serial busses (and to see where I got the idea for this post), check out Workbench Wednesdays 34: Triggering And Decoding Serial Protocols On An Oscilloscope. I show how to decode UART and I2C with an oscilloscope.

 

I2C Addressing

I2C is a two-wire bus, sometimes called Two Wire Interface (TWI) to get around trademarks, that has a clock and data line. All devices on the bus share these two signals. For multiple devices to work, each needs a unique address. (Unique to the bus.)

 

7-bit vs. 8-bit Address

You might hear that I2C supports 7-bit or 8-bit addressing. The original specification for I2C was only 7-bit. An "8th bit" determines if the transaction is a read or write. So some manufacturers say their I2C device is 8-bit. When they are actually providing both the "read" and "write" addresses. (There are also 10-bit addressing methods, but I am ignoring those for this post.)

 

So how does this difference affect the 1" OLED? Well, take a look at the back of the one I have.

 

OLED Silk Screen Is Wrong?

On the back, there are two I2C addresses shown. 0x78 and 0x7A. Like many breakout modules, there are solder jumpers to change the device's address. This module has 0x78 selected. However, if I put that into some Arduino code, nothing happens.

 

#include <Wire.h>
#include "SSD1306Ascii.h"
#include "SSD1306AsciiWire.h"

#define I2C_ADDRESS 0x78

SSD1306AsciiWire oled;
//------------------------------------------------------------------------------
void setup() {
  Wire.begin();
  Wire.setClock(400000L);

  oled.begin(&Adafruit128x64, 0x3c);
  oled.setFont(Verdana12_bold);
  oled.println("element14");
  oled.println("Workbench");
  oled.println("Wednesdays");
  oled.println("@baldengineer");
  delay(100); 
}

 

image

 

You might notice, most example code for these modules use 0x3C or 0x3D as the default address. And if you use one of those, the screens work great.

 

image

 

What gives?

 

Let's look at the I2C addresses, using an image from i2c-bus.org.

 

image

Notice the data pattern's sequence. There is a start condition followed by the 7-bit address and one bit for a read or write.

 

Why is it wrong?!

Let's combine everything we know now.

  1. I2C addresses are only 7-bit (except for a special 10-bit case)
  2. One bit in the serial sequence determines if there is a read or write
  3. 0x78 does not work
  4. 0x3C does work!

 

We need to compare the two addresses in binary:

0x78 = 0111 1000  // does not work
0x3C = 0011 1100  // does work

 

Broken out as nibbles may not make it obvious. So here are the 8-bits as one word.

 

0x78 = 01111000  // does not work
0x3C = 00111100  // does work

Can you see it yet? If 0x3C gets shifted one bit to the left, it would be the same address as 0x78! At first, when I looked at these addresses, I thought maybe the PCB designer was confused by the SSD1306's addresses. Since 0 = write and 1 = read. Maybe they just added a 0 to the 7-bit address from the datasheet.

image

One datasheet I found on the SSD1306 seems to confirm this idea. Here it is showing the 7-bit address with the first nibble as "0111" and the second nibble as "10XX." Where XX is the control signals Data/!Command and Read/!Write. So there you are, "0111 1000" = "0x78."

 

Whoops.

 

So in a way, both 0x78 and 0x3C are the correct addresses for these OLED devices. It depends on whether you include the SSD's internal Read/!Write flag as part of the I2C address. (I don't.)

 

In fairness, there could be some microcontroller registers that operate with the "8-bit" address scheme, so the 0x78 address may work correctly. However,  I prefer to think in terms of the actual 7-bit address and let the software handle the read or write.

 

Related Workbench Wednesdays

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 


The idea for this post came from an episode of Workbench Wednesdays. You can get the show notes from here: Workbench Wednesdays 34: Triggering And Decoding Serial Protocols On An Oscilloscope.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago +7
    Consistency in i2c address specification is not-a-thing . In a datasheet, an indication may be if they give a different address for read and write (->the 8 bits address) or not (->7bits). What also not…
  • jc2048
    jc2048 over 5 years ago +5
    The confusion was baked into the original spec. On datasheets at that time, Philips used the byte format. Here's an example of a device with addresses 0x8A or 0x8E: When writing code, I always stored the…
  • kmikemoo
    kmikemoo over 5 years ago +4
    baldengineer Bit banging to an answer is always cool. Thanks for sharing it.
Parents
  • Jan Cumps
    Jan Cumps over 5 years ago

    Consistency in i2c address specification is not-a-thing image.

    In a datasheet, an indication may be if they give a different address for read and write (->the 8 bits address) or not (->7bits).

    What also not helps is that you look in example code and some HALs expect the 7-bit address, while others the distinct 8-bit read and write ones.

    No matter how careful you are, it'll bite you once so often ...

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 5 years ago

    Consistency in i2c address specification is not-a-thing image.

    In a datasheet, an indication may be if they give a different address for read and write (->the 8 bits address) or not (->7bits).

    What also not helps is that you look in example code and some HALs expect the 7-bit address, while others the distinct 8-bit read and write ones.

    No matter how careful you are, it'll bite you once so often ...

    • Cancel
    • Vote Up +7 Vote Down