Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs One Guy's Pursuit for the Perfect Hand: 39 Years and a 3D Printer
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 23 Feb 2015 4:20 PM Date Created
  • Views 548 views
  • Likes 0 likes
  • Comments 0 comments
  • printer
  • 3d
  • cheap
  • desktop
  • label_printer
  • thermal_printer
Related
Recommended

One Guy's Pursuit for the Perfect Hand: 39 Years and a 3D Printer

e14 Contributor
e14 Contributor
23 Feb 2015

Jose Delgado, Jr., suches as the reaction he's reaching his brand-new 3D-printed hand. "Wow," his employers at the storage facility claim. "Where did you get that?".

 

 

It's one of the most realistic prosthesis he's ever before had, though it took Delgado, 53, 5 decades to get below.

 

 

When he was a young adult, Delgado was often selected last for softball or baseball, although he as well as his brothers routinely played catch. "They really did not assume I could possibly hold a round or a bat," claimed Delgado, that was born without a left hand.

 

 

At the time, Delgado had a hook prosthesis that worked via rubber bands. The bands drew open the hook when he unbent his arm. Delgado spent most of his adult life using hook prosthetics, until 3 years ago when he obtained his very first myoelectric substitute.

 

 

The arm fits over his stump, and also sensors against the lower arm react to muscle activity to open up as well as close the prosthetic hand. Also this tool, which Delgado has worn for three years, has its constraints.

 

 

VIEW ALSO: 6 Imaginative Hacks for Your Smartphone.

 

 

Delgado, which resides in Elgin, Ill., clarifies that when he drives an automobile as well as attacks a bump, the myoelectric hand launches the steering wheel as well as "appears to do whatever it desires do to." Plus, "you have to allow it warm up on your muscular tissues, since if it's cool, it won't do anything for a few minutes.".

 

 

These disappointments finally drove Delgado to look online for a choice. The search led him initially to E-enabling the Future, a charitable consortium of about 700 tinkerers, researchers, occupational therapists and also innovators all committed to structure as well as refining 3D mechanical hands for those in requirement.

 

 

It was there Delgado acquired the very first glance of just what would later on become his own 3D hand, as well as where he found Jeremy Simon.

 

 

Simon, 39, is an entrepreneur who marketed his 15-year-old information protection company a few years earlier as well as introduced 3D printing blog site 3D Universe. As he began to work with 3D printing, Simon likewise went in search of 3D printing's awesome application, which led him to E-nabling and also its prosthesis job.

 

 

After they satisfied, both talked detailed concerning Delgado's hand, yet Simon was a bit distressed concerning printing and delivering a working 3D prosthesis. "I was a little nervous, but was groom front with him the first time: I had not had an opportunity to do this for an actual individual." In the past, Simon had actually printed and also built hands indicated for youngsters, yet other experts had actually managed the fitting process.

 

 

Simon took some dimensions, then started preparing to build the hand as well as print. Though Simon was making use of Jorge Zuniga's design, he did have to make certain that it would certainly be a good suitable for Delgado, which meant essentially scaling the whole model using computer to suit over Delgado's stump as well as forearm. Simon claims future styles will be much more fully adjustable.

 

 

Simon printed the pieces on his set of approximately $1,200 FlashForge Developer 3D laser printers, making use of ABS plastic. Printing took 14 hrs. Then Simon placed it together as well as waited for Delgado's return.

 

 

Gliding it onto his arm, Delgado located the shiny black plastic and cord 3D-printed hand a near excellent fit. Simon did a few on-the area adjustments, then, "He told me, 'Go ahead, take it for a week,'" recollects Delgado.

 

 

Instantly Delgado noticed exactly how light the 3D-printed hand is compared to the myoelectric version, and also just how very easy it is to work. "When I first placed it on [I thought], 'Wow, I can bend all 5 fingers,'" claims Delgado, which works the hand by flexing his wrist. A bend forward shuts the hand; unbending opens it up.

 

 

For the next few weeks, Delgado used the 3D-printed hand at home and at the workplace in the warehouse where he move boxes on and also off skids (or pallets). The hand, which can sustain between 20 and 30 pounds appears appropriate to the job. Delgado says the hand makes it a lot easier to grip boxes, partially because all the fingers curl in, similar to an actual hand, and also considering that the fingers have actually rubberized pointers.

 

 

Delgado at some point went back to Simon to contrast his myoelectric hand, which he still puts on sometimes when he requires a vice-like grip, and the 3D-printed hand. They made the video above.

 

 

In addition to the functional distinctions, there's the obvious price comparison. Delgado's myoelectric hand expense about $42,000. Simon's 3D-printed hand expense $50 for product (effort as well as style are not factored in). Delgado asked Simon just what he owed him for the hand. "He said, 'It's cost-free.'".

 

 

Just before they split ways, Simon provided Delgado some added products so he can change, claim, used rubber pads and even mend the hand if essential. For Simon, that's one of the lasting goals, to not just allow people, yet "enable them to do it on their own." When youngsters will certainly publish and also build their own prosthetic hands, he visualizes a time.

 

 

That sort of market disruption-- simple bucks rather than tens of countless bucks for life-altering technology-- is unlikely to fly under the radar, especially by the health care market. Delgado has not talked with his doctors concerning the 3D-printed hand, as well as Simon has actually never ever addressed any of the firms that make myoelectric items about his tasks. "That hammer hasn't boil down yet, but it's certainly going to get their attention," says Simon.

 

 

As for Delgado, he remains to use as well as make use of Simon's 3D printer hand as well as claims it's cooler compared to the hard-to-clean, artificial flesh-covered myoelectric one. The 3D-printed hand "acquires seen a whole lot, particularly by youngsters." Every person who sees the expressed, black-plastic hand, including his siblings and also siblings, like it.

 

 

After they fulfilled, the 2 talked extensive about Delgado's hand, but Simon was a bit nervous concerning printing and also providing a functioning 3D prosthesis. Delgado says the hand makes it a lot it's much easier to grasp boxes, partly since all the fingers crinkle in, much like a real hand, as well as because the fingers have actually rubberized suggestions.

 

 

Prior to they parted means, Simon gave Delgado some additional products so he could possibly change, claim, worn rubber pads or even repair the hand if needed. Delgado has not chatted to his doctors about the 3D-printed hand, as well as Simon has never spoken to any of the companies that make myoelectric devices concerning his tasks. As for Delgado, he proceeds to use as well as use Simon's 3D-printed hand as well as claims it's cooler compared to the hard-to-clean, phony flesh-covered myoelectric one.