Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Overview
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 2 Mar 2012 12:08 AM Date Created
  • Views 1820 views
  • Likes 1 like
  • Comments 14 comments
  • model_a
  • hardware
  • pcb_design
  • pcb_fabrication
  • raspberry_pi
  • model_b
Related
Recommended

Overview

e14 Contributor
e14 Contributor
2 Mar 2012

In this blog I hope to share with you some of the more interesting way points on the journey to designing the Raspberry Pi Hardware from the ideas kicking around 6 years ago to the overwhelming (for me and a few servers!) launch on Wednesday. 

 

I was lucky enough to be with element14 in Nuremberg when the RPi arrived from the UK for the noon on-stand launch.  Mike Powell from element14 deftly cabled the RPi, but gave me the 'honour' of powering it up. As many of you will know - it's a heart stopping moment (especially in front of a crowd of enthusiasts) until the kernel boot appears on the screen - it's either command line, terminal silence or smoke!

 

There is plenty of stuff on the Web about the Foundation and it's aims so I won't be repeating it here (unless asked).  There will be little discussion about software - we have lots of talented people in the team that can talk way more sensibly about that.  There is also an equally talented team on the hardware side and I hope I can encourage them to chip in with useful comment and correct me when I go off the rails.

 

I'm very happy to be sign posted to things that interest you - so let me know, and I'm sure they can be worked in somewhere.

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor +1
    coder27 - I'm not an expert on driving the Silicon but there is an 128kB L2 cache and by choosing the address range you can either use it or bypass it with the CPU. The GPU is really slated the main user…
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Pete,

    Could you explain how a SOC was selected that has no L2 cache for the CPU?  Can you recall any successful Linux computers without an L2 cache?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    coder27 -

     

    I'm not an expert on driving the Silicon but there is an 128kB L2 cache and by choosing the address range you can either use it or bypass it with the CPU.  The GPU is really slated the main user.

     

    There is some scant information in: http://www.raspberrypi.org/wp-content/uploads/2012/02/BCM2835-ARM-Peripherals.pdf

     

    At the end of the day a cache just makes things go quicker, although nowadays it is often also used to unpack/pack SDRAM burst reads / writes.  With the L1data and instruction cache and the improved branch predict over the Arm 9, I never really considered it to be an issue.

     

    Within the scope of our project the Silicon was chosen because of it's overall capability - especially in Multimedia and the richness of perhiperals and the low supporting cast of components - it was never intended to be a compute workhorse. We could have chosen something else (but check into Eben's day job).... nuff said.

     

    I would be interested to hear your comments

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I am presuming that the lack of L2 cache for the CPU is the main reason why a 700Mhz ARM performs only at the speed of a Pentium II 300.  I cannot imagine putting a Pentium II 300 class machine in front of a student to get them excited about programming.  A sluggish computer is no fun at all to use, although for embedded applications it may be fine.

     

    L2 cache is normally a no-brainer, since it doesn't increase the number of cpu pins, and it doesn't increase power usage.  In fact it saves power because it reduces memory bus traffic.  Intel tried eliminating the L2 cache on the original Celeron, which they soon realized was a major mistake, even for a low-cost entry-level cpu.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    @coder27: The amount and organisation of caches really depends on the goals set by the designers.  The BCM2835 was not designed as an all-out speed demon on the CPU front, hence the descriptions of "Videocore IV with ARM bolted on the side" in some Hardware FAQ.  That said, the datasheet that PeteL pointed to says "BCM2835 provides a 128KB system L2 cache, which is used primarily by the GPU. Accesses to memory are routed either via or around the L2 cache depending on senior two bits of the bus address."

     

    So, it sounds like you can use the L2 cache from the CPU in some circumstances... is it done in the RPi Linux build at the moment?  Not sure.  Bear in mind that the datasheet was written for engineers looking at the BCM2835's suitability for embedded use - in which case the GPU would be the main user of the L2 cache.  Also, remember that the only reason an L2 cache exists in a single core system is to reduce cache miss rates for less overall (cost/latency/hit to the maximum achievable CPU frequency) than enlarging the L1 cache.  In a perfect world where you didn't have to care about such mundanities, you would just choose the L1 cache size to fit your cache miss rate for your chosen workloads.

     

    I went looking for a boot log to see if there was a mention of how big the ARM's L1 cache was - the ARM1176 architecture manual only says that L1 is between 4KB and 64KB in size - the decision is left to the licensee as to how much chip area they want to spend on the cache.  I couldn't find anything in the only dmesg output (from Paul Maunders' beta board).

     

    In any case, what are you worried about being slow in particular?  The GUI?  The boot time?  The actual programming environment?  It's got about as much memory and CPU performance as the machine I used as a staff member of a university Computer Science department in 2001... and I seem to remember being able to write a few programs with that.  Boot times can be tuned, simpler GUIs favoured, and lightweight IDEs chosen.  It's for schoolkids after all... they don't need Eclipse to write programs a few pages long; back when I was at secondary college, we thought that Turbo Pascal running on a 640KB PC was usable for what we were asked to do.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    I'll put my old academia hat on and agree with Jason that speed is not a major concern in education, which is the motivating force for Rpi.  The CPU just needs to be "fast enough" to keep it highly responsive so that interactive development is not bogged down.

     

    Of course it's always nice to have more speed, but I think we'll have to wait for Rpi Next Gen for that.  The BCM2835's ARM11 is inherently slower than a modern Cortex-A series, so it's not the best choice of ARM core for speed merchants --- but then, that was never a requirement in this design.

     

    The other ARM licensees are probably very dismayed at Broadcom's massive PR coup with Raspberry Pi, but they have ample opportunity to compete:  make a similar board within the $25-$35 price bracket but based on a more modern core.  And if ARM Holdings needs some major pummeling to lower Cortex licensing fees if they're too high for this niche (as the BeagleBone price suggests), so be it. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    I'll put my old academia hat on and agree with Jason that speed is not a major concern in education, which is the motivating force for Rpi.  The CPU just needs to be "fast enough" to keep it highly responsive so that interactive development is not bogged down.

     

    Of course it's always nice to have more speed, but I think we'll have to wait for Rpi Next Gen for that.  The BCM2835's ARM11 is inherently slower than a modern Cortex-A series, so it's not the best choice of ARM core for speed merchants --- but then, that was never a requirement in this design.

     

    The other ARM licensees are probably very dismayed at Broadcom's massive PR coup with Raspberry Pi, but they have ample opportunity to compete:  make a similar board within the $25-$35 price bracket but based on a more modern core.  And if ARM Holdings needs some major pummeling to lower Cortex licensing fees if they're too high for this niche (as the BeagleBone price suggests), so be it. image