Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Plaster Cast - Twitter Controlled Christmas Tree Lights
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: drlucyrogers
  • Date Created: 5 Dec 2015 5:56 PM Date Created
  • Views 3677 views
  • Likes 1 like
  • Comments 6 comments
  • cheerlights
  • drlucyrogers
  • adafruit_flora
  • neopixels
  • james_macfarlane
  • @andysc
  • twitter
  • andy_stanford-clark
  • Wearables
  • adafruit_bluefruit
  • adafruit
  • @drlucyrogers
  • @rocketengines
  • arduino
  • lucy_rogers
Related
Recommended

Plaster Cast - Twitter Controlled Christmas Tree Lights

drlucyrogers
drlucyrogers
5 Dec 2015

After breaking my wrist and decorating my cast as a Buzz Lightyear Cuff using sugru and 3doodler (Blog here), I needed further surgery and a new cast.

image

 

Seems my first step is always eyes ...

image

But it was December. And cheerlights

were beginning to flash across my twitter stream.

 

A tweet controlled Christmas Tree with lights was required.

 

I bought an Adafruit Flora, Bluefruit and Neopixels.

 

I sketched the design on my cast.

image

 

I transfered the design onto carboard ...

image

 

And stuck the neopixels on with bluetak

 

image

 

image

 

 

Although the neopixels are sewable, as it was going onto a solid cast, I soldered the wires - which also made the shape of the tree and tinsel.

A lithium Ion polymer battery (3.7V 1200mAh) powered the components.


 

imageimage

Using evostick contact adhesive, I stuck the soft and fluffy side of velcro to my cast (I thank myself for this at night!) and the prickly side to the components.

image

The adafruit flora coding was done by the amazing James Macfarlane and is on github here

 

The Bluefruit connected to my phone via bluetooth using the adafruit app Bluefruit LE.

 

If there is no bluetooth connection or no input for a while, the lights change randomly.

 

Using the UART connection, the code also allows for the UART feed to type in a colour.

image

By connecting the MQTT feed to the cheerlights topic from Andy Stanford-Clark's MQTT feed (mqtt://iot.eclipse.org with the topic cheerlights) the lights respond to tweets (Tweet #cheerlights and a colour).

image

 

(This works on android and iphone, but not on ipad1 and the mac app does not have the MQTT feed).

 

The colour picker from controller also works.

 

image

image

 

 

 

image

 

The first outing for my lights was to the Thingmonk conference

 

image

 

Where I and other delegates had a lot of fun!

image

image

image

  • Sign in to reply

Top Comments

  • zengirl2
    zengirl2 over 10 years ago +2
    I just saw this post! OMG, I'm so glad you did this because I found that code about a month ago and so wanted to try it. I think your explanation of it makes it easier to understand, too. The cool thing…
  • DAB
    DAB over 10 years ago +1
    Good post, I guess if you have to wear a cast, adding lights is a good way to have fun with it. I hope you get better and back to making soon, DAB
  • cbinrva
    cbinrva over 10 years ago +1
    Novel idea and interesting way to implement it!
Parents
  • cstanton
    cstanton over 10 years ago

    Could do with perhaps another layer, which helps to hide the wiring and such but brings out the LEDs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • cstanton
    cstanton over 10 years ago

    Could do with perhaps another layer, which helps to hide the wiring and such but brings out the LEDs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • drlucyrogers
    drlucyrogers over 10 years ago in reply to cstanton

    Without the wires, how would you know it's a Christmas tree? I have now turned down the brightness of the neopixels, so not everyone gets blinded!