Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Project case construction
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: billabott
  • Date Created: 15 Jul 2013 12:11 AM Date Created
  • Views 1432 views
  • Likes 0 likes
  • Comments 4 comments
Related
Recommended

Project case construction

billabott
billabott
15 Jul 2013

Having purchased some of these DC POWER JACK 2.1MM ENCLOSED FRAME WITH SWITCH, I began to wonder how am I going to create the proper precise opening to insert and secure it to.

 

image

Will someone point me in the right direction and the right terminology to find a punch that will "Make:" this hole?

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 13 years ago +1
    Hi William, You've got the right terminology I think. There are punches and dies available in various common shapes, but they cost ($100 or more - as an example, this one is for D-type connectors ) and…
  • billabott
    billabott over 13 years ago in reply to shabaz +1
    I recalled that in a fairly good book I read, the author made a big deal about sources of tools from a web site called www.mcmaster.com . The book is "Making Things Move DIY Mechanisms for Inventors, Hobbyists…
Parents
  • shabaz
    shabaz over 13 years ago

    Hi William,

    You've got the right terminology I think. There are punches and dies available in various common shapes, but they cost ($100 or more - as an example, this one is for D-type connectors) and require a press machine (could be a manual press or powered). There used to be tools where you would drill a smaller hole, and then screw the punch and die together through it, but I've not seen them for quite a while, and I don't know if they were ever available for small overall diameters. It is a pain to do it with no tool - I don't have one, and I have to drill about half a dozen holes for BNC connectors which have one flat side, and I'm not looking forward to it for the same reason. I'm planning on drilling a smaller hole and then using needle files - not ideal, but possibly the only way to do it at low cost - but it will take ages.

    Some would suggest to drill just a bigger round hole and squeeze in some epoxy resin glue to hold it in place permanently - really not nice, but I have done it sometimes :-(

    I'm always on the lookout for low cost metalwork tools - if I spot anywhere offering low cost punch and die tools, I'll paste it here!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • billabott
    billabott over 13 years ago in reply to shabaz

    I recalled that in a fairly good book I read, the author made a big deal about sources of tools from a web site called www.mcmaster.com.  The book is "Making Things Move DIY Mechanisms for Inventors, Hobbyists, and Artists" by Dustyn Roberts.

     

    They call that punch style a Double-D but they don't do small (or inexpensive) and they don't do metric sizes.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to billabott

    I just had a look on Amazon, it looks like a useful book.

    Another method would be to use a milling machine of course, but that is an even more expensive up-front cost :-(

    The mcmaster site looks extremely good. It's a useful reference to browse what kind of tools and components are possible. I also use this site to see what kinds of metalwork tools there are - this site has some semi-affordable items for individuals unlike some other sites in the UK.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 13 years ago in reply to billabott

    I just had a look on Amazon, it looks like a useful book.

    Another method would be to use a milling machine of course, but that is an even more expensive up-front cost :-(

    The mcmaster site looks extremely good. It's a useful reference to browse what kind of tools and components are possible. I also use this site to see what kinds of metalwork tools there are - this site has some semi-affordable items for individuals unlike some other sites in the UK.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 13 years ago in reply to shabaz

    William

    If you only have a few to do, two holes and a file.

    You probably only need one flat to stop it spinning.

     

    We once had a very clever guy at work make a punch for the D type connectors, it was tha same as the manual punches with a large 1/2 inch (12mm) and a locating hole.

    We used a Grade 10 Cap screw, plenty of lube and a sacrifical washer, or a thrust washer, and used thin cases.

     

     

    mark