Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Raspberry Pi OS - Fedora 16 (Choice subject to change)
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: macfan9000
  • Date Created: 11 Apr 2012 7:07 AM Date Created
  • Views 915 views
  • Likes 0 likes
  • Comments 4 comments
  • samsung
  • workstation
  • element14
  • fedora_16
  • junior
  • hdmi
  • programming
  • raspberry_pi
  • starter
  • component
  • os
  • system
  • tux
  • operating
  • linux
  • macfan9000
Related
Recommended

Raspberry Pi OS - Fedora 16 (Choice subject to change)

macfan9000
macfan9000
11 Apr 2012

It's finally ready: I now have a ready SDHC card for when my Raspberry Pi comes in! My Operating System of choice: Fedora 16.image

 

I know I know, a 650+ mb file on a 4GB SDHC card is preposterous. Hear me out on this I promise!

Whenever my Pi (Is that the politically correct abreviation for it?) comes in, I'm going to implement it as more of a Network Monitoring + basic programming. I'm trying to also figure out if I want to connect it to our 46" VIA HDMI (Which would be AMAZING), or get a dedicated monitor and have a separate workstation for it. I wouldn't mind having a separate workstation for it, so when I get my own place (I'm a college kid who still lives at home, I'm only 21. Cut me some slack haters!) I can organize my workstations throughout my future place.

 

I'll let you all decide: Dedicated workstation or 46" and deal with an external for when I move out? Let me know your thoughts in the comments!

 

I think linux was the best choice for my workflow, because I like to do things on a deep OS level , rather than a fancy GUI (which is always convenient). Plus I'll be able to sharpen my Linux knowledge a little better. The Raspberry Pi is still backordered unfortunately, but they're making GREAT progress none the less! I have faith in the team that they are working around the clock to get their orders out. In my opinion: $35 well spent (not a typo, Model B board is $35 USD, Model A is expected to be $25).

 

 

Peace out Y'all!

 

 

 

 

 

- Junior

  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    I didn't think there was a Fedora 16 for Raspberry Pi - Seneca College did a Fedora 14 Remix, but was a bit buggy, Debian Squeeze 17 is the current best choice but with an improved Debian release imminent according to JamesH, one of the programmers.  You do need something specifically tailored for the RPi's unusual hardware, though, in particular its somewhat exotic boot sequence - going off to Fedora's homepage and dropping their Fedora 16 ISO onto an SD card will not work at all on the RPi, I'm afraid.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 14 years ago

    I didn't think there was a Fedora 16 for Raspberry Pi - Seneca College did a Fedora 14 Remix, but was a bit buggy, Debian Squeeze 17 is the current best choice but with an improved Debian release imminent according to JamesH, one of the programmers.  You do need something specifically tailored for the RPi's unusual hardware, though, in particular its somewhat exotic boot sequence - going off to Fedora's homepage and dropping their Fedora 16 ISO onto an SD card will not work at all on the RPi, I'm afraid.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • macfan9000
    macfan9000 over 14 years ago in reply to e14 Contributor

    There isn't one specifically made for the Raspberry Pi image Oh bugger, Yeah that can cause complications in the long run. I did have a small chance to talk with the team (before when I'd test the .img I'd download from their website) I would get just a flashing cursor on my screen. They said "yep. That's because those images will NOT work on your PC. Only on your Pi". With all that being said and done, it looks like I'm not quite done with my project here. I'll just re-load one of their images and wait ever so patiently for my Pi to come in. That'll be the moment of truth it seems like.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to macfan9000

    Yes, the images which are specifically made for the RPi are the ones hosted on their site - http://www.raspberrypi.org/downloads - Fedora don't host it at their own page because they didn't create it.  To get these images onto an SD card, follow instructions on the Wiki at http://elinux.org/RPi_Easy_SD_Card_Setup - which includes Mac instructions, although I did something very slightly different when I used my Mac to get the image onto SD -http://www.raspberrypi.org/forum/distributions/fedora-arm-on-raspberry-pi/page-10#p50341 - and, the resulting SD card will only work on the RPi and won't boot a PC.  The most stable one to use at the moment in Debian.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • macfan9000
    macfan9000 over 14 years ago in reply to e14 Contributor

    Great resources there! Thanks image Yeah, I've been using my Windows XP Netbook to set it up over my iMac. After the Raspberry Pi team and I both realized my screwup, looks like I'm not done, LOL. I'd like to use their recommended one (I believe it's a fedora remix) , I'll re-load it on there and see what shakes loose when my board comes in. They say they're hoping to begin shipment next week!