Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Raspberry Pi Zero Cluster A.I Drone
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shadow999911
  • Date Created: 15 Jan 2017 9:58 AM Date Created
  • Views 715 views
  • Likes 0 likes
  • Comments 2 comments
Related
Recommended

Raspberry Pi Zero Cluster A.I Drone

shadow999911
shadow999911
15 Jan 2017

Could someone do this. Let say build a raspberry pi zero 10-node cluster for the (A.I) then take another raspberry pi zero then enable ssh so the (A.I) could control the drone then ssh wireless. then you could put a mic, cam on the pi I don't have the money to do this or I would try to do this but that's why i'm asking so if anyone can do it I would like to see it. If someone has done this can some one point me that way.

  • Sign in to reply
  • shadow999911
    shadow999911 over 9 years ago in reply to clem57

    because of this https://www.youtube.com/watch?v=RqcHj1DgAMM its a hat for a raspberry pi. so then you could have the head of the cluster a raspberry pi 3

    then the rest as pi zeros 4 of them for a total of 5 so if the specs of the raspberry pi 3 b is

    • 1.2GHz QUAD Core Broadcom BCM2837 64bit ARMv8 processor
    • BCM43438 WiFi on board
    • Bluetooth Low Energy (BLE) on board
    • 1GB RAM
    • 4x USB 2 ports
    • 40pin extended GPIO
    • HDMI and RCA video output

    the raspberry pi zero specs

    • 1Ghz, Single-core CPU
    • 512MB RAM
    • Mini HDMI and USB On-The-Go ports
    • Micro USB power
    • HAT-compatible 40-pin header
    • Composite video and reset headers
    • CSI camera connector (v1.2 only)

    The more i get look it would be better for there to only be one pi zero for the drone because with the four pi zeros it only adds about 2g ram and then 4Ghz of cpu but if you use 5  (Pi 3 B) you get 5Gb of ram then 6GHz of quad core.

    Thank you for asking that

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 9 years ago

    Why Raspberry Pi Zero???