Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Reading in a 0V - 5V Analogue voltage on the PSOC 4 Pioneer board
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 15 Nov 2013 10:50 AM Date Created
  • Views 1653 views
  • Likes 0 likes
  • Comments 1 comment
  • pioneer
  • pioneer_kit
  • psoc4
  • psoc
Related
Recommended

Reading in a 0V - 5V Analogue voltage on the PSOC 4 Pioneer board

e14 Contributor
e14 Contributor
15 Nov 2013

This confused me for a bit so if the following helps anyone then great.

 

Here is my circuit diagram..

C0YVPZT.png

 

The problem I was having was assuming that using a single ended ADC input at 12 bits was going to give me 0 for 0V and 4096 for 5V.

However the reality is different, if you look at the ADC data sheet on page 8 it says that the maximum value you can get from a single

ended input is 11 bits.

 

So the maximum you can get is 2047, the output is always signed.

 

Here is my ADC config

yDOb3TP.png

 

The other thing you need to watch out for is what voltage is the board powered by. You will need to change jumper J9 into 5V, it comes 3.3V as default.

Also you need to change the system tab in the .cydwr file to 5V VDDA or the calculations will come out wrong, this is set to 3.3V default too.

6kt0IOH.png

 

I am using a potentiometer on the input but if you want to quickly test if it is working you could just wire directly from the ADC pin to the 5V, 3.3V and 0V supplies

on the board like so..

3ga1EuS.jpg

 

Here is my source code.. (it is all included in the project below)

KrEhBHX.png

 

Incase it helps anyone this is the thread I opened on the Cypress forums asking for help, it explains all the problems I ran into there..

https://secure.cypress.com/?app=forum&id=4749&rID=88221

 

I have attached my project so you can use it too.

Attachments:
5V ADC Measurement.Bundle01.zip
  • Sign in to reply
  • DAB
    DAB over 13 years ago

    Good post.

     

    It always pays to check the fine print on the defaults.

    Like you, I would have assumed that the 12 Bits were 0 to 5v.

     

    Thanks,

    DAB