Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Relays, types and applications
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: theo_san
  • Date Created: 28 Nov 2017 9:27 AM Date Created
  • Views 929 views
  • Likes 1 like
  • Comments 1 comment
  • relay test equipment
  • relay test
  • relay
Related
Recommended

Relays, types and applications

theo_san
theo_san
28 Nov 2017

In this first entry in my blog I'm going to talk to you about the relays. A relay is a switch controlled by current remote control, the magnetism, or the temperature. Relay is a component common in many devices and there are many different types of relays.

 

 

Types of Relays:

The two main types of relays are electromechanical and state solid.  The relays use an electromagnet to move a series of contacts The contacts are attracted to the electromagnet, while that the current that flows to the contacts that are connected to a spring that pushes them up when the current stops flow. An interlocking relay acts as a two-pole switch in the contacts that remain in position when the current one stops flow. This is achieved by means of a solenoid to move a ratchet and the cam or by an electromagnet on both sides.

 

They have a set of ferro alloys and metal contacts inside of a glass tube. Close contacts is when in a field External magnetic is applied and reopening is eliminated. The relays are used as door sensors for the systems of alarm.

 

Overload relays are similar to the relays of cane, but use a bimetallic strip to move the contacts. At high temperature does that the double strip with the set of contacts.

 

 

Relay applications

Relays are used to control the flow of large currents with a small current. In the past they were widely used in telephone exchanges to pass calls, but in large part They have been replaced by digital equipment. They are used to change the motors and to protect them from overheating. It is to be noted that also the thermostats use an overload relay to turn off the current when the temperature rises above the required.

 

This is why it is very important to test all generations and types of protection relays. To avoid major problems! If someone wants to contribute their knowledge about relays or relay test equipment I will be happy to read it and respond it.

  • Sign in to reply
  • jw0752
    jw0752 over 8 years ago

    Hi Theo,

     

    Welcome to the forum and thank you for your post about relays. I have always liked relays and unfortunately I have continued to use them in some of my builds even though there is currently better technology in many cases. For me a relay has a much narrower definition than what you are using in your post. Many of the devices that you are calling relays I would call switches. For example the devices that use a bimetalic strip are thermal switches under my understanding of what is a relay and the magnetic reed devices are switches under the same definition. Even the devices that are commonly called solid state relays are borderline as they are more appropriately a switching circuit. To me a relay is a set of mechanical contacts that can be actuated by the mechanical movement of a piece of metal reacting to an electro magnetic field. It might be interesting for someone to create a poll to investigate where other engineers on the forum draw the line between what they consider a relay and what they consider a switch. This may seem trivial but in fact it is very important. If we can not agree on the definition of the word we use (like what is a relay) then we can not really communicate. I look forward to your insights and future posts.

     

    John