Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Retro Raspberry  Pi case with a real classic feel!
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 16 Mar 2014 7:23 AM Date Created
  • Views 2136 views
  • Likes 3 likes
  • Comments 1 comment
  • raspberry
  • commodore
  • keyboard
  • hack
  • vintage
  • pi
  • emulation
  • atari
  • ti
Related
Recommended

Retro Raspberry  Pi case with a real classic feel!

e14 Contributor
e14 Contributor
16 Mar 2014

I Have actually been working on this project for a couple months now but I had set Pi day as my target finish date. I just barely got It done. I thought I would like to show it off, offer this as a tutorial, or just offer it up for some inspiration. This I my brand new all purpose vintage computer emulation device with a real classic look!
BEFORE
Image
AFTER
Image
Image
Image
I am very interested in vintage computing and my goal is to make this a multi computer emulation machine with kind of a classic feel. I had stumbled upon an old Ultratec teletype machine for $1.50 at a thrift store. I thought it would make a sweet little Raspberry Pi case, but there were a lot of little issues that I had too work around.
Most of these issues revolved around the keyboard. It lacks important keys, and there is no way to hook it up to the Pi. I came up with a very time consuming work around. I first took a dremel and literally hacked off the back half of the teletypes main board.
Image
Image
The wires you see at this point were just test leads. I then had to take a dremel bit and cut all of the circuit traces connecting the keyboard keys on both sides of the board.
Image
On the outside of the teletype I used the area that housed the teletype screen to create a button panel out of tactile switches. There are 20 switches. Now on the Pi I plan to map each one of these keys with alternate shift functions. This will give me 40 more keys to play with. This solved the problem with the missing keys.
I bought a cheap usb keyboard and removed the circuit board.
Image
I removed the two plastic sheets with the keyboards key matrix printed on them. I used fine point sharpies to map the key map connections of the usb keyboard.
Image
I made lots of charts and lists of the connections.
Image
Using this I rewired the teletype key board and my key panel into the usb key board circuit.
Image
This required massive amounts of soldering and wire connections. I also included a wire harness between my own key panel so that I can disconnect it in need be.
Image
Every key is wired to the key that it corresponds with on the usb keyboard. This solved the problem of connecting it to the I will however still have to make a few adjustments using xmodmap.
Image
I bought a powered usb hub and removed most of the usb ports. I carefully cut holes for usb ports on the back of the teletype.
Image
I glued them into place with some JB weld and used wires to connect them back to the hub. I then connected the power for the usb hub to the barrel connector that was there for the teletype's power. I used original power switch of the teletype to turn my usb hub on and off. I also have my Raspberry Pi powered with the hub so the switch turns everything on and off. I bought a 6" hdmi extension cable and mounted it where the phone connections used to be on the teletype.
Image
The teletype I used had a battery compartment on the bottom.
Image
I removed the battery holder. I cut a slit in one of the walls of this compartment just big enough to slide a sd card through. I mounted my Pi and my usb hub on a piece of acrylic screwed into the bottom of the teletype. I oriented my Pi so that the sd card would go through the hole I cut.
Image
Now I have easy access to my sd card though the battery door.
Image
Finally I found some I Home speakers that when trimmed fit perfectly into the cups for the teletypes modem. So don't be fooled by the image with the rotary phone. Thats just for show. Those cups are now speakers for my PI.
Image
I am now mostly done with hardware mode and ready to go into software mode. I have the Pi set up with PiMAME, and I am emulating c64 that way.
Image
I want to make individual sd cards that will boot directly into certain emulators. That way changing systems will be as easy as swapping out sd cards. I also have plans to use it as a file server to my atari computer using AspeQt. Best of all my Pi wont look out of place next to my old machines. I hope some of you found this useful. This was a huge learning experience for me and hopefully this will inspire someone else. I am planing some more modifications and features. I will post updates if there is interest.
Image

  • Sign in to reply
Parents
  • cstanton
    cstanton over 12 years ago

    I love this, great work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • cstanton
    cstanton over 12 years ago

    I love this, great work!