Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Road Testing The FTDI Vinculo (VNC2) USB Development Board
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 17 Jun 2011 8:16 AM Date Created
  • Views 2420 views
  • Likes 0 likes
  • Comments 2 comments
  • vinculo
  • vinculum
  • vnclo
  • vinco
  • review
  • vnc2
  • vinclo
  • ftdi
Related
Recommended

Road Testing The FTDI Vinculo (VNC2) USB Development Board

e14 Contributor
e14 Contributor
17 Jun 2011

I was lucky enough to get involved in the Farnell/element14 'road test' programme, where individual electronic hobbyists get a chance to review (and keep) cool hardware items from Farnell.

 

Last year I was lucky enough to attend a really useful free Eagle (PCB Design Tool) course run by element14, and earlier this year my local hackspace, BuildBrighton, reached the final of the Great Global Hackspace Challenge which was sponsored (very generously) by element14. While other suppliers might give out samples and freebies to industry, its refreshing that Farnell/element14 really do seem to be actively targetting and supporting the electronics hobbyist/hacker community - and so I am more than happy to sing their praises!

 

Anyway, back to my road testing... I chose to review the FTDI VNCLO-START1 kit. This kit is made up of a USB development board and a separate programmer/debugger board and the current cost on Farnell's web site is a little under £28 (http://uk.farnell.com/jsp/displayProduct.jsp?sku=1872599&CMP=e-2072-00001000)


The development board is branded the Vinco/Vinclo/Vinculo/Vnclo (it seems that FTDI aren't sure about the name yet, but I will call it “Vinculo”) containing the 64-pin version of FTDI's VNC2 'Vinculum' USB Host/Slave chip.

 

image


Very interestingly, FTDI have given the board the same form factor as an Arduino Uno, including pin-compatible Arduino shield header sockets and even an on-board ADC chip to provide the six analog inputs. This means that you should be able to make use of existing Arduino shields (add on boards) with the Vinculo, which is a clever move by FTDI.

The Vinculo can emulate an Arduino because it's on-board VNC2 chip is so much more than just a USB controller... its a fully fledged MCU. In fact it's a very powerful one, with a 16-bit core, 256kB of Flash, 16kB of RAM and 48Mhz clock among some other nice features... This makes it substantially more powerful that the AVR chip on the Arduino....And that’s before we get on to its USB support: Two full speed USB ports, each individually configurable as host or slave!

So, we're talking an impressive piece of silicon (and a reasonably priced one, with the 64-pin VNC2 chips selling on Farnell's site for just over £3 (http://uk.farnell.com/ftdi/vnc2-64l1b/controller-usb-vinculum-ii-64lqfp/dp/1863858), which is cheaper than the Atmega328).

I am planning to use VNC2 chips in two projects I have in the pipeline:

  • The first to USB-host a Novation Launchpad keypad controller and run a suite of animation/MIDI-input apps. The idea is to make a standalone version of my 'playpad' MIDI controller projects.
  • The second is as the 'brain' of my laser projector, where I need a high speed USB device to push coordinate data from a PC to a pair of DACs driving laser-projector galvos. Using a VNC2 means I can use a single chip (no need for separate USB chip and MCU) while avoiding the slowness of a polled USB stack implemented in software.


The Vinculo board seems like the perfect way to prototype these projects... so how to get started?

FTDI have a free, downloadable developer toolchain for the VNC2. This works with the VNC2 programmer/debugger to allow programming and interactive debugging of the Vinculo. And I really do mean interactive debugging... single stepping, breakpoints, watches and so on... controlled via USB to the debug board.. put that in your Arduino pipe and smoke it image

So that's all good news, but once I got started I found a few problems with the developer tools which made me think FTDI may not be quite there yet...

First of all I was unable to use the IDE on my desktop computer (where I do all my coding) because of a strange display problem with the source code editor window - all the text becomes garbled and unreadable each time the window scrolls. I reported this to FTDI support who quickly got back with a 'That’s strange, we'll look into it' kind of response but no fix as yet. However, luckily my laptop doesn't get the same issue so I could move on.

The second issue I found was stability of the IDE, particularly during debug sessions but even some times when compiling, the IDE would stop responding and needs to be killed in task manager and restarted.

Moving on, I played a bit with some of the provided sample code. The Vinculo is not FTDI's first VNC2 evaluation board, and some of the sample code is for the older eval board, which has different pin mappings for the connectors, meaning that the olders sample programs don't work without modifications. For example the UART (used by the sample programs for debug output) is attached to different pins between the Vinculo and the older VNC2 evaluation board.

Luckily the remapping can be done in software.... a nice feature of the VNC2 is that all the IO's go through a programmable multiplexer, so IO functions can be assigned to pins of your choosing. However the need to reassign IO's just to get the sample programs to work isn't what you want when you're first starting with a new device.

Another niggle is that while there are sample programs provided to demonstrate standard Arduino stuff (blinking LED, PWM examples and so on) what is glaringly lacking are any USB code examples that will work, without modification, on the Vinculo. Since USB is the attraction of Vinculo over vanilla Arduino I think this is something FTDI need to work on to make the board attractive to Arduino users... I am still trying to work out how to modify the USB examples to get them running on Vinculo, and its not been straightforward.

On a more positive note, something FTDI have done is to create a simple application framework that should appeal to Arduino coders by presenting an Arduino-like syntax.... For example, when using the supplied main.c in your Vinculo project you define the Arduino standard entry points 'setup' and 'loop'. Arduino-likey functions like digitalOut() are provided and libraries like Serial are emulated with structures containing function pointers, so familiar Arduino syntax like Serial.begin(9600); can be used.... Its just syntactic sugar, since behind the scenes the VNC2 API functions are being called, and its not 100% compatible (don't expect your Arduino code to 'just work' on Vinculo). However, it's a nice idea and will certainly appeal to Arduino developers - or you can simply ignore it if you'd rather work directly with the VNC2 API.

FTDI also have a variety of documentation for online download, which I am still working my way through. I have to say the information seem to be a bit 'scattered' over many different application notes, but at least it mostly seems to be there. Its just a bit daunting and confusing when you first get started.

In conclusion, I have to say I am still very excited by this hardware. The VNC2 is a powerful and flexible chip, and the Vinculo is a great prototyping board, encompassing some innovative ideas by FTDI.

However, at the moment I think much could be improved in the accompanying development software package. For me it has been a uphill struggle, and I think that Arduino users who are not experienced coders may fall at the first hurdle with this.. that is until FTDI can iron out the IDE issues and provide a more consistent and usable set of Vinculo code samples.

This is a new product though, so I have hopes that these things will improve soon.

A couple of other things that would be nice are

  • That Arduino staple - A pin 13 LED!
  • The ability to direct debug text output over the same USB cable that runs the debugger, where is can perhaps show up as a virtual COM port on the host PC (like on the mbed).


I will post again soon with my progress applying the Vinculo/VNC2 to my own projects... watch this space!

  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Interesting and informative report on the product.

     

    I would like to try to assist in some of your issues:

     

    I can confirm FTDI have settled on "Vinco" as the product name and the part number is VNCLO-MB1A.

     

     

    The VNCLO USB port 2 requires IOBUS22 (pin 41) to be set to logic 0 via a GPIO setting to allow for power to be sent to CN2 and power external USB devices on that connector.

     

    Some code that might help is:

     

    ////////////////////////////////////////////////////////////////////////
            // Vinco....Reassign pins for USB port LED and Power Control (port E used)
            // Pin 40 is connected to LED and Pin 41 is Power Enable on Vinco

            //vos_iomux_define_input(40,IOMUX_IN_UART_RXD); // Vinco - commented out UART Rx
            vos_iomux_define_output(40,IOMUX_OUT_GPIO_PORT_E_5); // Vinco - USB port 2 LED

            //vos_iomux_define_output(41,IOMUX_OUT_UART_RTS_N); // Vinco - commented out UART RTS#
            vos_iomux_define_output(41,IOMUX_OUT_GPIO_PORT_E_6); // Vinco - Power control

            // Note that LED0..LED3 which are used in the code below are not present
            // on the Vinco board
            ////////////////////////////////////////////////////////////////////////

     

     

    ////////////////////////////////////////////////////////////////////////
        // Vinco....Initialise Port E to control power transistor and LED
        gpioCtx.port_identifier = GPIO_PORT_E;     // Vinco
        gpio_init(VOS_DEV_GPIO_E,&gpioCtx);        // Vinco
        ////////////////////////////////////////////////////////////////////////

     

    ////////////////////////////////////////////////////////////////////////
        // Vinco....Set port E bits
        // LED is on E5 and Power Enable is on E6 so 8 port bits are as follows
        // Bit 7        Not used
        // Bit 6        Power Enable (active low)
        // Bit 5        LED (active low)
        // Bit 4        Not used
        // Bit 3        Not used
        // Bit 2        Not used
        // Bit 1        Not used
        // Bit 0        Not used

        hGpioE = vos_dev_open(VOS_DEV_GPIO_E);        // Vinco - Handle = port E

        gpio_iocb.ioctl_code = VOS_IOCTL_GPIO_SET_MASK; // Vinco
        gpio_iocb.value = 0x60;    // Vinco - 01100000   set bits 6 and 5 as output
        vos_dev_ioctl(hGpioE, &gpio_iocb);            // Vinco

        leds = 0x00;                     // Vinco
        vos_dev_write(hGpioE,&leds,1,NULL);        // Vinco - Write data of 00000000 to port
        ////////////////////////////////////////////////////////////////////////

     

     

     

    Additional Vinco examples are expected to be released soon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 15 years ago

    Interesting and informative report on the product.

     

    I would like to try to assist in some of your issues:

     

    I can confirm FTDI have settled on "Vinco" as the product name and the part number is VNCLO-MB1A.

     

     

    The VNCLO USB port 2 requires IOBUS22 (pin 41) to be set to logic 0 via a GPIO setting to allow for power to be sent to CN2 and power external USB devices on that connector.

     

    Some code that might help is:

     

    ////////////////////////////////////////////////////////////////////////
            // Vinco....Reassign pins for USB port LED and Power Control (port E used)
            // Pin 40 is connected to LED and Pin 41 is Power Enable on Vinco

            //vos_iomux_define_input(40,IOMUX_IN_UART_RXD); // Vinco - commented out UART Rx
            vos_iomux_define_output(40,IOMUX_OUT_GPIO_PORT_E_5); // Vinco - USB port 2 LED

            //vos_iomux_define_output(41,IOMUX_OUT_UART_RTS_N); // Vinco - commented out UART RTS#
            vos_iomux_define_output(41,IOMUX_OUT_GPIO_PORT_E_6); // Vinco - Power control

            // Note that LED0..LED3 which are used in the code below are not present
            // on the Vinco board
            ////////////////////////////////////////////////////////////////////////

     

     

    ////////////////////////////////////////////////////////////////////////
        // Vinco....Initialise Port E to control power transistor and LED
        gpioCtx.port_identifier = GPIO_PORT_E;     // Vinco
        gpio_init(VOS_DEV_GPIO_E,&gpioCtx);        // Vinco
        ////////////////////////////////////////////////////////////////////////

     

    ////////////////////////////////////////////////////////////////////////
        // Vinco....Set port E bits
        // LED is on E5 and Power Enable is on E6 so 8 port bits are as follows
        // Bit 7        Not used
        // Bit 6        Power Enable (active low)
        // Bit 5        LED (active low)
        // Bit 4        Not used
        // Bit 3        Not used
        // Bit 2        Not used
        // Bit 1        Not used
        // Bit 0        Not used

        hGpioE = vos_dev_open(VOS_DEV_GPIO_E);        // Vinco - Handle = port E

        gpio_iocb.ioctl_code = VOS_IOCTL_GPIO_SET_MASK; // Vinco
        gpio_iocb.value = 0x60;    // Vinco - 01100000   set bits 6 and 5 as output
        vos_dev_ioctl(hGpioE, &gpio_iocb);            // Vinco

        leds = 0x00;                     // Vinco
        vos_dev_write(hGpioE,&leds,1,NULL);        // Vinco - Write data of 00000000 to port
        ////////////////////////////////////////////////////////////////////////

     

     

     

    Additional Vinco examples are expected to be released soon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Thankyou very much for this information! I am sure this will be very useful. I'm also looking forward to the new sample projects for Vinco. Cheers, Jason