Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Rug Warrior Pi: Life in 10 Hour Segments
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: alanmcdonley
  • Date Created: 18 Jun 2016 1:34 PM Date Created
  • Views 1587 views
  • Likes 3 likes
  • Comments 3 comments
  • raspberry-pi-b+
  • battery life
  • ni-mh
  • robot-power-management
Related
Recommended

Rug Warrior Pi: Life in 10 Hour Segments

alanmcdonley
alanmcdonley
18 Jun 2016

I have tested my bot's battery life a few times in the last days to find the safe operating limit to avoid memory card corruption.

 

RWPi Battery Life Tests

 

Configuration ***:

EBL 5000mAh Ni-MH C Batteries: $25 15Dec2014

Raspberry Pi B+ 512MB

Mikronauts.com Pi Droid Alpha interface card (MCP3008 Analog Digital Conversion)

Pololu S18V20F5 5v 2A Step-Up/Step-Down voltage regulator

Pololu Pushbutton power switch

Fair Top 5A Current Sensor Module ACS712

 

*************

Test 17Jun2016

 

(Batteries are 18 months old)

 

Analysis ***:

 

  •   Safety Shutdown Voltage: (10 readings) of 6.7v leaves 10 minutes remaining charge.
  •   Voltage knee starts at 7v, 10.25 hours run after removal of trickle charge
  •   Starting at removal from the charger, robot will sit quietly

         10 hours 45 minutes (6.7v) and then should shutdown for safety.

  •   0.9v per cell reached at 10.9h,

          less than one minute before voltage plummeted precipitously

 

 

Results ***:

 

  • The sometimes recommended 0.9v per cell discharge limit ( 5.4v ) occurred at less than one minute of juice left before shutdown.
  • Voltage Knee began at 7v, 10.25 hours
  • Precipitous voltage drop at 1v per cell, 6v was reached at 10.9 hours.
  • Recharge, took about 4 hours to replenish the roughly 3000 mAh run

 

 

Method ***:

 

  • Battery was charged fully overnight before the test.
  • Test was started promptly after removal from trickle charge.
  • center.py was executed to initialize tilt/pan servos holding at centers.
  • Test began with the command: sudo python battery_life.py
  • battery_life.py measured the 7v2 unregulated power through a 2:1 15k Ohm resister divider to ADC6, roughly once per second, printing to a WiFi connected remote ssh shell, until 10 readings of 5.3v were seen, then the system executed sudo shutdown -h now.

 

image

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 10 years ago +1
    I have down a lot of graphs like this and that is one of the sharpest knees I have seen in real live analysis. I came close after many tries in as many months of work to find one of these. Clem
  • alanmcdonley
    alanmcdonley over 10 years ago in reply to clem57 +1
    I found that interesting also, but then in retrospect I think I understand why: I don't know at what voltage the step-up/step-down regulator changes from step-down mode to step-up mode, but after that…
Parents
  • bonzadog
    bonzadog over 8 years ago

    Interesting.

    I think perhaps it would be "better" to use LiPo batteries.

    Any chance of a Circuit diagram etc?

     

    I want to power a Rpi 3 with a 20,000 Ma Power pack or LiPo and really need to

    1) have a shutdown switch

    2) Automatic battery low detection and auto shutdown - preferably over an USB port sice I have a sensor hat on board.

     

    Due to a handicap I cannot build kits or solder myself so I am forced to use build and tested products - OR get them made for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • bonzadog
    bonzadog over 8 years ago

    Interesting.

    I think perhaps it would be "better" to use LiPo batteries.

    Any chance of a Circuit diagram etc?

     

    I want to power a Rpi 3 with a 20,000 Ma Power pack or LiPo and really need to

    1) have a shutdown switch

    2) Automatic battery low detection and auto shutdown - preferably over an USB port sice I have a sensor hat on board.

     

    Due to a handicap I cannot build kits or solder myself so I am forced to use build and tested products - OR get them made for me.