Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Self Driving Car (Automatic Lane Detection) (on a Robot)
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: vimarsh_
  • Date Created: 18 Nov 2019 4:58 PM Date Created
  • Views 8074 views
  • Likes 8 likes
  • Comments 3 comments
  • visionthingch
  • makevember 2019
  • makevember
  • raspberry pi
  • computer vision
Related
Recommended

Self Driving Car (Automatic Lane Detection) (on a Robot)

vimarsh_
vimarsh_
18 Nov 2019
My Robo v/s ... imageimage

The idea:

I wanted to create a quick project that can demonstrate the power of computer vision and its applications in real world. With the advancement in the self driving technology I wanted to create a small scale working model of an actual car inspired by Tesla.

Tesla basically follows lanes on highways/roads to go from one place to another with help of GPS. We are not going to create a full self driving car overtaking model but a lane follower will be the first step to driving autonomously.

           imageimageimage

 

The hardware:

I wanted to create a small scale lane following car using computer vision. So i immediately thought about Raspberry Pi and camera along with a Robot Chassis.

 

  1. Raspberry Pi 2 or newer (I used Pi 3B+ because it was laying around)
  2. Raspberry Pi camera color (I used the v1 also laying around)
  3. Robot Chassis (I used a chassis i had made with some acrylic sheets some time ago. Any can work)
  4. L298/L293D motor driver (i used L298 as it is more powerful and was already mounted on the robo)
  5. Battery (LiPo for motors and a powerbank for Pi)
  6. SD Card
  7. Wires, Glue Gun, Other tools

 

{gallery} Parts in order

image

image
image
image
image
image
image

 

Step 1: Building the Robot Chassis

The first step of the project is ti build your own robot chassis. If bought from somewhere follow the steps. But you can make one for yourself with some acrylic or plastic sheets. I made a 4 wheel drive setup and two motors of one side are controlled by same signal.

 

Step2: Setting up Raspberry Pi

The next important step is to setup Raspberry Pi with OS and libraries required to do the task.

First start my flashing Raspbian on an SD card (16GB recommended). A wonderful guide is here: https://www.raspberrypi.org/documentation/installation/installing-images/

Note: Please install buster for RPi 4 otherwise Raspbian for other boards

image

 

After you install Raspbian on an SD card connect it to your wifi network and enable VNC as it can be used to access the desktop of RPi from your computer.

It is recommended to use Python3 for the project as Python2 is going out of support in few weeks and OpenCV easily gets installed if you use Python3!

 

Now we need to install some Libraries:

commands in gist below>>>image

Step3: Connections

image

This is the basic schematic but you can change the pin connections to the Raspberry Pi according to your wish. But remember to change it in the code.

You can replace a 9V battery with a LiPo (preferably for 4WD) as L298N have input voltage upto 20V easily.

Also you can directly connect the 5V out from the motor driver to RPi but I would not recommend it as it fluctuates and can harm your Pi.

image

I have used the pins 5,12,13,19 to connect pins IN1,IN2,IN3,IN4 of the motor driver.

Make sure to not connect any high voltage source directly to your Pi as it will kill it!

 

Step4: Full Code and Explanation

 

So first of all we need to import libraries

from picamera.array import PiRGBArray
import RPi.GPIO as GPIO
from picamera import PiCamera
import time
import cv2
import numpy as np
import math

Picamera for interfacing with the camera attached to the Pi.

RPi.GPIO to access the GPIOs to give commands to L298N motor driver to control the motors.

time for delays.

OpenCV (cv2) the main library to be used to do image processing

Numpy and math to perform certain operations.

 

Next we declare the GPIOs and some variables.

GPIO.setmode(GPIO.BCM) #Sets the mode to be used. BOARD will be numbered according to mapping of pins (1,2,3,4,...) and BCM for GPIOs as they are.

#Declaring functions of the GPIOs
GPIO.setup(13, GPIO.OUT)
GPIO.setup(19, GPIO.OUT)
GPIO.setup(5, GPIO.OUT)
GPIO.setup(12, GPIO.OUT)

#Setting all the GPIO to LOW uring startup. Refer to schmeatic for your mapping
GPIO.output(5, GPIO.LOW)
GPIO.output(12, GPIO.LOW)
GPIO.output(19, GPIO.LOW)
GPIO.output(13, GPIO.LOW)

#Variable to store data about track and rotation.
theta=0
minLineLength = 5
maxLineGap = 10

Next we use the PiCamera and link it to variables and perform startup commands

camera = PiCamera()
camera.resolution = (640, 480)
camera.framerate = 15

rawCapture = PiRGBArray(camera, size=(640, 480))
time.sleep(0.1)

Then comes the actual program logic (broken into two parts here)

for frame in camera.capture_continuous(rawCapture, format="bgr", use_video_port=True):
   GPIO.output(5, GPIO.LOW)
   GPIO.output(12, GPIO.LOW)
   GPIO.output(13, GPIO.LOW)
   GPIO.output(19, GPIO.LOW)
   time.sleep(0.0)
   image = frame.array
   gray = cv2.cvtColor(image, cv2.COLOR_BGR2GRAY) #Convert the image from color to Grayscale
   blurred = cv2.GaussianBlur(gray, (5, 5), 0)
   edged = cv2.Canny(blurred, 85, 85)
   lines = cv2.HoughLinesP(edged,1,np.pi/180,10,minLineLength,maxLineGap)
   
   if(lines !=[]):
       for x in range(0, len(lines)):
           for x1,y1,x2,y2 in lines[x]:
               cv2.line(image,(x1,y1),(x2,y2),(0,255,0),2)
               theta=theta+math.atan2((y2-y1),(x2-x1))

 

First off all we open a loop that will go on continuosly to take input from the camera.

Then we set all our GPIOs LOW as its begining of detection (after first iteration)

OpenCV marks color in order of BGR (Blue, Green, Red) instead of RGB(Red, Green, Blue) for seemingly no reason.

Now we start with Image Processing.

First we convert all pixels to GrayScale

then we 'Smoothen the Images"

and use "Canny Edge Detection" to bring out the borders between the objects

And ultimately we use Hough Line Transformation basically identifies shapes and lines.

 

The explanation of these are greatly explained here:

Gaussian Blur - Smoothening of image

opencv tutorial and explanation on Hough Line Transformation Hough Tranformation is a really good tool and very usefull.

The Hough Transform: The Basics - AI Shack

Canny Edge detection Tutorial and explaination

 

Explaining the turn decision:

After drawing the lines we map out the distance as vectors and and measure their angles from horizontal. Its a very interesting technique. We add all the measured angles and predict the path of the lane.

image

As you can see in this image that most of the lines are drawn <Pi/2 so it return the value as right.

 

image

Even in this diffult scenarios when one lane is only visible because it measures the angles it can tell to go left which is correct

 

Note: the angle measured is in Radians not in degrees.

Now about controlling the robot with those data

     threshold=6
   
   if(theta>threshold):
       GPIO.output(5, GPIO.LOW)
       GPIO.output(12, GPIO.HIGH)
       GPIO.output(19, GPIO.LOW)
       GPIO.output(13, GPIO.HIGH)
       print("left")
       
   if(theta<-threshold):
       GPIO.output(12, GPIO.LOW)
       GPIO.output(5, GPIO.HIGH)
       GPIO.output(13, GPIO.LOW)
       GPIO.output(19, GPIO.HIGH)
       print("right")
       
   if(abs(theta)<threshold):
      GPIO.output(5, GPIO.LOW)
      GPIO.output(12, GPIO.HIGH)
      GPIO.output(13, GPIO.LOW)
      GPIO.output(19, GPIO.HIGH)
      print ("straight")
   
   theta=0
   cv2.imshow("Frame",image)
   key = cv2.waitKey(1) & 0xFF
   rawCapture.truncate(0)
   
   if key == ord("q"):
       break

please see this code from gist linked below because indentation might be incorrect here.

 

First we declarte the threshold that we want I found 6 to be a good spot thoug 6.4 was best suited for me.

We check if the sum of angles (the length of line is also taken into consideration while measuring the angle) was greater than threshold so when it detected lines more that 90 degrees it says to go right. The GPIO output is done accordingly.

If it is lesser tha -6 that means it is in dfferent quadrant we know that it is because more lines are bend towards left.

Similarly for Straight going but you may have to change the threshold to make it go perfectly.

 

The we show the lines on the image as output and check if 'q' is pressed to quit and then the llop above goes on.

 

Full Code:

 

 

Demonstration:

 

 

{gallery} My Robot

image

Picture

image

Robot side view

image

Robot front view

image

Camera modeule

image

Raspberry Pi showing connections

image

Robot bottom view: Messy wiring

 

 

 

Video>>>

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This is the first iteration that just uses some Image processing, I am working on next version where ML is used to train it to follow a path....

 

Conclusion

Overall I was very happy with the project even though it didn't perform extraordinary in navigating lanes.

Checkout the video if not yet.

But I had made the project in just 4 hours so I would call it a day.

I would like to add a better navigation by training a custom model and then predicting the path ahead. But that is for another day.

 

The next thing I learnt was that robot was too fast in moving and so the frame would freeze and it wouldn't detect any line and give error for no line detected and stop there. So it is better to create a new function and then use PWM signals to control the speed of the motors.

image

 

I would love to use more of OpenCV's inbuilt features to just use Image processing to navigate because once we involve training a model and then Deep Learning Implementation that is very heavy for the Pi.

Here you can see that even when the SBC is making critical decisions the CPU usage is not much and it stays cool.image

 

You may also see some inefficiencies in the code because I learnt and gathered sources to make it in one day so it is rough. Let us make it a huge project and let us all collaborate to work on the existing framework to built on top a better Self-Driving car system.

What I learnt is that you can not go to the Tesla level because a lot of very smart engineers are working on the system to make it really "Autonomous". This makes me really optimistic for the future of Computer Vision.

 

Update 1:

As per dubbie 's comment I reduced the speed of the motor. I just connected both the enable pins (ENA and ENB) to GPIO 18 on Raspberry Pi. Then I enabled 1KHz 50% duty-cycle on Raspberry Pi code and that worked out very well. It can follow lanes now very well but the ride has become very jerky. Tying to find a sweet spot between them.

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 6 years ago +4
    I really liked this project and I think you have achieved a significant amount. It looks like it is almost working. When I made a black line follower I had some similar problems, it was going much to fast…
  • shabaz
    shabaz over 6 years ago +3
    Hi Vimarsh, Great project. Any robotics project can be very challenging, so to achieve this much is still very impressive. Good documentation too. I'm seeing some black image anomaly in a couple of areas…
  • clem57
    clem57 over 6 years ago +3
    Great project and it worked in under 4 hours. Keep up the good work. Thanks vimarsh_
  • clem57
    clem57 over 6 years ago

    Great project and it worked in under 4 hours. Keep up the good work.

    Thanks vimarsh_

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago

    Hi Vimarsh,

     

    Great project. Any robotics project can be very challenging, so to achieve this much is still very impressive. Good documentation too. I'm seeing some black image anomaly in a couple of areas, but apart from that, the documentation is good.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago

    I really liked this project and I think you have achieved a significant amount. It looks like it is almost working. When I made a black line follower I had some similar problems, it was going much to fast and was jerky, so I just made it go slower so that the sensor system could work better. You could use some pulse width modulation on the motor driver to slow the car down, that should help. You might need a bigger road as well, it looks like your vehicle would work outside. Light levels are a problem, I tend to have to customise my black line follower to every different lighting environment it is used in. The alternative is to learn a lot of control theory.

     

    I have not made a vision based black line follower and never even thought of making a lane follower. Your example has encouraged me to think about what I might be able to do.

     

    Dubbie

    • Cancel
    • Vote Up +4 Vote Down