Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Solar Cell On A Sunny Day
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 6 May 2020 9:15 PM Date Created
  • Views 1151 views
  • Likes 8 likes
  • Comments 2 comments
  • solar cell
  • efficiency
Related
Recommended

Solar Cell On A Sunny Day

dubbie
dubbie
6 May 2020

As the sun was shining much more brightly today I decided to repeat my measurements of the solar cell (Solar Cell Maximum Power Output (Hazy Sunshine) ) to try and obtain a more detailed view. This time I only took measurements in the range 600 Ohms to 10 Ohms, in steps of 100 Ohms down to 200 Ohms and then in steps of 10 Ohms. The graph is displayed below and seems much better.

 

image

This has produced a much better curve and shows that the peak power output of 426 mW is at 60 Ohms load, comprising 83 mA at 5.1 V, which is pretty impressive for such a small solar cell. Nearly 0,5 Watts. That's enough to run a small mobile robot, albeit on a very sunny day. Still, two of these solar cells would be more likely to work better and three would be even better.

 

These solar cells have an area of 0.12 x 0.038  =  0.00456 square metres

 

Now work out how many of these solar cells are needed to make one square meter

 

Number = 1/0.00456  == 219.3

 

So if I have 219 of these solar cells I should be able to obtain a total power of:

 

Power  = 219 x 0.428

            =  93.9 W

 

I have had difficulty finding the average solar irradiation (insolation) in the south of the UK in May but I thought that it was about 800 Watts per square metre (some sources put it as low as 200 W m−2 ), but assuming 800 Wm−2 this would imply an efficiency of this solar cell of:

 

Efficiency = 93.9/800 x 100%

                =  11.3 %

 

which seems about right for this type of solar cell.

 

Dubbie

  • Sign in to reply

Top Comments

  • genebren
    genebren over 6 years ago +3
    Good job Dubbie! The curve look much better. I guess the minor changes in lighting as you were collecting data were the cause of the bumps and valleys in your earlier waveform. I look forward to seeing…
  • dubbie
    dubbie over 6 years ago in reply to genebren +2
    Gene, Yes, the curve does look much better, but I was reading about insolation levels in the UK and apparently they factor in the effect of wind on solar panels. The wind reduces the temperature of the…
  • dubbie
    dubbie over 6 years ago in reply to genebren

    Gene,

     

    Yes, the curve does look much better, but I was reading about insolation levels in the UK and apparently they factor in the effect of wind on solar panels. The wind reduces the temperature of the solar panels which increases their efficiency. Maybe some of the little blips of the first set of results were due to transient winds. I must remember to try this out some time. Blowing on my solar cells to get more power!

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 6 years ago

    Good job Dubbie!  The curve look much better.  I guess the minor changes in lighting as you were collecting data were the cause of the bumps and valleys in your earlier waveform.

     

    I look forward to seeing the robots running about.

    • Cancel
    • Vote Up +3 Vote Down