Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Solar Garden Light
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 31 Mar 2017 1:49 PM Date Created
  • Views 3047 views
  • Likes 8 likes
  • Comments 10 comments
  • solarpwrdevicesch
Related
Recommended

Solar Garden Light

jc2048
jc2048
31 Mar 2017

A couple of days ago, I was in a store here in the UK (in the garden department looking at seeds and bulbs) when some 'solar lights' caught my eye. The very cheap

ones didn't look up to much, but the £2 ones had a decent solar cell on them so I bought one. I was curious as to how something with a CE sticker saying it had

a 1.2V battery inside was able to light a white LED that would need a forward voltage of around 3V to illuminate.

 

Here are some photographs as I disassembled it.

 

image

image

image

 

image

image

 

There's not a lot to it. The battery is a 1.2V Ni-MH cell. What at first glance might appear a transistor is actually an integrated circuit (three legs good,

four legs better!) and there's a single passive component that you might, at first glance, mistake for a resistor.

 

The cell voltage was very low and it would only power the LED for a few seconds, so I put it on a window sill in the sun for a day. By the evening, the cell was

charged and the terminal voltage (off load) was up to 1.32V.

 

As you might expect, to get the 1.3V up to the 3V needed to power the LED requires a switching circuit and the device that looks like a resistor is actually a choke (coil).

 

Here's a schematic

 

image

 

Here are some waveforms. The yellow trace is the connection between the coil and the LED. The blue trace is the current through the LED. A switch to ground in

the IC waits for the coil to ramp up to about 18mA, then lets it go, allowing it to run into the LED. The average LED current looks to be about 4mA overall.

 

image

 

If I calculate (roughly) the coil value from the waveforms

 

L = V x dT / dI = 1.32V x 2.4uS / 18mA = 176uH.

 

That agrees with the coil markings: brown-grey-brown would be 180.

 

I haven't looked at the solar cell and the charging side of things as of yet.

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 9 years ago in reply to jc2048 +4
    Hi John, I just finished finding my solar light circuits of which I have two styles. The older one is perhaps 15 years old. Here are pictures of it. The little 5 legged ic has the number 5438 on it. Besides…
  • fluxcap
    fluxcap over 9 years ago +2
    Very interesting that's a good deal for the price on just parts. Even if they were pretty cheap parts still a good deal. Very interested if that solar panel is any good. Have a great day!!
  • jw0752
    jw0752 over 9 years ago +2
    Hi Jon, Great analysis of a good mystery. I too have bought these lights but I never realized that they were small switching buck circuits. I made the assumption that the only purpose of the IC was to…
Parents
  • jw0752
    jw0752 over 9 years ago

    Hi Jon,

    Great analysis of a good mystery. I too have bought these lights but I never realized that they were small switching buck circuits. I made the assumption that the only purpose of the IC was to switch between charge and illuminate when the ambient light drops below a threshold. Tonight I will be going back to look at the similar circuits that I have accumulated. The Dollar Tree store here often has these for $1.00 a piece. It is hard to buy batteries that cheap.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 9 years ago

    Hi Jon,

    Great analysis of a good mystery. I too have bought these lights but I never realized that they were small switching buck circuits. I made the assumption that the only purpose of the IC was to switch between charge and illuminate when the ambient light drops below a threshold. Tonight I will be going back to look at the similar circuits that I have accumulated. The Dollar Tree store here often has these for $1.00 a piece. It is hard to buy batteries that cheap.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jc2048
    jc2048 over 9 years ago in reply to jw0752

    It's a boost converter, not a buck. Normally, a boost converter would have the diode feeding an output capacitor and topping it up each cycle with the energy from the coil (with feedback necessary to keep the voltage steady). In this case there's no need for the capacitor because the current through the diode (LED) is what we are interested in and not generating a fixed voltage. It doesn't matter at all that it falls to zero because our eyes happily integrate the light energy to give the average (at least they do when it occurs 215,000 times a second). No feedback is necessary because the LED start current will be the value the coil current has reached at the end of the switch 'on' period (that value may be determined by a current sense in the IC or probably, more simply, just having a fixed period for the 'on' time - the rate at which the coil current ramps is a function of the inductance). The output voltage you can see in the scope trace is then just the LED forward voltage at whatever current is flowing.

     

    I'd be interested to hear if the ones you have operate in the same way.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to jc2048

    Of Course you are correct and I misspoke. It has to be a boost not a buck. Time willing I will check out and show some picture of the ones I have tonight.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to jc2048

    Hi John,

    I just finished finding my solar light circuits of which I have two styles. The older one is perhaps 15 years old. Here are pictures of it.

     

    image

     

    image

     

    image

     

    The little 5 legged ic has the number 5438 on it. Besides the IC there is a resistor, diode, inductor, and a capacitor. In this case they are bothering to smooth out the pulse train that is operating at 54 kHz.

     

    Here are the pictures of the newer unit which is perhaps only 3 years old.

     

    image

     

    image

     

    image

     

    I suspect that this one is more like yours. The numbers on the IC are YX8018 and it operates at 227 kHz. They must have moved all the other components onto the chip as the only externals are the inductor 470 uH and the LED just as you described your unit.  Even at this level of simplicity one has to marvel that they can manufacture this unit, package it, ship it to the USA, distribute it to the stores and then sell it for $1.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fluxcap
    fluxcap over 9 years ago in reply to jc2048

    I still have a lot to learn so just in these comments I've bunches about something I thought was so simple. This is a reason I love engineering, it's more than meets the eye!!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to jw0752

    Yes, it's the same IC. I can make out the YX8018, though the lettering is very faint.

     

    Interesting development path - once the quantities get large enough it becomes worth doing a custom chip.