Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Some Tips about Selecting The Best iPhone 4 Cases For You
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ahstuzl100
  • Date Created: 20 Nov 2010 7:32 AM Date Created
  • Views 794 views
  • Likes 0 likes
  • Comments 0 comments
  • cases
  • case
  • iphone
  • 4
Related
Recommended

Some Tips about Selecting The Best iPhone 4 Cases For You

ahstuzl100
ahstuzl100
20 Nov 2010
As you probably have heard, the new iPhone 4 has a "reception issue" when you hold the iPhone 4 towards the lower left corner and then press down hard. What you will notice is that the reception bars start to drop and then if you are on a call while doing this, the call will drop out.
 
If you hold it in the left hand at the bottom you will see that the signal will often times drop and can result in a lost call. If you have experienced this in the past and want to avoid it then you will need to invest in one of the available iPhone 4 cases.
 
Many people are looking for the best iPhone 4 Leather Case but this is a matter of the use that you have for the iPhone. If you are simply using it as a phone that includes the ability to chat via the video function then you should go with a simple design.
 
Enjoy every single photo-op with your Apple iPhone 4, as the recent issues for camera flash with regards to different iPhone 4 Silicone Case are now a thing of the past. Accessoriesofapple makes sure that you will enjoy all the features of your extremely wonderful device as they made a great cut for the camera and flash opening that does not intrude or mess up your photo-capture moments.
 
Everything but the kitchen sink, aside from the Nude case you will get two screen protectors, a microfiber cloth, squeegee card for screen film application, two 3.5mm inserts to keep it away from dust and two dock connector protectors.
 
Where do you shop? I suggest this iPhone 4 case shop because you'll see a great range and if you find something that you love, you can order for it and have it delivered.