Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs STM32F103ZE ARM Cortex-M3 Board
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kennyxie
  • Date Created: 12 Nov 2009 1:58 AM Date Created
  • Views 768 views
  • Likes 0 likes
  • Comments 0 comments
  • board
  • arm_eval_board
  • arm_development_board
  • stm32f103_
  • arm_development_tools
  • st_cortex-m3
  • evaluation_board
Related
Recommended

STM32F103ZE ARM Cortex-M3 Board

kennyxie
kennyxie
12 Nov 2009

For more details, please feel free to visit: http://www.embedinfo.com/en/list.asp?id=31.

 

The STM32F103ZEH6STM32F103ZEH6 is an ARM embedded evaluation board produced by Embest, integrate the STMicroelectronic ARM Cortex-M3 core-based processor STM32F103ZE, operating at a 72 MHz frequency. The board features USB, CAN, SD Card interface, TFT-LCD, RS232 serial interface, four 26-pin user extended interface, etc. Plenty of software examples, which can be used in Keil MDK environment, are accompanied in CDROM.

  • 512KB Flash memory, 64KB SRAM
  • uCOS-II v2.86 ported
  • Source code of example program

 

Hardware Specifications:

The connectors on the STM32F103ZEH6STM32F103ZEH6 ARM evaluation board provide easy access to many of the STM32F103ZE's on-chip peripherals.

  • Serial Port
    A standard DB9 connector is on the STM32F103ZEH6STM32F103ZEH6 board for the STM32F103ZE's built-in UART interfaces. This is a full duplex, serial port.
  • CAN Port
    A standard DB9 connector for applications requiring CAN communications.
  • USB Port
    A standard USB Type B connector for applications requiring USB communications.
  • LCD Display
    A detachable, 240x320 TFT, color LCD display. You may use this graphic display device to show real-time debug and program status messages.
  • On-board Battery
    A removable, lithium battery is included on the STM32F103ZEH6STM32F103ZEH6 to maintain power to the real-time clock when the board disconnects from the main power supply.
  • Analog Voltage Control for ADC Input
    An adjustable analog voltage source for testing the Analog to Digital converter built into the STM32F103ZEH6STM32F103ZEH6.
  • External Memory
    The STM32F103ZEH6STM32F103ZEH6 board includes 1 Mbyte of external static RAM and 8 Mbytes of external SPI Flash memory.
  • MicroSD Card Connector
    A MicroSD Card connector for developing applications requiring access to MicroSD Cards.
  • ETM Trace Debug
    An ETM connector for on-chip debugging via the Embedded Trace Macrocell capabilities of the STM32F103 device.
  • JTAG Download and Debug
    A JTAG on-chip debug interface, coupled with the ULINK USB-JTAG adapter, provides flash programming and real-time in-circuit emulation of the STM32F103 device.

Attachments: