Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Streaming sound to arduino using serial
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: idanre1
  • Date Created: 18 May 2017 1:24 PM Date Created
  • Views 2219 views
  • Likes 1 like
  • Comments 1 comment
  • music
  • arduino
  • music_streaming
  • streaming
Related
Recommended

Streaming sound to arduino using serial

idanre1
idanre1
18 May 2017

Hi

I have searched the internet for a way to stream music to arduino using serial port.

What I actually wanted doing is playing music during the time arduino drive DC motor.

I can say I couldn't find a descent library for doing it, so I ended up doing it by myself.

 

I found some template which I can work with: Streaming Audio over Serial

But many things were missing, mostly the remote software and the parsing of WAV files...

 

After a weekend (my most productive times are weekends image) I managed to play sound in arduino and in the middle of playing the sound do something else (e.g. turn led pin on/off)

Since many files are needed (arduino code, wav parser, remote SW) I put it all on github.

https://github.com/idanre1/audioStreamArduino

 

To play sound i used 2N222 transistor in this setup:

image

 

 

My remote program is written in Perl, and I'm using linux as a remote station.

I am using ffmpeg as a generic converter to pre-process the files for arduino format (8 bit PCM), convert.sh file is provided under music folder.

 

I would like to hear your thought about it

  • Can somebody try run it on windows? I know many users like windows.
  • Do you think the code is robust enough?
    • Is it self explained how to add new codes?
  • Do you think this is something you could use for some project?
  • Using bluetooth serial module this project can be wireless.
    • Is there an android fan who thinks he can code Java remote client to interface with the code?
      I think a phone as a remote could be great...

 

Regards

Idan

  • Sign in to reply
  • balearicdynamics
    balearicdynamics over 9 years ago

    To be honest I found it very well done and organised. Good idea to put the code on GitHub, I am doing it too by a while and I think it is the right solution for sharing, better than attaching the sources in zip format to the bottom of the post.

    I managed to play sound in arduino and in the middle of playing the sound do something else

    As your specific case is driving a motor while playing, I suggest to make a test instead of using a led to be 100% sure that there are no interferences due the motor magnetic field. In theory I think no but maybe helpful a out-of-the-box test. Maybe the problem, if occur, can be easily solved with a discrete component. There are many other valued member more expert than me to investigate this potential issue. My suggestion is just empiric.

     

    Enrico