Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Supercap to the Rescue
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: nikhilstephen
  • Date Created: 27 Aug 2018 12:32 PM Date Created
  • Views 1574 views
  • Likes 5 likes
  • Comments 3 comments
  • self discharge
  • leakage_current
  • supercapacitors
  • ac current
  • battery
  • ripple voltage
  • passive_blog
Related
Recommended

Supercap to the Rescue

nikhilstephen
nikhilstephen
27 Aug 2018

image

The relationship between Superman and Lois Lane is equivalent to a supercapacitor and capacitance. Unlike Superman with Lois Lane, a supercapacitor cannot come to the rescue every time. “What is this mighty supercapacitor?” one might ask. To make this easier let’s break it down, according to Dictionary.com Super is defined as “more effective, more powerful, or more successful than others”. It is a common misconception that people might think a supercapacitor is just a more powerful capacitor.

How can anything be this powerful? The answer is it can’t! Just like kryptonite is Superman’s weakness, a supercapacitor has several weaknesses. One weak point is that they are limited to low voltage applications because of the high equivalent series resistance (ESR). When a supercapacitor is connected to a power supply, the voltage drop increases when a high current flows, due to the high internal resistance. This means that it is unable to output sufficient energy during periods of high demand. After reading this blog post, you will understand how supercapacitor is indeed more than some capacitor that wears underwear over his pants and claims to be from a mysterious planet.

One major drawback of electricity is that it is relatively difficult to store in a hurry. Batteries can hold a large amount of power, but they take hours to charge up. Capacitors, on the other hand, charge almost instantly but store only tiny amounts of power. When we need to store and release large amounts of electricity very quickly, we turn to supercapacitors (also known as ultracapacitors). A supercapacitor has 2 plates that are separated, like an ordinary capacitor. The plates are made from metal coated with a porous substance such as powdery, activated charcoal. Imagine electricity is water; where an ordinary capacitor is a piece of cloth that can mop up only a small spill, a supercapacitors porous plates makes it a sponge that can soak up a lot more water.

 

image

Leakage Current & Self- Discharge

A supercapacitors leakage current and self-discharge characteristic are important things to consider when designing a circuit. A supercapacitor has a high internal resistance, thus a small current is needed to keep the charge on the supercapacitor. Leakage current determines self- discharge of the supercapacitor. If a charged supercapacitor is kept unpowered for long, it will discharge itself.

Leakage Current

The amount of current necessary to keep the capacitor charged to a certain voltage is known as leakage current. The charge current decreases as time go by, and it becomes stable over time. A steady-state current is called “Leakage Current”. The figure below shows the leakage current characteristics at room temperature and the measurement circuit. When the supercapacitor is charged, there is a stable parasitic current. A supercapacitor is charged by ion absorption and desorption, and the parasitic current at beginning of charge is high as ions are trying to reach deep inside of fine pores of the activated carbon. This initial current is called “absorption current”. This charge current decreases as time go by, and it becomes stable over time.

image

Self- Discharge Characteristics

Now that we know about leakage current, let’s talk about self- discharge. When the main charging source is disconnected from the supercapacitor, the supercapacitor starts losing its charge because of its high internal resistance. This is called self- discharge characteristics. It is a voltage drop in the charged capacitor after a period with no load condition, voltage losses in the range of 5-60% occur every two weeks. Experiments show a dependency of the self-discharge rate on various parameters such as temperature, charge duration and short-term history. The figure below shows the self- discharge characteristics of the FC series supercapacitors.

image

Finding your Leakage and Self- Discharge

Current is found by applying a voltage to the capacitor [C] and measuring the voltage across the resistor after 30 minutes ( The voltage is applied after both terminals of the capacitor are shorted for 30 minutes or more to discharge it). The main current component after 30 minutes of voltage application is an absorption current. It takes several tens to hundreds of hours for a leakage current to become the main component as the absorption current reduces.

Current, I = (VR/RC) x 103(mA)

  • I: Current (A)
  • VR: Voltage (V)
  • RC: Series resistor (Ω)

The self- discharge characteristics is measured by charging a voltage of 5.0VDC  (charge protection resistance: 0 Ω- No resistor in between power supply & supercapacitor)according to the capacitor polarity for 24 hours, then releasing between the pins for 24 hours and measuring the pin- to- pin voltage. This test should be carried out in an environment with an ambient temperature of 25oC or below and relative humidity of 70%RH or below.Self-Discharge Current, ISD = (C x (V0 – V0 – Vdrop) ) / T

  • ISD: Self-discharge current (A)
  • C: Capacitance (F)
  • V0: Voltage (V)
  • V1: Voltage (V)
  • Vdrop: Voltage drop due to DCR (V)
  • T: Time (sec)

 

Now that you have a good understanding of supercapacitors and its characteristics, who’s the actual hero? Superman or supercapacitors? Head over to Component Edge to find a supercapacitor appropriate for your next project.

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 8 years ago +3
    I'm afraid that this article is not at all illuminating. The author seems somewhat confused between internal series resistance (often called DCR and ESR in specs) and and leakage resistance (almost never…
  • jw0752
    jw0752 over 8 years ago +3
    Hi Nick, Thanks for taking the time to write the blog on Super Capacitors. It was interesting and likely to generate some discussion and a chance for everyone to learn. As Michael pointed out you will…
Parents
  • michaelkellett
    michaelkellett over 8 years ago

    I'm afraid that this article is not at all illuminating.

    The author seems somewhat confused between internal series resistance (often called DCR and ESR in specs)  and and leakage resistance (almost never quoted in specs which usually specify leakage current).

    This is kind of worrying because the web site linked to seems to belong to Kemet who make some pretty decent capacitors.

     

    I'm not going to go through the whole article but I'll illustrate with this quote form the second paragraph:

     

    One weak point is that they are limited to low voltage applications because of the high equivalent series resistance (ESR).

     

    This is quite simply nonsense. ESR has nothing to do with the rated voltage of a capacitor. Supercaps are limited to typically about 2.5V max voltage by of the chemistry of their operation. Some Supercaps have very low DCR, so low that they can be used instead of lead acid batteries for starting engines !

     

    In fact ESR is usually an AC (often 1kHz or 100kHz) characteristic, for supercaps we are often more interested in DCR (the DC equivalent series resistance).

     

    There is an article on Wiki that is fairly helpful but it's weak on actual specifications:

     

    https://en.wikipedia.org/wiki/Supercapacitor

     

    I'll give an example, Nichicon do a 2600F at 2.5V part with a DCR of 1.3mOhm and Leakage current of 1.3A, It's 63mm diameter, 150mm tall and costs about £350 for one. They don't specify the maximum discharge current but do use M6 bolt style terminals. The short ciruit current would be about 2000A so I guess it could actually be used to provide 100A or so.

    They don't quote peak current allowed but Vishay quote 35A for  an 18 mOhm part.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 8 years ago in reply to michaelkellett

    I thought I was the only one going "ehhh ... what?" when reading the article!

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Gough Lui
    Gough Lui over 8 years ago in reply to michaelkellett

    I thought I was the only one going "ehhh ... what?" when reading the article!

     

    - Gough