Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Testing Home Automation with ARM mbed IoT Starter Kit.
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mudz
  • Date Created: 2 Apr 2015 10:13 PM Date Created
  • Views 1074 views
  • Likes 0 likes
  • Comments 0 comments
  • starter_kit
  • ibm_cloud
  • mbed
  • home_automation
  • iot
  • arm
  • ibm
  • arm_mbed_iot_starter_kit
Related
Recommended

Testing Home Automation with ARM mbed IoT Starter Kit.

mudz
mudz
2 Apr 2015

AIM: To establish a connection between IoT starter Kit and Internet enabled Modem via AirGrid Modules.

Requirements: ARM mbed IoT Starter Kit, 2 AirGrid M5-HP Modules, 4 Ethernet Cables, 2 PoE adapters, Internet enabled Modem.

                                     image

                             FRDM-K64F Starter Kit connected with AP(AirGrid Module)                              Station(AirGrid Module) connected to office Modem(Internet) or pc

 

Introduction:

The Idea is to test the ARM mbed IoT starter Kit for Home automation. It is just a test not full implementation of this kit for home automation. In this Experiment we are going to connect Starter Kit(at home) to the Modem(Internet at workplace) with the help of two AirGrid modules which create a Wireless Lan link between Home and office. If this experiment is successful we know that we can replace the modem with our PC (at workplace) to give control commands over Wireless link to Starter Kit for Home automation or smart home like features.

 

Tasks to perform:

1. Configure AirGrid M5-HP modules to Work as Wireless link.

2. Connect ARM mbed IoT starter Kit with AirGrid M5-HP module(AP).

3. Connect Station AirGrid module to Internet(modem)

 

Task 1:

Aim: To establish a Wireless link between two AirGrid Modules.

This is done by configuring one of the AirGrid module to work as a Station and the other one as Access Point. How to do it? I will Explain it step by step but first lets get familiar with the equipments we will be using for this experiment.

 

imageimage

                                                  1. AirGrid M5-HP Module                                                                          2. Power over Ethernet (PoE)

 

1. AirGrid M5-HP : These modules provides a Wireless Lan Links for long distance data transmission with the help of Antenna. These Modules generally works on 5GHz (Unlicensed Band Radio) frequency range. for more on these moduels visit: https://www.ubnt.com/airmax/airgridm/

     These modules does not work right away after opening them from the box. We need to configure these modules to work and that too as per our requirements i.e. how we want to use them. For now, we just want to create a wireless link between our home and Office. So we need to make one module to work as Station (at Internet side; office) and Access point (at Kit side: Home).

2. PoE: Power over Ethernet adapters provide power to these AirGrid modules. These PoE's are highly reliable and are generally used for continous working  conditions. Output voltage is in range of : DC 24v, 0.5A.

If we take a closer look at these PoE, we find two Ethenet ports mentioned as POE & LAN written on its surface. We connect Airgrid Module to POE via Ethernet cable. This POE provides the required power to drive the AirGrid Modules. To establish a connection between PC/Modem to this Airgrid Module we connect Ethernet cable to this(PoE's) LAN port.

 

Powering the AirGrid Module:

Connect POE to the AirGRid Module via ethernet cable and connect power cord to the PoE adapter. Switch on the PoE adapter.

                                                          image

                                                                      3. Airgrid Module connected to POE via ethernet Cable

 

 

Configure the AirGrid Modules:

We need to configure each AirGrid module one by one. Lets first connec one of the module and configure it as Station.

Configuring Airgrid Module as STATION:-

1. We already have supplied power to the Airgrid module, now connect the ethernet cable coming out of the LAN port of the PoE adapter(shown in above picture 3.) to the PC/Laptop.

2. Now the pc is connected to AirGrid module and the connection is shown as limited connection on pc.

3. To access the AirGrid module we need to login it by its Default IP Address: 192.168.1.20. Lets try opening in internet Explorer.

4. There was a problem opening this default IP address. Lets try one more time but this time we configure our ethernet adaptor on our computer with IP Address: 192.168.1.41 & subnet mask: 255.255.255.0.

5. Lets try to login again. This time it shows certificate error and asks whether to continue to this site or not. Click continue and a Login page is shown over the browser.

6. Login with default username and password: ubnt. Choose your country, accept Terms & conditions and hit login.

7. A welcome screen as shown in Image below will appear. We now know that this module is already configured as Station(by looking at the Wireless Mode in MAIN tab). We still need to configure it with our specifications. Lets move to WIRELESS Tab.

8. Enable WDS. Write MAC address(written adjacent to the ethernet port) of the other AirGrid Module. Enable Frequency Scan List and choose 5835 MHz.

9. Important Step: Lower Down the Output Power near to 0 dBm. I have done this as my distance is very close. Sometimes they blow up if the power set is 25dBm. So for closer range it should be as low as possible.

10. Hit change and Apply settings.

11. Select Network Tab, change IP address to 192.168.1.21. Hit change and Apply. Thats it.

Now one of the Module is configured as Station:-

 

imageimage

     1. Ethernet cable connected to pc                         2. Problem in Accessing default IP address of AirGrid Module

 

imageimage

                            3. Configuring ethernet adaptor on computer                                           4. validate settings and selec Ok, network diagnostic will run automatically

imageimage

      5. Trying default IP again, shows Certificate Error, click Continue & add certificate in exception List.                        6. Login page

 

imageimage

                                   7. Not configured Airgrid Module MAIN page                                                      8. MAIN page showing No AP information

 

 

Configuring Module to Station:

imageimage

                                                       9. Select Wireless Mode                                                           10. Enable WDS, insert MAC Address of other AirGrid Module

imageimage

                         11. Select Frequency from list                                                                                           12. Output Power to 0dBm

                                                                      image

                                                                                                    13. Change and Apply Settings

                        

Now changing the IP address of Station Module:

imageimage

                              14. NETWORK page, change IP address                                                                            15. Click change and Apply

 

imageimage

       16. New IP address of Station Module, login with default Username & password                    17. AirGrid Mosule configured as Station WDS

 

Configuring second Airgrid Module as Access Point(AP):-

1. Power up the second AirGrid module with PoE and connect the ethernet cable coming out of PoE adapter to PC.

2. Now enter the default IP address in browser: 192.168.1.20. Enter the Login details same as previous.

3. Select WIRELESS tab and choose Access Point in Wireless mode. Now the page will change few settings.

4. Enable WDS & Frequency list. Choose 5835 MHz from frequency list tab.

5. Change Output power to 0 dBm. Hit change and Apply. That's it. We need not to change NETWORK settings.

Now the other module is configured as AP(Access Point):-

imageimage

           18. Configuring AirGrid Module for Access Point                                           19. Keep NETWORK settings as it is

                                                                      image

                                                                                                                             20. AirGrid Module configured as AP

Now, Place both the Modules in Line of sight but little far from each other:

imageimage

                              21. Station and AP connected, LED's shows the signal strength                                                            22. Station and AP connected, details are shown by airOS

Now we have established a Wireless connection between both the Modules, Now, we can use various test tools on airOS.

                                                            image

                                                                                          23. Different tools used to test, debug AirGrid Modules



Align Antenna:

This is used to alignment of the two AirGrid modules when they are installed on site. For better data transmission Line of Sight of two modules must be clear. We use this tool to align both the modules to get maximum data transfer with low loss and low Output Transmission power.

imageimage

                              Align Antenna tool showing signal & noise levels                                                                                Changed position of modules shows change in these readings

 

Site Survey:

This tool is used to Search all the wireless networks in range on all supported channels. As we have already set it for 5835 MHz it will scan for all the wireless networks in range with this frequency.

                                                                 image

                                                                                               Station Module Site Survey scanning results showing AP module

 

Discovery:

The Device Discovery tool searches for all Ubiquiti devices on the network.

                                                            image

                                                                               Discovery tool showing both the discovered modules with their respective IP Address

 

Ping:

Ping is the most common tool we use in networking. We use it to discover & find latency of the device on the network. With this tool we can ping other devices on the network directly from the device. The Ping tool uses ICMP packets to check the preliminary link quality and packet latency estimation between two network devices.

We know,

     IP Address of our laptop: 192.168.1.41

     IP Address of Station Module: 192.168.1.21

     IP Address of AP Module: 192.168.1.20

imageimage

                         Station side Ping tool showing AP and Laptop IP addresses to ping.                                                             Result when AP IP address is selected to ping with mentioned packets.

 

Traceroute:

The Traceroute tool traces the hops from the device to a specified outgoing IP address. This tool is used to find the route taken by ICMP packets across the network to the destination host.

                                                       image

                                                                                          Station side results when AP address is selected

Speed Test:

This tool is used to test the connection speed between two modules.

imageimage

                    Station module speed test tool located two devices IP Addresses on network                                                                      Speed test between Station and AP

                                                                           image

                                                                                                              Results of Speed test between Station and AP modules

 


All these tests shows we have establish a Wireless link between two AirGrid Modules Successfully and these are working with proper data transmission rate & speed.

                                                                                                               

                                                                                                                                                    Task 1: Complete.

 

Task 2: Connect ARM mbed IoT starter Kit with AirGrid M5-HP module(AP).

Disconnect both the ethernet cable from pc side, which are used to establish connection between Airgrid modules and pc/laptop. Now, we are going to install these Airgrid modules on poles and create Home to office like conditions by placing them far from each other. Connect one of the ethernet cable coming out of the PoE adapter of AP AirGrid Module to the ethernet port on the Starter Kit.

                                                                      image

                                                                                               AP connected to ARM mbed IoT Starter Kit

                                                                

                                                                                   

                                                                                                                   Task 2: Complete.

 

Task 3: Connect Station AirGrid module to Internet(modem).

We left with one ethernet cable coming out of PoE adapter of Station Airgrid Module. We are going to connect this cable to the Modem which has Internet Access to it.

                                                                                                                   Task 3: Complete.

                                

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
image

                                                   Station Module Connected with Modem

 

Final Steps & Working:

What we have done till now:

We have connected ARM mbed Iot Starter kit to AP module and Station module to Modem(Internet). Indirectly we can say, (If we consider Station and AP modules Wireless link as a single LAN cable link) we have connected Internet to the IoT starter Kit. So, Starter Kit running demo code will try to connect to IBM cloud and when the connection is established(Green LED will glow) it will send its sensors data to IBM Site over the internet. This means if the whole setup is working we should get our Startkit sensors reading on the IBM site. Let's see what happens when we power on both the modules PoE and Modem. For this experiment I have supplied power to Starter Kit with the help of a smartphone charger to show that all the readings on laptop are coming over the internet not from USB cable.

imageimage

                                             Starter Kit(at home) trying to connect to Internet(at Office)                                                                  Starter Kit(Home) connected to Internet(Office) via AirGrid Modules

 

Though, the whole story got completed in above two Pictures but it was not that easy for me to establish this connection as I have some problems with my ISP(nowadays) and after every half minute my modem gets disconnect from the internet. You will find that problem in the video I made. The Voice in the video is not clear as It was not intended to attach here (I was just testing it). I tried to make another good quality video but as my ISP is dropping everytime and I only had this video in which my ISP got stable for few minutes.

                                                                                                                                                      Video




                                                          

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image





In this video we can see that our Starter Kit has successfully established a connection to Internet(Modem at Station side) and it can be confirmed by looking at the readings of sensor data on IBM foundation of Things page which is coming over internet.


Result: By this experiment we have seen that we can use this Kit to sent data Over Internet even if we have Internet Access is  far away from the Kit with the help of AirGrid Modules. We have succesfully established a connection between IoT starter Kit and Internet enabled Modem with the help of AirGrid Modules. So the experiment is a Success.


Confused?

How or In what way this experiment is related to Home Automation?

Home Automation type Conditions:-

Suppose, we have a starter Kit at our home which is connected to several input sensors & output devices like motor, Fan etc (might be connected with the help of bluetooth/Wi-fi or through Wires directly). Now, Home Automation for this case will be, to read the reading of Sensors and to control the output devices accordingly from some place far from the home.

We have two case to control the Starter Kit and use it for home automation purposes.

Cases:-

#Homeautomation1. We can give Internet direct access to the Starter Kit, get its reading over the internet from anywhere else in the world and control this Kit over the same Internet.

#Homeautomation2. We do not have Internet and we Just want to control aur home devices from a distant place like Office/Workplace. This is the case where we use AirGrid modules to connect our Home to workplace. Now we need to do little tweaks in the experiment done above.


1. First case is simple, just connect Internet to the Starter Kit and then we just need a controlling software on pc(Internet enabled) to use it for Home automation.

2. For the Second case, we will make few changes in the above experiment.

This case is exactly like what we have done in experiment above:

                                  

|  ARM mbed IoT Starter Kit  |                   _______________                                                   __________________                 | Internet(Modem) |

|               (at Home)             |-----------| AP AirGrid module }   ===================  { Station AirGrid Module |------------|       (at Office)     |


Lets make few change in this:

             

                     

|  ARM mbed IoT Starter Kit  |                  _______________                                                        __________________                    | pc with Software program to control Kit |

|               (at Home)             |-----------| AP AirGrid module }   ===================  { Station AirGrid Module |------------|                    (at Office)                          |

              

So, we have replaced Internet(Modem) at office with Laptop/pc which has a software program written in C/python or any other language which reads the Starter Kit inputs and send control commands to it. Now, we can control this Starter Kit (at home) from my workplace via laptop(has Kit control software Program). This will work just as fine as it worked in our experiment above.


So, this concludes the whole experiment explained above is about Home Automation.