Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs The Deeter Group is proud to announce...
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: deetergroup
  • Date Created: 21 Jul 2011 8:07 AM Date Created
  • Views 540 views
  • Likes 0 likes
  • Comments 0 comments
  • distributor
  • wireless
  • system
  • sensor
Related
Recommended

The Deeter Group is proud to announce...

deetergroup
deetergroup
21 Jul 2011

The Deeter Group are proud to announce the launch of their Asia campaign. The Deeter Group has launched www.deetergroup.asia and also would like to announce and welcome a new distributor.

MaxMega was established in 1996. We specialised in marketing, sales and distribution of high performance electronics components and system integrations services.
We distribute both active and passive components. Active components such as Fast/Gigabit Ethernet Switch Controller, System Controller for RISC CPU, High-Speed Physical Layer Solutions, PC Chips sets, CPU, Bluetooth Wireless Solution, Power Management IC and etc. Passive components namely surface mount chip capacitors, precision high power resistors, transformers, connectors, etc.
We serve the major sectors in the hi-tech industry specifically the Data Communications, Data Storage, PC & PDA, Office Equipment, Cellar Phone and Contract Manufacturing.
In additional, we have also diversified our core business into System Integration and Computer Telephony Services. Download Profile in English or Download Profile in Chinese
The guys at Maxmega are really enthusiastic and are looking forward to getting stuck in when it comes to the distribution of Deeter Products.
Last but not least Deeter Engineering would like to let you know about our Liquid Volume Dispenser. Typical applications include dosing of chemicals, colours, flavourings or control of any liquid being dispensed in a manufacturing process or laboratory.

The Deeter Liquid Volume Dispenser will repeatedly deliver a precise, operator selected, measured volume of liquid at the press of a button. The unit features automatic calibration and is temperature compensated to ensure accurate dosing across the wide temperature range of possible fluids being delivered. A USB data-link and control software suite is provided to allow users to externally control the Liquid Volume Dispenser and collect data for logging and archiving.
The liquid volume required is simple to select and the setting is retained in non-volatile memory for repeat operation. Volumes between 0.10 litres and 100.00 litres can be selected in increments of 0.01 litres. The dispenser will accurately measure volumes over a flow rate range of between 0.6 litres/minute and 5 litres/minute.
Peter Whiteaker, Managing Director of Deeter Group comments;”We designed our first fluid dispenser over twenty years ago. We now see a growing market in many manufacturing and laboratory applications and our new design offers customers temperature controlled accuracy and the convenience of control or data-logging via an external computer.”
The Deter Liquid Volume Dispenser has two SpeedfitRegistered push-fit connectors for fluid in and out. These can accommodate a tube with an outside diameter of 8mm. Wetted surfaces are nylon, PTFE, Buna and acetal, making the Liquid Volume Dispenser suitable for a wide range of fluids.
Operator controls consist of a three-button keypad and a liquid crystal display. The display shows the selected volume and progress during dispensing. A number of additional features are available through the keypad, including pause and restart during dispensing, cancelling dispensing, and manual ‘top-up’ control.
An audible ‘beep’ option is provided to indicate when dispensing has stopped and a further option will produce continuous ‘beeps’ if the flow rate is outside of  the limits for accurate volume measurement. These audio options can be enabled or disabled through a display menu and are also saved to non-volatile memory and are restored to the operator’s preference after power-up.
The Liquid Volume Dispenser is powered by a low-voltage supply, making it safe to use if liquid is spilt and a 12VDC mains socket adapter is supplied with each dispenser. Fluid temperature range is +1 to +65ºC and the unit is housed in a 175x125x78mm enclosure. It offers a flow rate range of 0.6 to 5.0 litres per minute with a dispensing volume accuracy of -3%+0% over the flow rate range. Fluid connections are via 8mm outside diameter tube which may be polyethylene, polyurethane, nylon, brass, copper or stainless steel.

# # #


The Deeter Group is regarded as a leading international company in the design, development and production of electronic sensors, switches and control and instrumentation systems.