Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs TI Hercules LaunchPad Type 2: Ultrasound Radar
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: martinvalencia
  • Date Created: 7 Jun 2015 1:47 PM Date Created
  • Views 1064 views
  • Likes 3 likes
  • Comments 1 comment
  • capture
  • ultrasound
  • hercules_launchpad_evaluation_kit
  • steeper
  • boosterpack
  • pwm
  • radar
  • het
  • sp:texas_instruments
  • glcd
Related
Recommended

TI Hercules LaunchPad Type 2: Ultrasound Radar

martinvalencia
martinvalencia
7 Jun 2015
Christian Huelsmeyer, Radar inventor

Radar is an object-detection system that uses radio waves to determine the range, altitude, direction, or speed of objects. It can be used to detect aircraft, ships, spacecraft, guided missiles, motor vehicles, weather formations, and terrain. The radar dish (or antenna) transmits pulses of radio waves or microwaves that bounce off any object in their path. The object returns a tiny part of the wave's energy to a dish or antenna that is usually located at the same site as the transmitter.

Radar was secretly developed by several nations before and during World War II. The term RADAR was coined in 1940 by the United States Navy as an acronym for RAdio Detection And Ranging. The term radar has since entered English and other languages as a common noun, losing all capitalization.

The modern uses of radar are highly diverse, including air and terrestrial traffic control, radar astronomy, air-defense systems, antimissile systems; marine radars to locate landmarks and other ships; aircraft anticollision systems; ocean surveillance systems, outer space surveillance and rendezvous systems; meteorologicalprecipitation monitoring; altimetry and flight control systems; guided missile target locating systems; and ground-penetrating radar for geological observations. High tech radar systems are associated with digital signal processing and are capable of extracting useful information from very high noise levels.(Radar - Wikipedia, the free encyclopedia)

 

 

I made a different range of video where I explain my progress in the development of a RADAR based on the Cortex R4 Texas Instruments family,  videos explains the following:

 

1.- response speed of ultrasound (Arduino) is improved using the PWM generator module microcontroller with  characteristicsT = 50ms  and a positive pulse trigger 10 microsegundos to excite the      ultrasound or dutty cicly of 0.01%; in this way the MCU always get a quick response from the ultrasound.

2. The implementation of a stepping motor (1.65 degree), at every step the MCU makes a catch away and stored in its memory.

3. Once the memory is full, the microcontroller interprets the data as being data in cylindrical coordinates.

4. The MCU performs coordinate transformation using:

 

   x = R * cos (angle)

   y = R * sin (angle)

  were:

   R= ultrasound distance

  angle = angle of stepping motor

 

5. microcontroller proceeds the cartesian coordinates and plot the points on the LCD screen.

6. The distance between the lines of the radar is 7 cm.

 

Warning: Videos in Spanish
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
Picture Album

 

top view of the circuit in general, the first evidence for a DC motor with a reduction box but the response is used as the angle of rotation were quite poor.

image

Ultrasound is that it always uses the Arduino family.

 

image

 

Radar screen operation


image

 

for the first image, I have the radar without moving, that's the reason why one entire line appears on the screen, it is necessary that the radar is in motion so that the MCU makes a graph of objects.

image

 

Once the radar is in operation, it can be clearly seen as the microcontroller average measurements and with better resolution graphics on the screen.

image

image

Download the program and schematic:

Radar Link program - Mediafire

  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +1
    Nice post. I wonder what the early radar developers would make at the level of time control you just demonstrated. Some of those early sets were very difficult to tune and maintain good pulse to pulse…
  • DAB
    DAB over 11 years ago

    Nice post.

     

    I wonder what the early radar developers would make at the level of time control you just demonstrated.

     

    Some of those early sets were very difficult to tune and maintain good pulse to pulse stability.

     

    Still, a nice project and great learning project.

     

    DAB