| My Goal |
|---|
I'm designing a Holter Monitor to cardiac signals that store for 24 hours, the design must use 4 batteries AA as a power source while should methods to extend the life of the batteries.
The Holter Monitor includes 4GB memory SD and a Bluetooth module for transmisicion data to a mobile device that will serve to display the beats per minute (PPM) of the patient.
In the memory must store the impression Time and Date, together with PPM
|
| Block Diagram |
|---|
The following diagram shows the basic idea of the project. As the project was progressed in its development, I had to make some corrections and modifications to the diagram, as a result have the following picture: |
| Hardware Implementation |
|---|
First is implemented, communication with the SD memory [1] and communication with the DS1302 [2] clock circuit. the power supply voltage symmetrical [3] of +1.5 and -1.5V , in order to operate as a power source for cardiac signal amplifiers. This time the high quality amplifiers OPA316 [4] company Texas Instruments is used in the stage cardiac amplifier, which allow me a better behavior of the analog signal and a lower offset voltage. As a last step the Bluetooth RN42 [5] module is configured and connect. |
|
|---|
| In the next part |
|---|
I just hope to improve the algorithm and design of the heart amplifier, since I'm working with a bandwidth of 200Hz, many components are used, will simplify the design of amplifier and filter Analogs by an amplifier and a low pass filter to 16Hz.
I hope the circuit and greatly reduce the power consumption, thus increasing battery life. |
References |
|---|
[1] TI Launchpad MSP432 Memory SD and Energia.nu [3] TIDA-00349 - Amplifier Cardiac Signals [4] OPA316.pdf |
















Top Comments
-
mrchunckuee
-
Cancel
-
Vote Up
+1
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
mrchunckuee
-
Cancel
-
Vote Up
+1
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children