Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs TI MSP432 EKG Monitor Holter Part 1
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: martinvalencia
  • Date Created: 30 Apr 2016 3:11 AM Date Created
  • Views 2337 views
  • Likes 6 likes
  • Comments 10 comments
  • msp432_launchpad
  • bluetooth
  • ds1302
  • Energia.nu
  • texas_instrutments
  • movil
  • ekg
  • monitor holter
  • dsp
  • analog filter
  • opa316
  • apk
Related
Recommended

TI MSP432 EKG Monitor Holter Part 1

martinvalencia
martinvalencia
30 Apr 2016
My Goal

I'm designing a Holter Monitor to cardiac signals that store for 24 hours, the design must use 4 batteries AA as a power source while should methods to extend the life of the batteries.

 

The Holter Monitor includes 4GB memory SD and a Bluetooth module for transmisicion data to a mobile device that will serve to display the beats per minute (PPM) of the patient.

 

In the memory must store the impression Time and Date, together with PPM

 

image

 

 

Block Diagram

The following diagram shows the basic idea of the project.

image

As the project was progressed in its development, I had to make some corrections and modifications to the diagram, as a result have the following picture:

image

 

Hardware Implementation

First is implemented, communication with the SD memory [1] and communication with the DS1302 [2] clock circuit.

image

the power supply voltage symmetrical [3] of +1.5 and -1.5V , in order to operate as a power source for cardiac signal amplifiers.

image

This time the high quality amplifiers OPA316 [4] company Texas Instruments is used in the stage cardiac amplifier, which allow me a better behavior of the analog signal and a lower offset voltage.

image

As a last step the Bluetooth RN42 [5] module is configured and connect.

image

 

Software Implementation (Still Beta)

All application of Holter monitor, this check in Energia 17

This image shows the form of heart wave, catch the oscilloscope.

image

For treatment of cardiac signal, the first capture each 14.6ms a number of 1024 samples, to capture 15 seconds of the cardiac signal.

image

 

Then the cardiac signal is derived to obtain a vector where we find it much easier to recognize what points maximums of cardiac function.

image

Eliminate the negative area "derived vector", so only work with positive values, an algorithm to count the number of peaks stored during a sampling period of 15 seconds is then implements, and for last this value is multiplied by 4 to obtain the pulse per minute.

image

 

Implementation of communication with the DS1302 Clock by energia.nu

image

 

The algorithm of counting pulses and display of heart beats per minute in the serial screen Energia.nu

image

 

Finally the transmission was implemented by bluetooth to the mobile deice and here the result.

(During these tests, there was no patient connected to the computer so the measurement pulse is erratic, even I must devote more hours to count algorithm heheimageimage)

image

 

 

In the next part

I just hope to improve the algorithm and design of the heart amplifier, since I'm working with a bandwidth of 200Hz, many components are used, will simplify the design of amplifier and filter Analogs by an amplifier and a low pass filter to 16Hz.

 

I hope the circuit and greatly reduce the power consumption, thus increasing battery life.

 

 

References

[1] TI Launchpad MSP432 Memory SD and Energia.nu

[2] DS1302 Circuit Clock  

[3] TIDA-00349 - Amplifier Cardiac Signals

[4] OPA316.pdf 

[5] RN42 Module Bluetooth 

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 10 years ago +2
    Hi Martin, This is a great project. I enjoyed your presentation and I hope to continue following your progress. John
  • dougw
    dougw over 10 years ago +1
    Nice job, Have you tested your battery life yet? Does Energia have SD card drivers or do you need to program them yourself?
  • martinvalencia
    martinvalencia over 10 years ago +1
    I can not yet test lifetime with the battery but I'm making an estimate of the current consumption of the circuit in general and I count the hours of life, the testing effected, when I have the circuit…
  • martinvalencia
    martinvalencia over 10 years ago in reply to DAB

    Thank you very much for your comment, I always try to use a good combination between images and explanation, since my native language is Spanish, almost always used as support images to leave the reader better understand my message.

     

    Best Regards

    Martin V.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • martinvalencia
    martinvalencia over 10 years ago in reply to mrchunckuee

    Hey Muchas gracias, por su comentario!

    Saludos

    Martin V.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • martinvalencia
    martinvalencia over 10 years ago in reply to clem57

    It was easy solder to wires at SD adapter memories but only I should be very careful not to overheat the plastic.

    Best Regards

    Martin V.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • martinvalencia
    martinvalencia over 10 years ago in reply to jw0752

    Thank you very much for your feedback!

    this is a project I had in mind since a long time ago.

     

    Best Regars

    Martin V.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Excellent detailed post and methodical development procedure.

     

    Well done.

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>