Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Tibbo Project System-based Office Aircon Controller Application
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dmitry_slepov
  • Date Created: 3 Oct 2016 8:04 AM Date Created
  • Views 675 views
  • Likes 0 likes
  • Comments 0 comments
  • application
  • tps
  • iot"
  • tibbo
Related
Recommended

Tibbo Project System-based Office Aircon Controller Application

dmitry_slepov
dmitry_slepov
3 Oct 2016

The app allows you to manage traditional air conditioners that are controlled through infrared remotes. Designed for the office environment, the app relies on the ambient brightness (measured by Tibbit #28) to determine whether the aircon should be running or not. In the office setting, no lights = no people = no need for the aircon to work.

 

TPS-based aircon controller

TPS-based aircon controller

Air conditioning is a wasteful business, and air cons are expensive to run. Most aircon systems, especially older ones, do not have any real temperature feedback. The temperature you set on your remote has absolutely nothing to do with the actual temperature in the room. Even when the weather gets colder, many air conditioners continue to blast cold air into your space. As a result, you have to adjust and constantly readjust your room temperature.

No doubt, AC systems are improving day by day, but there are still old systems that cannot get updated. In some instances, it's absolutely impossible to invest in a new system. Sometimes, it is just a catch 22 to rip the old aircon out and install a new one. A basic aircon has many parts that typically are split between an outside and inside configuration, hence you may have to undergo a drastic interior renovation. In Tibbo office in Taipei, we have got trapped in an identical situation. We just have to get by with the AC system we've got. Our aircon is controlled with a dozen of infrared remotes lying around.

A while back, we set a challenge to create a management system for our dated HVAC system. Needless to say, we used our Tibbo Project System (TPS) for this endeavor. Our spec for the aircon controller consisted of two main items:

  • We wanted the aircon to run or not run depending on whether the lights are on or off. Since this is an office, no lights = no people = no need to run the aircon.
  • We wanted the device to monitor the actual temperature in the room and stop the aircon whenever the temperature cooled off to the preset point.

 

We have achieved our goal by using a TPS2L system equipped with these Tibbits:

 

  • Ambient temperature probe
  • IR code processor Tibbit (#26)
  • IR front-end Tibbit (#27)
  • Ambient light sensor Tibbit (#28)

 

A  few words about the probe. This is a new item that will be announced this fall. The probe replaces the ambient temperature meter (Tibbit #29). It is handy to have the meter built right into the TPS. The bottleneck is, the meter is influenced by the internal heat of the TPS system itself. This impact is particularly visible for the TPS2L device - it's LCD really warms up the box! The latest sensor has the same circuit as the Tibbit #29, with the additional advantage of being external to the TPS device. From now on, the measurements are accurate.

Here is a look at the items you need to set up in the menu:

IR commands. This is where you train your IR code processor to be able to transmit two commands: "On," and "Off." For the "On" command, use the lowest temperature that your aircon's remote allows you to set (usually 16 degrees C). The logic here is that when you need to lower the temperature in the room you can use the coldest temperature setting, and when the room cools down to the preset temperature, the aircon is turned off. So really, you only need two commands.

Target temperature. You don't need to set it here. There are dedicated buttons on the main screen.

Pre-cool start time. This is something we added along the way. Now it is possible to turn the aircon on, once a day, even before we all arrive at the office. Our day starts at 9 am. We set this time for 8:30 am, and by the time we get in, the office is nice and cool (while the scorching Taipei summer keeps on raging outside). The pre-cool timer is hardcoded for 45 minutes. If the lights are still off at 9:15 the aircon is turned off.

Brightness threshold. This is the brightness that the TPS will consider to correspond to "lights on." The value is not expressed in any standard measurement units; it's just the value the Tibbit #28 returns. So, how do you know what number to set here? Simple: the brightness is displayed on the main screen, like this: "Light level: 718". Note the value with the lights off and on, then set the threshold to some value in the middle between the two.

Temp. meas. adjustment. This is useful for when you choose to use the Tibbit #29. As we've explained above, its measurements are affected by the internal heat of the TPS itself. You can use a regular thermometer and determine the measurement error. For example, if your thermometer reads 25C, and TPS shows 28C, then you must adjust the temperature by 3 degrees C. The data returned by the new external probe need no adjustment.

Further work

In phase 2 of this project we will connect our aircon controller to an AggreGate server. It will be possible to control the system via a smartphone app, which we going to design for this purpose. Now you know why our configuration menu has items like Network, AggreGate, etc. Stay tuned!

Zen...