Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Transistors: Some Very Old Ones
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 25 Apr 2017 9:45 AM Date Created
  • Views 1558 views
  • Likes 9 likes
  • Comments 5 comments
Related
Recommended

Transistors: Some Very Old Ones

jc2048
jc2048
25 Apr 2017

The other day, I was sorting through some old boxes and found a small bag of old transistors. There were two types, both

of them PNP devices. One kind was an OC204 part, made by the old British company Mullard, the other a 2S3220 device made

by Texas Instruments. I presume they date from the 1960s.

 

image

 

image

 

image

 

I wondered if they still worked and what their characteristics would be like compared to a modern device so I built up

this circuit of a simple common-emitter amplifier on a breadboard (shown with a modern 2N3906 PNP transistor) so that I

could test them.

 

image

 

For the base bias resistor (R2), I actually used a pot so that I could adjust the collector voltage to be -4.5V (half the

supply voltage). Both devices needed just 13.6k for R2 to bias the collector to -4.5V, unlike the 2N3904, which in the simulation

needed 430k. The gain worked out to be approximately 7 (at a collector current of 2mA). Yes, that's not a typo, the hFE

really is just 7 for both parts.

 

Here are the waveforms of the 2S3220 amplifying a 10kHz sinewave - yellow trace is the input and the blue trace is the collector (AC coupled)

 

image

 

I was curious about the frequency response, so I plotted a crude graph of the amplifier's response for both parts. As you

can see, the response is starting to drop off at just 100kHz, so they'd have been ok for low frequency work - audio

amplifers, etc - but not much use above a couple of hundred kHz.

 

image

 

For contrast, here's what the 2N3906 does in simulation

 

image

  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 9 years ago in reply to shabaz +2
    Unfortunately, I've only got four of the OC204s. The rest are 2S3220s, which a webpage tells me are silicon. I don't know what the date of them is, but the TI parts have codes like 610, 612, 615 on them…
  • DAB
    DAB over 9 years ago +2
    Now you have me wondering about the types of interesting components my be hidden in my stash. Sounds like an excuse to do a treasure hunt. DAB
  • jw0752
    jw0752 over 9 years ago +2
    Hi Jon, I love these explorations into the foundations of electronics. Just like DAB I am going to have a look into my parts graveyard for some moldy oldies to test out. John
Parents
  • shabaz
    shabaz over 9 years ago

    This is very cool : ) Germanium transistors sell for a lot of money these days, even with that gain of 7 probably ; )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to shabaz

    Unfortunately, I've only got four of the OC204s. The rest are 2S3220s, which a webpage tells me are silicon. I don't know what the date of them is, but the TI parts have codes like 610, 612, 615 on them, so I would guess that's showing 1966 followed by a week code (week 10, 12, etc). The American companies were well into silicon by then. The OC204s have a code of '3 R 5' which might be 1965. [I would have bought them in the early 1970s as a bargain pack of usable, but no longer state of the art devices.]

     

    The construction of the Mullard parts is fascinating because inside the metal cover there's a glass envelope that houses the semiconductor. That shows their heritage in valve (vacuum tube) manufacture - they knew how to work with glass, so that's what they though to do.

     

    Both cases predate having a tab for the emitter - the Mullard part has a red dot and the TI part has the leads arranged in a triangle.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 9 years ago in reply to shabaz

    Unfortunately, I've only got four of the OC204s. The rest are 2S3220s, which a webpage tells me are silicon. I don't know what the date of them is, but the TI parts have codes like 610, 612, 615 on them, so I would guess that's showing 1966 followed by a week code (week 10, 12, etc). The American companies were well into silicon by then. The OC204s have a code of '3 R 5' which might be 1965. [I would have bought them in the early 1970s as a bargain pack of usable, but no longer state of the art devices.]

     

    The construction of the Mullard parts is fascinating because inside the metal cover there's a glass envelope that houses the semiconductor. That shows their heritage in valve (vacuum tube) manufacture - they knew how to work with glass, so that's what they though to do.

     

    Both cases predate having a tab for the emitter - the Mullard part has a red dot and the TI part has the leads arranged in a triangle.