Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Transistors: The Ho Serial Astable
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 3 Feb 2018 2:26 PM Date Created
  • Views 2006 views
  • Likes 12 likes
  • Comments 4 comments
  • leds
  • transistors
Related
Recommended

Transistors: The Ho Serial Astable

jc2048
jc2048
3 Feb 2018

Back when I first became interested in electronics, a simple way to make an oscillator was a circuit called an astable

multivibrator. These got used a lot - the electronics magazines that I used to buy as a teenager were full of them. This

is the form of it

 

image

 

The two transistors are arranged like a flip-flop, with either one or the other conducting. Unlike the flip-flop, where

the conducting transistor will hold the other off, here the additional capacitors mean that after a period the stable

state ends and the circuit will flip (or, maybe, flop) of its own accord.

 

One of the disadvantages of such an oscillator is that the transistors saturate and there was quite a lot activity from

people trying to come up with alternative designs that would oscillate faster. Another disadvantage was that the

waveforms at the collectors weren't all that good. For the speed side, obviously changing to circuits where the transistors

didn't saturate was the way to go. For the waveform shape issue, several people came up with circuits which had two

transistors in series. This circuit I'm looking at here is by C. F. Ho. I came across it in a Ferranti transistor applications manual from the 1970s.

 

Here it is in the manual

 

image

 

and here it is in the simulator with meters attached to measure things

 

image

At first sight, the circuit looks wonderful; symmetry is often very good in circuit design and this looks like the bee's

knees of circuits (Bat's hats? Cat's corsets? Dog's wotsits?), but appearences can be deceptive as we'll see in a minute.

 

Note: the component labelled 'IC1 2' isn't a real component and isn't needed for circuit operation, it's an initial

condition for the simulator. Effectively, it gives the circuit a 'kick' at start-up. You'll often find something like

this is necessary to get an oscillator going in simulation (the simulation doesn't have the noise and transients that get

real circuits started).

 

If I run it in the simulator and plot the charging waveforms of the capacitors, we'll immmediately see one issue with it

 

image

 

VM3 and VM4 are plots of the voltage across each capacitor and you can immediately see that they charge at the same time.

The period of the pulse is then determind by the discharge time.

 

Nice properties are that there are two outputs - the output can be from either collector - which are complementary (well,

it's a nice property if you have an application where you need two complementary outputs, one of which comes down from

the rail and the other goes up from ground) and the edge rate when it switches is quite good too because there's regeneration

round the loop ("Talkin' 'bout my regeneration" - The Who might have been really big if they'd had me to do the song lyrics

for them) which is where the improvement to the waveform shape comes from.

 

This is a close up of one edge for the two complementary outputs. The other two traces (the green and red ones) are the

voltages across the two timing capacitors and at this scale hardly seem to be moving.

 

 

image

 

The horizontal scale is 200nS per division. The edges really move once they get started and the lower one would be fine

for driving 5V CMOS logic. (Ok, perhaps not; who wants a 5V logic system that then needs a 9V supply for the clock?)

 

Less nice properties are that is sensitive to component values. I found that it was quite fussy about the base resistor

values and if you get it wrong the circuit just sits there and sulks. That in turn limits the charging current so, for

high speed use, the capacitors start to get very small in value.

 

I don't know if anyone ever did anything with this - perhaps Mr Ho had a specific application for it - but it's an

interesting curiosity to look at with the simulator.

 

Since the current through the two transistors when they are both on is something like you might use to light up a

reasonably efficient small LED I thought I'd try doing just that. Simply placing the LED between the two transistor

emitters like this suffices.

 

image

 

I can slow down the timing by simply massively increasing the capacitor values; changing the capacitors to 10uF gives a

suitable timing interval between the flashes and the discharge time is just right for the flash time. It's a natural for

operating off of a 9V battery, too - it will happily work down to 6V or so. Now the low current during the charging

period is something of an advantage; here's the current draw running in the simulator - the bulk of the draw from the

battery is only when the LED is lit

 

image

One disadvantage is that the charging current is so low that if you used poor quality or old electrolytics you might find

the leakage was of the same order as the charging and it would never get to the switching point.

 

Anyway, enough theory, you want to see it working. Here it is wired on a breadboard

 

image

 

and finally, here is a video of the LED flashing (because the world doesn't have anything like enough videos of LEDs

flashing - but at least it wasn't an Arduino this time).

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +3
    Nice article. Fun with transistors! I too would see many articles in magazines and 'electronic cookbooks' with similar circuits. Funny, but today I rarely ever look at transistors (the workhorses of yesteryear…
  • jw0752
    jw0752 over 8 years ago +3
    Hi Jon, I like your writing style as it always keeps me fascinated right up to the last word of your posts. I enjoy that you focus on these simpler circuits that I can mock up on my own bench and take…
  • DAB
    DAB over 8 years ago +2
    Now here is a post that takes be back a bunch of decades. I built my first oscillator using tubes in tech school. I did not get my hands on any transistors until I started working in the real world. Well…
Parents
  • jw0752
    jw0752 over 8 years ago

    Hi Jon,

    I like your writing style as it always keeps me fascinated right up to the last word of your posts. I enjoy that you focus on these simpler circuits that I can mock up on my own bench and take a look at. Your analysis is always above my knowledge level so it is never a review for me but an actual learning process. In my opinion post like these are a core element of what this forum is about.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 8 years ago

    Hi Jon,

    I like your writing style as it always keeps me fascinated right up to the last word of your posts. I enjoy that you focus on these simpler circuits that I can mock up on my own bench and take a look at. Your analysis is always above my knowledge level so it is never a review for me but an actual learning process. In my opinion post like these are a core element of what this forum is about.

    John

    • Cancel
    • Vote Up +3 Vote Down