Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs TRISE to be an Output.
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: YT2095
  • Date Created: 28 Feb 2012 11:27 AM Date Created
  • Views 627 views
  • Likes 1 like
  • Comments 0 comments
Related
Recommended

TRISE to be an Output.

YT2095
YT2095
28 Feb 2012

Awww c`mon, my spelling`s not That bad! image

I`v been experimenting with the Digilent Uno32 board over the last 2 days, in particular to sse just How arduino compatible it is in the IDE, and what neat things can be done with a board that`s ~5X faster than a 328p chip.

being a simple soul that`s happy with an 8 bit data bus and few control lines to do almost anything I`m likely to want, the First thing I wanted to check was things DDRD and PORTD type commands.

now I know you can use pinmode and digitalwrite and stuff, but I find it more natural to write to ports directly (personal taste), the thing that really surprised me with the MPide, was that PORT`x` commands were actually allowed! image

it totally didn`t like DDR`x` though, so I tried the TRIS command that PICs use and That worked just fine, a Note: on AVR chip all 1`s are Output, on PIC 0`s are output!

ie/

DDRD = B11111111 for outputs on AVR

TRISD = B00000000 for outputs on a PIC

 

anyway, I tried all the Arduino ports like B and D, and they`re not 100% compatible at all, in fact one of them only gives you 7 bits? so Im guessing it`s used internally or on the board for something else.

so naturaly I went through the Alphabet poking around with an LED to see what changed, and port `E` seems to be the droids I was looking for! image

the magic command is TRISE.

so... I wired up my recently built D to A convertor to pins 26 to 33 (LSB to MSB respectively), and wrote probably the smallest program ever;

 

void setup (void) {

TRISE =B00000000;

}

void loop() {

  PORTE = (analogRead(A0)>>1);             

}

 

this little prog simply takes a reading from analog pin 0 and shoves it out as an 8 bit binary number onto pins 26-33, where the D to A board turns it back into Analog again.

you Could use /2 to make it into an 8 bit number instead, but shifting to the right  ">>1" does the same only faster and uses less mem.

also the prog will take a delay of up to 50 micro seconds, so there`s plenty of room to manipulate this data if you plan on using it for Audio without any noticable effects.

 

use this for a simple white noise gen:

void setup()

{ TRISE = B00000000; //sets pins 26 to 33 as outputs

}

 

void loop()                    

{

  int n = random(0,256); //picks a random 8 bit number

  {  

    PORTE = n;  //outputs number `n` to port E                               

    delay(10); // kill this line for a higher frquency

  }

}

 

or for real speed, just have this as your Loop:

PORTE =random(0,256);

 

Hopefully this may save someone a bit of time figuring it out for themselves, and leave them free for doing all sorts of funky Maths stuff with the data!

Now I`m off to listen to Blondie again through my Uno32 board, I have no idea why, but She`s always the "victim" of my A to D to A experiments?

 

C`mon baby, hit those High notes, I need to test my lowpass filter!