Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Unboxing the Logitech C920 HD Pro Webcam
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ninjatrent
  • Date Created: 9 Mar 2018 3:59 PM Date Created
  • Views 13702 views
  • Likes 8 likes
  • Comments 7 comments
  • usb camera
  • h.264
  • logitech c920
  • microsoft windows
  • opencv
  • beaglebone blue
  • beagleboard.org
  • bonecv
  • BeagleBone
  • ios
  • pocketbeagle
  • beagleboard
  • webcam
  • logitech
  • beaglebone black wireless
  • BeagleBone Black
  • linux
Related
Recommended

Unboxing the Logitech C920 HD Pro Webcam

ninjatrent
ninjatrent
9 Mar 2018

Unboxing the Logitech C920 HD Pro Webcam

image

Hi everyone. I recently purchased the Logitech c920 HD Pro Webcam for a project and I thought it would be nice to share this experience.

http://www.newark.com/logitech/960-000764/webcam-hd-1920-x-1080-usb/dp/48T0195?ost=Logitech+C920+HD+Pro+Webcam&ddkey=htt…

The Logitech c920 HD Pro Webcam is a 15 MP USB webcam that is capable of Full HD 1080p and comes equipt with 20-step autofocus and stereo microphones. This webcam features native H.264 video compression, automatic low-light correction, and HD glass lens with tuned autofocus. It is USB 2.0 certified and USB 3.0 ready.

image

image

There appears to be some dust on the inside of the package.

image

The stats for this webcam are listed in the column on the right side.

image

First layer of defense.

image

Mr. Task Force is here to assist with the unboxing.

image

image

image

Normal documentation

image

This document contains some helpful illustrations of mounting options.

image

Okay. Now on to the main course. What's this? There's dust particles on the camera. Hmmm

image

With the webcam freed of it's imprisonment in the package, we can get a better look.

The camera is a bit heavier than expected. It weighs about the same as a standard Android Smartphone. (sorry Apple)

image

This shot is actually upside down. This is the mount at point of articulation when the webcam's lens is tilted upward.

image

And in this photo, the mount when the webcam is tilted downward. It is very solid and remains in position when adjusted.

image

The mount folds out and can be adjusted to fit most screens.

image

There is a thin layer of silicone on the surfaces to further stabilize the mount.

image

When the mount is  in the closed position, the webcam can be placed on a desktop, table, or other horizontal surface.

On the bottom surface of the mount is a threaded socket for mounting to a standard camera tripod. On the topside of the mount, there are some scratches that occured during removal of the protective factory shrink-wrapped plastic. The finish of the plastic mount and webcam case scratch fairly easy.

image

Here is the forward view when then webcam is pointed downward as far as it can go.

image

And here the webcam is looking up. There is a microphone on each side of the lense for recording audio in stereo.

image

According to this label, the webcam is powered by 5V 500 mA.

image

The USB plug is a slim design that should not conflict with other plugs in adjacent USB ports.

 

Summary

 

The Logitech c920 HD Pro Webcam appears to be a well designed product. It is Windows and iOS compatible, but I will be testing it for compatibility with Linux.

 

I will post some samples of video and image captures with this Logitech webcam in comparison with another webcam.

 

Thanks for stopping by.

 

Trent

 

 

 

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 8 years ago +4
    It's surprising that these USB web cams are still available to buy after all those years (6+ ?). I think it has since been superseded by the C922 version. They worked well with the camera-based NEC projector…
  • beacon_dave
    beacon_dave over 8 years ago in reply to shabaz +4
    We tend to use it for stacking more than edge blending - usually when we need around 20,000 ANSI lumens for a large screen projection. So the images from 4 projectors layered directly on top of each other…
  • genebren
    genebren over 8 years ago +3
    Enjoy your new toy, I mean camera. Gene
  • beacon_dave
    beacon_dave over 8 years ago in reply to shabaz

    It can also be a good technique in case a lamp should fail - you lose a bit of brightness rather than the complete image.

     

    One downside is that if  the projectors are nudged, then you get a ghosted image.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to beacon_dave

    That's very clever! Nice how it allows the presenter to walk across without impairing the image significantly.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to shabaz

    We tend to use it for stacking more than edge blending - usually when we need around 20,000 ANSI lumens for a large screen projection. So the images from 4 projectors layered directly on top of each other.

    https://www.youtube.com/watch?v=NarilvwH4fk

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago

    Hi Trent,

     

    Great review! Nice to see some manufacturers make decent video cameras for laptops/PCs.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to beacon_dave

    Very cool video!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>