Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs USB-C Power Delivery Sink (CYPD3177)
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wolfgangfriedrich
  • Date Created: 17 Feb 2020 12:55 PM Date Created
  • Views 6250 views
  • Likes 8 likes
  • Comments 8 comments
  • power delivery
  • usb-c
  • p-fet
  • cypd3177
  • usb pd
Related
Recommended

USB-C Power Delivery Sink (CYPD3177)

wolfgangfriedrich
wolfgangfriedrich
17 Feb 2020

A USB-C PD Sink up to 20V 5A based on the Cypress CYPD3177 USB PD Controller

 

Edit: NEW Rev 4 now available. Important improvement with a 2nd switch to select the current! New FETs have a Rds_on of only 9.5 mOhm, which cuts the dissipation almost in half and keeps the board cooler, even with 5 A current draw.

 

image

 

USB-C PD offers the option to negotiate power delivery from a compatible power supply. This board plays the role of a sink device, enabling any device to be powered from a USB power supply. Any type of power connector can be attached through a 2-pin screw terminal or directly soldered into the PCB for a lower profile.

The voltage can be set to 5V, 9V, 12V, or 20V and  current can be set to 1A, 2A, 3A, or 5A.

BCR stands for Barrel Connector Replacement, the term is invented by Cypress, the manufacturer of the controller chip in use here.

 

Details

 

 

This board has the goal to replace random power adapters with a standardized way to use a USB-C power delivery (USB PD) adapter instead. For regular operation, no programming or software configuration is involved with this design. All options are set through the switches or resistor values. If needed an I2C interface to a microcontroller is available, to access status and control registers. This part of the board is separated through a break-off tab (mouse bites) and can be snapped off. I made the conscious design decision to not add a USB-A connector option at the output end. I did not want to build a device, that is capable of putting more than 5V on the VBUS pin of a regular USB cable and potentially destroy the device that is plugged in. A heatshrink tube can protect the board in a permanent installation.

 

This is a set and forget device. Set your current and voltage needs before plugging the device to your USB-PD source and enjoy the power at the output. This is not a power supply to change voltage and current during operation.

 

All Features:

  • USB-C PD Power Delivery Sink
  • Selector switch S1 for 5V, 9V, 12V, or 20V
  • Selector switch S2 for 1A, 2A, 3A, or 5A
  • Max current 5A, settable in 250mA steps through resistor options
  • Red LED to indicate failed power request
  • I2C telemetry interface to controller chip
  • Snap off option for telemetry interface
  • For fixed voltage, the switch can be replaced by wire jumper
  • Small form factor to be heat shrinked as part of the power cable
  • Size 53mm x 15.4mm (without telemetry interface)
  • Height 12mm with screw terminal and switch, 6mm without.
  • 3" (7.5cm) heatshrink tube for protected installation
  • 2oz copper to safely handle 5A
  • Lead free RoHS compliant

 

Design Information

 

New FETs with lower Rds_on (and another FET)

 

Selecting the right FET

 

Schematic attached below and available here:

 

https://hackaday.io/project/168762-usb-c-power-delivery-sink-bcr/files

 

 

 

Full disclosure

This board is for sale in my Tindie Store.

I sell on Tindie

 

Attachments:
imageSC USBC-Sink_ver4.pdf
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz +2
    There’s more info on https://hackaday.io/project/168762-usb-c-power-delivery-sink-bcr https://cdn.hackaday.io/files/1687627220313408/SC%20USBC-Sink_ver1.pdf
  • wolfgangfriedrich
    wolfgangfriedrich over 6 years ago in reply to Jan Cumps +2
    That is good detective work. HaD.io is where this project started. All is updated with rev 2 files now.
  • wolfgangfriedrich
    wolfgangfriedrich over 6 years ago in reply to Jan Cumps +2
    Thank you very much, this is very helpful. And I learnt something today, so I can go home now. Oh, I am home already, YAY for Heritage day in Canada.
Parents
  • shabaz
    shabaz over 6 years ago

    No schematic? Otherwise it's just an ad for a product it seems.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 6 years ago in reply to shabaz

    Yes, you are right. The blog post is updated and there will be more information in the future.

    How do I attach documents to blog posts, without the need to link them from somewhere else?

     

    And yes, this is a shameless self-plug, I hope somebody will find it useful and wanted to get it out there.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • wolfgangfriedrich
    wolfgangfriedrich over 6 years ago in reply to shabaz

    Yes, you are right. The blog post is updated and there will be more information in the future.

    How do I attach documents to blog posts, without the need to link them from somewhere else?

     

    And yes, this is a shameless self-plug, I hope somebody will find it useful and wanted to get it out there.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to wolfgangfriedrich

    wolfgangfriedrich  wrote:

     

     

    And yes, this is a shameless self-plug, I hope somebody will find it useful and wanted to get it out there.

    When you edit a post (link in the right margin) , you'll find an "attach" link at the bottom of your post.

    Click it, and you can upload documents.

    Save after you've attached them (you can attach more than 1 doc).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 6 years ago in reply to Jan Cumps

    Thank you very much, this is very helpful. And I learnt something today, so I can go home now. Oh, I am home already, YAY for Heritage day in Canada.image