Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Using Docker on Raspberry Pi B+
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 6 Feb 2015 9:04 AM Date Created
  • Views 1667 views
  • Likes 0 likes
  • Comments 0 comments
  • smart_home
  • single-board_computers
  • raspberrypi
  • iot
  • benchmark
  • docker
Related
Recommended

Using Docker on Raspberry Pi B+

e14 Contributor
e14 Contributor
6 Feb 2015

In 2014 I watched new single-board-computers enter the market. Since I am very fond of the Raspberry Pi project and I am using RPi for quite some time, I am now curious about the differences. I am currently looking for a suitable platform to be used as a base station for my home automation project. I wouldn't call this a server since this term is in most cases used for different hardware. In this context reliability, cost of operation running 24/7, ease of use are the most important factors for me. I am going to write a series of blog posts on benchmarks of the different models in this context.

 

Raspberry Pi B+ replaced the B model mid 2014. It offers four USB ports, a micro sd card slot and lower power consumption. I has a 700MHz BCM2835 ARM processor and 512MB SDRAM.

 

image

To install Archlinux on RPi I followed this perfect set of instructions for installation:

Raspberry Pi | Arch Linux ARM

 

Then I booted the RPi B+ from that sdcard and now I use my laptop to ssh into the RPi:

$ ssh root@alarmpi
The authenticity of host 'alarmpi (192.168.1.214)' can't be established.
ECDSA key fingerprint is db:8c:db:b9:bd:cc:b0:cb:de:a2:c8:a0:2f:73:17:e4.
Are you sure you want to continue connecting (yes/no)? yes
Warning: Permanently added 'alarmpi,192.168.1.214' (ECDSA) to the list of known hosts.
root@alarmpi's password:
Welcome to Arch Linux ARM

     Website: http://archlinuxarm.org
       Forum: http://archlinuxarm.org/forum
         IRC: #archlinux-arm on irc.Freenode.net

 

Sync and update:

$ pacman -Syyu
$ pacman-db-upgrade

 

An optional step is to configure a suitable hostname to replace "alamrpi" for your new RPi based docker machine. I choose "kujira04" for that.

$ hostnamectl set-hostname kujira04

 

And now the installation of the docker package itself:

$ pacman -S docker systemd

 

Enable docker to run as a service:

$ systemctl enable docker.service

 

Done! Now we will reboot the RPi and check if everything worked as expected:

$ shutdown -r now

 

Check that the docker service is running:

$ ifconfig
...
docker0: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500
    inet 172.17.42.1  netmask 255.255.0.0  broadcast 0.0.0.0
    ether 56:84:7a:fe:97:99  txqueuelen 0  (Ethernet)
    RX packets 0  bytes 0 (0.0 B)
    RX errors 0  dropped 0  overruns 0  frame 0
    TX packets 0  bytes 0 (0.0 B)
    TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
...

 

I am now able to use arm specific docker containers (as a convention they are usually prefixed with "rpi-"). In this example I load my "rpi-bench" container from docker hub and run it.

$  docker run -t finklabs/rpi-bench   
180.3751s
1.6125Mb/sec
374.174 MiB/s

 

That's it. Here my benchmark results for the Raspberry Pi B+ model:

 

BoardRaspberry Pi B+ model
CPU (lower is better)180.4 sec
FileIO1.6 MB/sec
Memory374.2 MiB/sec
Wattage1.41 Watt

If you are interested in this work let me know.


Parts used:

  • Raspberry Pi B+ Model


Resources

  • Raspberry Pi | Arch Linux ARM
  • IBM Docker benchmarking research paper


Have fun!

Mark